Package | Description |
---|---|
nxopen.features.sheetmetal |
Provides classes and interfaces for Sheet Metal Features.
|
Modifier and Type | Field and Description |
---|---|
static FlangeBuilder.WidthTypeOptions |
FlangeBuilder.WidthTypeOptions.AT_EDGE_END
The flange starts from the specified end of the edge.
|
static FlangeBuilder.WidthTypeOptions |
FlangeBuilder.WidthTypeOptions.CENTER_OF_EDGE
The flange is centered on the edge.
|
static FlangeBuilder.WidthTypeOptions |
FlangeBuilder.WidthTypeOptions.CUSTOM
The flange sketch has been edited after creation and may or may not conform to any of the above.
|
static FlangeBuilder.WidthTypeOptions |
FlangeBuilder.WidthTypeOptions.FROM_BOTH_ENDS
The flange starts and ends at specified distances from the ends of the edge.
|
static FlangeBuilder.WidthTypeOptions |
FlangeBuilder.WidthTypeOptions.FROM_EDGE_END
The flange starts at a specified distance from an end of the edge.
|
static FlangeBuilder.WidthTypeOptions |
FlangeBuilder.WidthTypeOptions.FULL_EDGE
The flange spans the entire edge.
|
Modifier and Type | Method and Description |
---|---|
static FlangeBuilder.WidthTypeOptions |
FlangeBuilder.WidthTypeOptions.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static FlangeBuilder.WidthTypeOptions |
FlangeBuilder.WidthTypeOptions.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static FlangeBuilder.WidthTypeOptions[] |
FlangeBuilder.WidthTypeOptions.values()
Returns an array that contains the values for this enum.
|
FlangeBuilder.WidthTypeOptions |
FlangeBuilder.widthType()
Returns the width type for flange.
|
Modifier and Type | Method and Description |
---|---|
void |
FlangeBuilder.setWidthType(FlangeBuilder.WidthTypeOptions widthType)
Sets the width type for flange.
|
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.