public static class FlangeBuilder.WidthTypeOptions extends Enum
Modifier and Type | Field and Description |
---|---|
static int |
_AT_EDGE_END
The flange starts from the specified end of the edge.
|
static int |
_CENTER_OF_EDGE
The flange is centered on the edge.
|
static int |
_CUSTOM
The flange sketch has been edited after creation and may or may not conform to any of the above.
|
static int |
_FROM_BOTH_ENDS
The flange starts and ends at specified distances from the ends of the edge.
|
static int |
_FROM_EDGE_END
The flange starts at a specified distance from an end of the edge.
|
static int |
_FULL_EDGE
The flange spans the entire edge.
|
static FlangeBuilder.WidthTypeOptions |
AT_EDGE_END
The flange starts from the specified end of the edge.
|
static FlangeBuilder.WidthTypeOptions |
CENTER_OF_EDGE
The flange is centered on the edge.
|
static FlangeBuilder.WidthTypeOptions |
CUSTOM
The flange sketch has been edited after creation and may or may not conform to any of the above.
|
static FlangeBuilder.WidthTypeOptions |
FROM_BOTH_ENDS
The flange starts and ends at specified distances from the ends of the edge.
|
static FlangeBuilder.WidthTypeOptions |
FROM_EDGE_END
The flange starts at a specified distance from an end of the edge.
|
static FlangeBuilder.WidthTypeOptions |
FULL_EDGE
The flange spans the entire edge.
|
Modifier and Type | Method and Description |
---|---|
static FlangeBuilder.WidthTypeOptions |
valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static FlangeBuilder.WidthTypeOptions |
valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static FlangeBuilder.WidthTypeOptions[] |
values()
Returns an array that contains the values for this enum.
|
public static final FlangeBuilder.WidthTypeOptions FULL_EDGE
public static final FlangeBuilder.WidthTypeOptions CENTER_OF_EDGE
public static final FlangeBuilder.WidthTypeOptions AT_EDGE_END
public static final FlangeBuilder.WidthTypeOptions FROM_EDGE_END
public static final FlangeBuilder.WidthTypeOptions FROM_BOTH_ENDS
public static final FlangeBuilder.WidthTypeOptions CUSTOM
public static final int _FULL_EDGE
public static final int _CENTER_OF_EDGE
public static final int _AT_EDGE_END
public static final int _FROM_EDGE_END
public static final int _FROM_BOTH_ENDS
public static final int _CUSTOM
public static FlangeBuilder.WidthTypeOptions valueOf(int value)
public static FlangeBuilder.WidthTypeOptions valueOf(String name)
public static FlangeBuilder.WidthTypeOptions[] values()
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.