Package | Description |
---|---|
nxopen.features.sheetmetal |
Provides classes and interfaces for Sheet Metal Features.
|
Modifier and Type | Field and Description |
---|---|
static BridgeTransitionBuilder.WidthDirectionOptions |
BridgeTransitionBuilder.WidthDirectionOptions.LEFT
It means Bridge Transition width direction at point specified and fin direction are in opposite direction.
|
static BridgeTransitionBuilder.WidthDirectionOptions |
BridgeTransitionBuilder.WidthDirectionOptions.RIGHT
It means Bridge Transition width direction at point specified and fin direction are in same direction.
|
Modifier and Type | Method and Description |
---|---|
static BridgeTransitionBuilder.WidthDirectionOptions |
BridgeTransitionBuilder.WidthDirectionOptions.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static BridgeTransitionBuilder.WidthDirectionOptions |
BridgeTransitionBuilder.WidthDirectionOptions.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static BridgeTransitionBuilder.WidthDirectionOptions[] |
BridgeTransitionBuilder.WidthDirectionOptions.values()
Returns an array that contains the values for this enum.
|
BridgeTransitionBuilder.WidthDirectionOptions |
BridgeTransitionBuilder.widthDirection()
Returns the width direction.
|
Modifier and Type | Method and Description |
---|---|
void |
BridgeTransitionBuilder.setWidthDirection(BridgeTransitionBuilder.WidthDirectionOptions widthDirection)
License requirements: nx_flexible_pcb ("NX Flexible PCB") OR adv_sheet_metal_dsgn ("ADVANCED SHEET METAL DESIGN") . |
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.