public static class BridgeTransitionBuilder.WidthDirectionOptions extends Enum
Features.SheetMetal.BridgeTransitionBuilder.WidthOptions#FINITE
.
The Features.SheetMetal.BridgeTransitionBuilder.WidthDirectionOptions#RIGHT
option indicates that
the width is in the counter clockwise direction of flow of the start edge in the
non-thickness face adjacent to it. The Features.SheetMetal.BridgeTransitionBuilder.WidthDirectionOptions#LEFT
option indicates the width is in the opposite direction.Modifier and Type | Field and Description |
---|---|
static int |
_LEFT
It means Bridge Transition width direction at point specified and fin direction are in opposite direction.
|
static int |
_RIGHT
It means Bridge Transition width direction at point specified and fin direction are in same direction.
|
static BridgeTransitionBuilder.WidthDirectionOptions |
LEFT
It means Bridge Transition width direction at point specified and fin direction are in opposite direction.
|
static BridgeTransitionBuilder.WidthDirectionOptions |
RIGHT
It means Bridge Transition width direction at point specified and fin direction are in same direction.
|
Modifier and Type | Method and Description |
---|---|
static BridgeTransitionBuilder.WidthDirectionOptions |
valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static BridgeTransitionBuilder.WidthDirectionOptions |
valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static BridgeTransitionBuilder.WidthDirectionOptions[] |
values()
Returns an array that contains the values for this enum.
|
public static final BridgeTransitionBuilder.WidthDirectionOptions LEFT
public static final BridgeTransitionBuilder.WidthDirectionOptions RIGHT
public static final int _LEFT
public static final int _RIGHT
public static BridgeTransitionBuilder.WidthDirectionOptions valueOf(int value)
public static BridgeTransitionBuilder.WidthDirectionOptions valueOf(String name)
public static BridgeTransitionBuilder.WidthDirectionOptions[] values()
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.