Package | Description |
---|---|
nxopen.features.sheetmetal |
Provides classes and interfaces for Sheet Metal Features.
|
Modifier and Type | Field and Description |
---|---|
static AeroFlangeBuilder.EndType |
AeroFlangeBuilder.EndType.CLOSED
Periodic Bend Edge
|
static AeroFlangeBuilder.EndType |
AeroFlangeBuilder.EndType.END1
Start of section
|
static AeroFlangeBuilder.EndType |
AeroFlangeBuilder.EndType.END2
End of section
|
Modifier and Type | Method and Description |
---|---|
static AeroFlangeBuilder.EndType |
AeroFlangeBuilder.EndType.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static AeroFlangeBuilder.EndType |
AeroFlangeBuilder.EndType.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static AeroFlangeBuilder.EndType[] |
AeroFlangeBuilder.EndType.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
AeroFlangeBuilder.EndCompensationData |
AeroFlangeBuilder.getEndCompensation(AeroFlangeBuilder.EndType endType)
Get end compensation.
|
Plane |
AeroFlangeBuilder.getEndPlane(AeroFlangeBuilder.EndType endType)
Get the end plane
License requirements: aero_sheet_metal ("Aerospace Sheet Metal") OR adv_sheet_metal_dsgn ("ADVANCED SHEET METAL DESIGN") . |
void |
AeroFlangeBuilder.setEndCompensation(AeroFlangeBuilder.EndType endType,
AeroFlangeBuilder.CompType compType,
String valueExpression)
Set end compensation.
|
void |
AeroFlangeBuilder.setEndPlane(AeroFlangeBuilder.EndType endType,
Plane endPlane)
Set the end plane
License requirements: aero_sheet_metal ("Aerospace Sheet Metal") OR adv_sheet_metal_dsgn ("ADVANCED SHEET METAL DESIGN") . |
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.