public static class AeroFlangeBuilder.EndType extends Enum
Modifier and Type | Field and Description |
---|---|
static int |
_CLOSED
Periodic Bend Edge
|
static int |
_END1
Start of section
|
static int |
_END2
End of section
|
static AeroFlangeBuilder.EndType |
CLOSED
Periodic Bend Edge
|
static AeroFlangeBuilder.EndType |
END1
Start of section
|
static AeroFlangeBuilder.EndType |
END2
End of section
|
Modifier and Type | Method and Description |
---|---|
static AeroFlangeBuilder.EndType |
valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static AeroFlangeBuilder.EndType |
valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static AeroFlangeBuilder.EndType[] |
values()
Returns an array that contains the values for this enum.
|
public static final AeroFlangeBuilder.EndType END1
public static final AeroFlangeBuilder.EndType END2
public static final AeroFlangeBuilder.EndType CLOSED
public static final int _END1
public static final int _END2
public static final int _CLOSED
public static AeroFlangeBuilder.EndType valueOf(int value)
public static AeroFlangeBuilder.EndType valueOf(String name)
public static AeroFlangeBuilder.EndType[] values()
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.