Package | Description |
---|---|
nxopen.die |
Provides classes and interfaces relating to Die Engineering and Die Design.
|
Modifier and Type | Field and Description |
---|---|
static MachineReliefBuilder.Types |
MachineReliefBuilder.Types.CAM
Add casting material for the trim, or flange, steel mating surface.
|
static MachineReliefBuilder.Types |
MachineReliefBuilder.Types.RELIEF
Remove casting material to allow for clearance between two mating objects (such as the upper and lower castings).
|
static MachineReliefBuilder.Types |
MachineReliefBuilder.Types.THICKEN
Add casting material to thicken an existing wall.
|
Modifier and Type | Method and Description |
---|---|
MachineReliefBuilder.Types |
MachineReliefBuilder.type()
Returns the value defining the type of build to perform for this tool.
|
static MachineReliefBuilder.Types |
MachineReliefBuilder.Types.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static MachineReliefBuilder.Types |
MachineReliefBuilder.Types.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static MachineReliefBuilder.Types[] |
MachineReliefBuilder.Types.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
MachineReliefBuilder.setType(MachineReliefBuilder.Types type)
License requirements: ug_die_design ("Die Design") . |
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.