public static class MachineReliefBuilder.Types extends Enum
Modifier and Type | Field and Description |
---|---|
static int |
_CAM
Add casting material for the trim, or flange, steel mating surface.
|
static int |
_RELIEF
Remove casting material to allow for clearance between two mating objects (such as the upper and lower castings).
|
static int |
_THICKEN
Add casting material to thicken an existing wall.
|
static MachineReliefBuilder.Types |
CAM
Add casting material for the trim, or flange, steel mating surface.
|
static MachineReliefBuilder.Types |
RELIEF
Remove casting material to allow for clearance between two mating objects (such as the upper and lower castings).
|
static MachineReliefBuilder.Types |
THICKEN
Add casting material to thicken an existing wall.
|
Modifier and Type | Method and Description |
---|---|
static MachineReliefBuilder.Types |
valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static MachineReliefBuilder.Types |
valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static MachineReliefBuilder.Types[] |
values()
Returns an array that contains the values for this enum.
|
public static final MachineReliefBuilder.Types CAM
public static final MachineReliefBuilder.Types RELIEF
public static final MachineReliefBuilder.Types THICKEN
public static final int _CAM
public static final int _RELIEF
public static final int _THICKEN
public static MachineReliefBuilder.Types valueOf(int value)
public static MachineReliefBuilder.Types valueOf(String name)
public static MachineReliefBuilder.Types[] values()
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.