Package | Description |
---|---|
nxopen.die |
Provides classes and interfaces relating to Die Engineering and Die Design.
|
Modifier and Type | Field and Description |
---|---|
static FillAreaBuilder.Types |
FillAreaBuilder.Types.BASE_FLANGE
Fill area is in the base flange area.
|
static FillAreaBuilder.Types |
FillAreaBuilder.Types.PRODUCT_CONTACT
Fill area is in the upper deck where relief for the product has been added.
|
static FillAreaBuilder.Types |
FillAreaBuilder.Types.SCRAP_AREA
Remove the volume instead of filling.
|
static FillAreaBuilder.Types |
FillAreaBuilder.Types.USER_DEFINED
The user must defined all the constraints for the area (inputs from the target are ignored).
|
Modifier and Type | Method and Description |
---|---|
FillAreaBuilder.Types |
FillAreaBuilder.type()
Returns the indicator for the type of fill area to build.
|
static FillAreaBuilder.Types |
FillAreaBuilder.Types.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static FillAreaBuilder.Types |
FillAreaBuilder.Types.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static FillAreaBuilder.Types[] |
FillAreaBuilder.Types.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
FillAreaBuilder.setType(FillAreaBuilder.Types type)
License requirements: ug_die_design ("Die Design") . |
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.