public static class FillAreaBuilder.Types extends Enum
Modifier and Type | Field and Description |
---|---|
static int |
_BASE_FLANGE
Fill area is in the base flange area.
|
static int |
_PRODUCT_CONTACT
Fill area is in the upper deck where relief for the product has been added.
|
static int |
_SCRAP_AREA
Remove the volume instead of filling.
|
static int |
_USER_DEFINED
The user must defined all the constraints for the area (inputs from the target are ignored).
|
static FillAreaBuilder.Types |
BASE_FLANGE
Fill area is in the base flange area.
|
static FillAreaBuilder.Types |
PRODUCT_CONTACT
Fill area is in the upper deck where relief for the product has been added.
|
static FillAreaBuilder.Types |
SCRAP_AREA
Remove the volume instead of filling.
|
static FillAreaBuilder.Types |
USER_DEFINED
The user must defined all the constraints for the area (inputs from the target are ignored).
|
Modifier and Type | Method and Description |
---|---|
static FillAreaBuilder.Types |
valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static FillAreaBuilder.Types |
valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static FillAreaBuilder.Types[] |
values()
Returns an array that contains the values for this enum.
|
public static final FillAreaBuilder.Types BASE_FLANGE
public static final FillAreaBuilder.Types PRODUCT_CONTACT
public static final FillAreaBuilder.Types SCRAP_AREA
public static final FillAreaBuilder.Types USER_DEFINED
public static final int _BASE_FLANGE
public static final int _PRODUCT_CONTACT
public static final int _SCRAP_AREA
public static final int _USER_DEFINED
public static FillAreaBuilder.Types valueOf(int value)
public static FillAreaBuilder.Types valueOf(String name)
public static FillAreaBuilder.Types[] values()
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.