Package | Description |
---|---|
nxopen.die |
Provides classes and interfaces relating to Die Engineering and Die Design.
|
Modifier and Type | Field and Description |
---|---|
static DrawBeadBuilder.MaleBeadPositionTypes |
DrawBeadBuilder.MaleBeadPositionTypes.LOWER
Attach the male bead to the lower die casting.
|
static DrawBeadBuilder.MaleBeadPositionTypes |
DrawBeadBuilder.MaleBeadPositionTypes.UPPER
Attach the male bead to the upper die casting.
|
Modifier and Type | Method and Description |
---|---|
DrawBeadBuilder.MaleBeadPositionTypes |
DrawBeadBuilder.maleBeadPosition()
Returns the casting in which to create the male bead.
|
static DrawBeadBuilder.MaleBeadPositionTypes |
DrawBeadBuilder.MaleBeadPositionTypes.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static DrawBeadBuilder.MaleBeadPositionTypes |
DrawBeadBuilder.MaleBeadPositionTypes.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static DrawBeadBuilder.MaleBeadPositionTypes[] |
DrawBeadBuilder.MaleBeadPositionTypes.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
DrawBeadBuilder.setMaleBeadPosition(DrawBeadBuilder.MaleBeadPositionTypes maleBeadPosition)
License requirements: die_engineering ("DIE ENGINEERING") OR prog_die_wizard ("UG/Progressive Die Wizard") . |
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.