public static class DrawBeadBuilder.MaleBeadPositionTypes extends Enum
Modifier and Type | Field and Description |
---|---|
static int |
_LOWER
Attach the male bead to the lower die casting.
|
static int |
_UPPER
Attach the male bead to the upper die casting.
|
static DrawBeadBuilder.MaleBeadPositionTypes |
LOWER
Attach the male bead to the lower die casting.
|
static DrawBeadBuilder.MaleBeadPositionTypes |
UPPER
Attach the male bead to the upper die casting.
|
Modifier and Type | Method and Description |
---|---|
static DrawBeadBuilder.MaleBeadPositionTypes |
valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static DrawBeadBuilder.MaleBeadPositionTypes |
valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static DrawBeadBuilder.MaleBeadPositionTypes[] |
values()
Returns an array that contains the values for this enum.
|
public static final DrawBeadBuilder.MaleBeadPositionTypes UPPER
public static final DrawBeadBuilder.MaleBeadPositionTypes LOWER
public static final int _UPPER
public static final int _LOWER
public static DrawBeadBuilder.MaleBeadPositionTypes valueOf(int value)
public static DrawBeadBuilder.MaleBeadPositionTypes valueOf(String name)
public static DrawBeadBuilder.MaleBeadPositionTypes[] values()
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.