Package | Description |
---|---|
nxopen.die |
Provides classes and interfaces relating to Die Engineering and Die Design.
|
Modifier and Type | Field and Description |
---|---|
static DrawBeadBuilder.FemaleDepthTypes |
DrawBeadBuilder.FemaleDepthTypes.CONSTANT
The female depth is a user specified constant.
|
static DrawBeadBuilder.FemaleDepthTypes |
DrawBeadBuilder.FemaleDepthTypes.DERIVED
The female depth is derived from the male bead (Max Male Depth + Constant).
|
Modifier and Type | Method and Description |
---|---|
DrawBeadBuilder.FemaleDepthTypes |
DrawBeadBuilder.femaleDepthType()
Returns the method used to calculate the female depth.
|
static DrawBeadBuilder.FemaleDepthTypes |
DrawBeadBuilder.FemaleDepthTypes.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static DrawBeadBuilder.FemaleDepthTypes |
DrawBeadBuilder.FemaleDepthTypes.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static DrawBeadBuilder.FemaleDepthTypes[] |
DrawBeadBuilder.FemaleDepthTypes.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
DrawBeadBuilder.setFemaleDepthType(DrawBeadBuilder.FemaleDepthTypes femaleDepthType)
License requirements: die_engineering ("DIE ENGINEERING") OR prog_die_wizard ("UG/Progressive Die Wizard") . |
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.