public static class DrawBeadBuilder.FemaleDepthTypes extends Enum
Modifier and Type | Field and Description |
---|---|
static int |
_CONSTANT
The female depth is a user specified constant.
|
static int |
_DERIVED
The female depth is derived from the male bead (Max Male Depth + Constant).
|
static DrawBeadBuilder.FemaleDepthTypes |
CONSTANT
The female depth is a user specified constant.
|
static DrawBeadBuilder.FemaleDepthTypes |
DERIVED
The female depth is derived from the male bead (Max Male Depth + Constant).
|
Modifier and Type | Method and Description |
---|---|
static DrawBeadBuilder.FemaleDepthTypes |
valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static DrawBeadBuilder.FemaleDepthTypes |
valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static DrawBeadBuilder.FemaleDepthTypes[] |
values()
Returns an array that contains the values for this enum.
|
public static final DrawBeadBuilder.FemaleDepthTypes DERIVED
public static final DrawBeadBuilder.FemaleDepthTypes CONSTANT
public static final int _DERIVED
public static final int _CONSTANT
public static DrawBeadBuilder.FemaleDepthTypes valueOf(int value)
public static DrawBeadBuilder.FemaleDepthTypes valueOf(String name)
public static DrawBeadBuilder.FemaleDepthTypes[] values()
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.