Package | Description |
---|---|
nxopen.cae |
Provides classes and interfaces relating to Advanced Simulation and Design Simulation.
|
nxopen.cam |
Provides classes and interfaces for Manufacturing.
|
nxopen.drafting |
Provides classes and interfaces for the Drafting.
|
nxopen.drawings |
Provides classes and interfaces for Drafting Drawings.
|
nxopen.features |
Provides classes and interfaces for features.
|
nxopen.features.shipdesign |
Provides classes and interfaces for Ship Design.
|
nxopen.motion |
Provides classes and interfaces for Motion Simulation.
|
Modifier and Type | Method and Description |
---|---|
SelectTaggedObject |
NodeProjectBuilder.geometry()
Returns the geometry on which projection will happen
License requirements: None. |
Modifier and Type | Method and Description |
---|---|
SelectTaggedObject |
HoleBossGeom.selection()
Returns the selection geometry
License requirements: None. |
Modifier and Type | Method and Description |
---|---|
SelectTaggedObject |
CutCopyPasteLeaderBuilder.leaderSelection()
Returns the selection to reassociate single leader
License requirements: None. |
SelectTaggedObject |
CutCopyPasteLeaderBuilder.selection()
Returns the selection to reassociate leader
License requirements: None. |
Modifier and Type | Method and Description |
---|---|
SelectTaggedObject |
ViewPlacementBuilder.alignmentPoint()
Returns the point to align to.
|
SelectTaggedObject |
ViewPlacementBuilder.candidatePoint()
Returns the point to align in the view being edited.
|
SelectTaggedObject |
SectionLineStyleBuilder.selectLetter()
Deprecated.
Deprecated in NX10.0.0. Use
ViewSectionLineBuilder.selectRotationLetter() instead.
|
SelectTaggedObject |
ViewSectionLineBuilder.selectRotationLetter()
Returns the selected objected should be note type only which is the desired location of the rotation point of the section line specified
License requirements: None. |
Modifier and Type | Method and Description |
---|---|
SelectTaggedObject |
PartGeometryCopySelectBuilder.bodyObject()
Returns the body group
License requirements: None. |
SelectTaggedObject |
PartGeometryCopySelectBuilder.datum()
Returns the datum
License requirements: None. |
SelectTaggedObject |
RefitFaceBuilder.face()
Returns the refitting face
License requirements: None. |
SelectTaggedObject |
PatternFaceBuilder.plane()
Returns the mirror plane of mirror pattern, don't use it until nx502
License requirements: None. |
SelectTaggedObject |
SnipSurfaceBuilder.snippingObject()
Returns the snipping object
License requirements: solid_modeling ("SOLIDS MODELING") OR studio_free_form ("STUDIO FREE FORM") . |
SelectTaggedObject |
PaintParametersBuilder.sourceObject()
Returns the source paintable object
License requirements: None. |
Modifier and Type | Method and Description |
---|---|
SelectTaggedObject |
PillarBuilder.adoptionBody()
Returns the adoption body (only used with "JA_PILLAR_BUILDER_CreationMethod_AdoptionBody" creation method).
|
SelectTaggedObject |
WeldCut2Builder.guideCurve()
Returns the guide curve to position the weld cut.
|
SelectTaggedObject |
PillarBuilder.guideCurve()
Returns the select guide curve (only used with "JA_PILLAR_BUILDER_CreationMethod_SpecifyLine" creation method).
|
SelectTaggedObject |
PillarBuilder.line1()
Returns the first line (only used with "JA_PILLAR_BUILDER_CreationMethod_TwoPlanesandLines" creation method).
|
SelectTaggedObject |
PillarBuilder.line2()
Returns the second line (only used with "JA_PILLAR_BUILDER_CreationMethod_TwoPlanesandLines" creation method).
|
SelectTaggedObject |
PillarSystemBuilder.orientationLine()
Returns the orientation line, used only if the creation method is "Specify Line".
|
SelectTaggedObject |
PillarBuilder.orientationLine()
Returns the orientation line (only used with "JA_PILLAR_BUILDER_CreationMethod_SpecifyLine" creation method).
|
SelectTaggedObject |
CornerCutListItemBuilder.seamCurve()
Returns the seam curve to resize the corner cut.
|
SelectTaggedObject |
SeamBlockBuilder.seamSelection()
Returns the seam selection
License requirements: None. |
SelectTaggedObject |
ShipEndCutBuilder.selectCSYSFace()
Returns the select csysface
License requirements: None. |
SelectTaggedObject |
ShipEndCutBuilder.selectEdge()
Returns the select edge
License requirements: None. |
SelectTaggedObject |
VentilationHoles2Builder.selectEndTrim()
Returns the select end trim
License requirements: None. |
SelectTaggedObject |
SteelVentHolesBuilder.selectEndTrim()
Returns the select end trim - used to trim the end of the section guide.
|
SelectTaggedObject |
WeldCutBuilder.selectGuideCurve()
Returns the selection object for the guide curve.
|
SelectTaggedObject |
VentilationHoles2Builder.selectStartTrim()
Returns the select start trim
License requirements: None. |
SelectTaggedObject |
SteelVentHolesBuilder.selectStartTrim()
Returns the select start trim - used to trim the start of the section guide.
|
SelectTaggedObject |
ShipEndCutBuilder.selectTargetFace()
Returns the select target face
License requirements: None. |
Modifier and Type | Method and Description |
---|---|
SelectTaggedObject |
JointDriverBuilder.joint()
Returns the joint
License requirements: None. |
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.