Package | Description |
---|---|
nxopen |
Provides classes and interfaces for the NX Open Common API.
|
nxopen.die |
Provides classes and interfaces relating to Die Engineering and Die Design.
|
nxopen.features |
Provides classes and interfaces for features.
|
nxopen.features.sheetmetal |
Provides classes and interfaces for Sheet Metal Features.
|
Modifier and Type | Interface and Description |
---|---|
interface |
DatumPlane
Represents a datum plane
This object can not be created by KF it's the display objet of the datum plane . |
interface |
Face
Represents a face .
|
interface |
Plane
Represents an
Plane class. |
Modifier and Type | Field and Description |
---|---|
ISurface |
SelectISurface.ValueData.selection
selected object
|
ISurface |
SelectISurface.ValueWithCaeSetObjectInfoData.selection
selected object
|
ISurface |
SelectISurface.ValueWithSnapData.selection1
first selected object
|
ISurface |
SelectISurface.ValueWithSnapData.selection2
second selected object
|
Modifier and Type | Method and Description |
---|---|
ISurface |
Sketch.attachPlane()
Returns the plane that the sketch is attached to
License requirements: None. |
ISurface |
SelectISurface.value()
Returns the object being selected
License requirements: None. |
Modifier and Type | Method and Description |
---|---|
Sketch |
SketchCollection.createSketch(String name,
ISurface attachmentPlane,
IReferenceAxis referenceAxis,
Vector3d referenceDirection,
AxisOrientation referenceAxisOrientation,
Sense referenceAxisSense,
PlaneNormalOrientation normalOrientation)
Deprecated.
Deprecated in NX7.5.3. Use
SketchInPlaceBuilder instead.
|
Sketch |
SketchCollection.createSketch(String name,
ISurface attachmentPlane,
IReferenceAxis referenceAxis,
Vector3d referenceDirection,
AxisOrientation referenceAxisOrientation,
Sense referenceAxisSense,
PlaneNormalOrientation normalOrientation,
NXObject view)
Deprecated.
Deprecated in NX7.5.3. Use
SketchInDraftingBuilder instead.
|
void |
Sketch.reattach(ISurface attachmentPlane,
IReferenceAxis referenceAxis,
Vector3d referenceDirection,
AxisOrientation referenceAxisOrientation,
Sense referenceAxisSense,
PlaneNormalOrientation normalOrientation,
Point3d localCoordinateSystemOrigin)
Reattaches a sketch.
|
void |
SelectISurface.setValue(ISurface selection)
Sets the object being selected
License requirements: None. |
void |
SelectISurface.setValue(ISurface selection,
View view,
Point3d point)
The object being selected with the object's view and object's point
License requirements: None. |
void |
SelectISurface.setValueWithCaeSetObjectInfo(ISurface selection,
CaeObjectType.CaeSubType caeSubType,
int caeSubId)
Deprecated.
Deprecated in NX10.0.0. Use other versions of
SelectObject.setValue(nxopen.TaggedObject) .
|
void |
SelectISurface.setValueWithSnap(InferSnapType.SnapType snapType,
ISurface selection1,
View view1,
Point3d point1,
ISurface selection2,
View view2,
Point3d point2)
The object being selected with the objects view and objects point and snap information.
|
Modifier and Type | Field and Description |
---|---|
ISurface |
TrimTaskBuilder.CheckAndMovePlanesData.targetendplanetag
End plane in target operation.
|
ISurface |
TrimTaskBuilder.CheckAndMovePlanesData.targetstartplanetag
Start plane in target operation.
|
Modifier and Type | Method and Description |
---|---|
ISurface |
SteelInsertBuilder.baseOrientation()
Returns the base orientation of the steelinsert
License requirements: ug_die_design ("Die Design") . |
ISurface |
DrawDiePunchBuilder.baseOrientation()
Returns the base orientation of the draw die punch casting.
|
ISurface |
HandlingCoreChildBuilder.coreOrientation()
Returns the core orientation of the handling core.
|
ISurface |
SteelInsertBuilder.endOrientation()
Returns the end orientation of the steelinsert
License requirements: ug_die_design ("Die Design") . |
ISurface |
TrimTaskBuilder.endPlane()
Returns the end plane of the trim task
License requirements: die_engineering ("DIE ENGINEERING") . |
ISurface[] |
SteelInsertBuilder.getBackShape()
Gets the back shape of the die steelinsert
License requirements: ug_die_design ("Die Design") . |
ISurface[] |
RotorBuilder.getEndOrientation()
Gets the end orientation of the rotor casting.
|
ISurface[] |
TrimTaskBuilder.getScrapCutters()
Gets the scrap cutters of the trim task
License requirements: die_engineering ("DIE ENGINEERING") . |
ISurface[] |
RotorBuilder.getStartOrientation()
Gets the start orientation of the rotor casting.
|
ISurface |
DeckParentBuilder.intermediateDeckOrientation()
Returns the intermediate deck orientation of the deck.
|
ISurface |
FillBuilder.mirrorPlane()
Returns the plane to mirror the area fill about
License requirements: die_engineering ("DIE ENGINEERING") . |
ISurface |
WearPlateLocChildBuilder.orientation()
Returns the orientation plane of die wear plate and locators
License requirements: ug_die_design ("Die Design") . |
ISurface |
HoleChildBuilder.plane()
Returns the plane of the die hole.
|
ISurface |
FlangeSteelRibChildBuilder.plane()
Returns the plane of the Flange Steel Rib
License requirements: ug_die_design ("Die Design") . |
ISurface |
SteelInsertBuilder.startOrientation()
Returns the start orientation of the steelinsert
License requirements: ug_die_design ("Die Design") . |
ISurface |
TrimTaskBuilder.startPlane()
Returns the start plane of the trim task
License requirements: die_engineering ("DIE ENGINEERING") . |
Modifier and Type | Method and Description |
---|---|
TrimTaskBuilder.CheckAndMovePlanesData |
TrimTaskBuilder.checkAndMovePlanes(nxopen.features.Feature origTip,
nxopen.features.Feature targetTip,
ISurface origStartPlaneTag,
ISurface origEndPlaneTag)
Move end planes if the position of Trim Task is changed.
|
void |
SteelInsertBuilder.setBackShape(ISurface[] backEntries)
License requirements: ug_die_design ("Die Design") . |
void |
SteelInsertBuilder.setBaseOrientation(ISurface baseOrientation)
Sets the base orientation of the steelinsert
License requirements: ug_die_design ("Die Design") . |
void |
DrawDiePunchBuilder.setBaseOrientation(ISurface baseOrientation)
Sets the base orientation of the draw die punch casting.
|
void |
HandlingCoreChildBuilder.setCoreOrientation(ISurface coreOrientation)
Sets the core orientation of the handling core.
|
void |
SteelInsertBuilder.setEndOrientation(ISurface endOrientation)
Sets the end orientation of the steelinsert
License requirements: ug_die_design ("Die Design") . |
void |
RotorBuilder.setEndOrientation(ISurface[] endEntries)
Sets the end orientation of the rotor casting.
|
void |
TrimTaskBuilder.setEndPlane(ISurface endPlane)
Sets the end plane of the trim task
License requirements: die_engineering ("DIE ENGINEERING") . |
void |
DeckParentBuilder.setIntermediateDeckOrientation(ISurface intermediateDeckOrientation)
Sets the intermediate deck orientation of the deck.
|
void |
FillBuilder.setMirrorPlane(ISurface mirrorPlane)
Sets the plane to mirror the area fill about
License requirements: die_engineering ("DIE ENGINEERING") . |
void |
WearPlateLocChildBuilder.setOrientation(ISurface orientation)
Sets the orientation plane of die wear plate and locators
License requirements: ug_die_design ("Die Design") . |
void |
HoleChildBuilder.setPlane(ISurface plane)
Sets the plane of the die hole.
|
void |
FlangeSteelRibChildBuilder.setPlane(ISurface plane)
Sets the plane of the Flange Steel Rib
License requirements: ug_die_design ("Die Design") . |
void |
TrimTaskBuilder.setScrapCutters(ISurface[] planes)
Sets the scrap cutters of the trim task
License requirements: die_engineering ("DIE ENGINEERING") . |
void |
SteelInsertBuilder.setStartOrientation(ISurface startOrientation)
Sets the start orientation of the steelinsert
License requirements: ug_die_design ("Die Design") . |
void |
RotorBuilder.setStartOrientation(ISurface[] startEntries)
Sets the start orientation of the rotor casting.
|
void |
TrimTaskBuilder.setStartPlane(ISurface startPlane)
Sets the start plane of the trim task
License requirements: die_engineering ("DIE ENGINEERING") . |
Modifier and Type | Method and Description |
---|---|
ISurface |
SectionCurveBuilder.basePlane()
Returns the base plane
License requirements: None. |
ISurface |
EmbossTarget.endcapPlane()
Returns the plane to produce End-Cap
License requirements: None. |
ISurface |
Hole.placementFace()
Returns
the placement face of the hole.
|
ISurface |
SectionEditBuilder.plane()
Returns the sectioning plane for cutting section on a body
License requirements: None. |
ISurface |
EmbossProjection.plane()
Returns the projection plane
License requirements: None. |
ISurface |
FaceBlendBuilder.tangentSurface()
Returns the tangency object for face blend.
|
ISurface |
Hole.thruFace()
Returns
the thru face of the hole.
|
Modifier and Type | Method and Description |
---|---|
void |
SectionCurveBuilder.setBasePlane(ISurface basePlane)
License requirements: solid_modeling ("SOLIDS MODELING") . |
void |
EmbossTarget.setEndcapPlane(ISurface endcapPlane)
Sets the plane to produce End-Cap
License requirements: solid_modeling ("SOLIDS MODELING") . |
void |
SectionEditBuilder.setPlane(ISurface plane)
License requirements: solid_modeling ("SOLIDS MODELING") . |
void |
EmbossProjection.setPlane(ISurface projectionPlane)
Sets the projection plane
License requirements: solid_modeling ("SOLIDS MODELING") . |
void |
FaceBlendBuilder.setTangentSurface(ISurface object)
License requirements: solid_modeling ("SOLIDS MODELING") . |
Modifier and Type | Method and Description |
---|---|
ISurface |
NormalCutoutBuilder.from()
Returns the face or datum plane from which the cutout begins.
|
ISurface |
NormalCutoutBuilder.to()
Returns the face or datum plane at which the cutout ends.
|
Modifier and Type | Method and Description |
---|---|
void |
NormalCutoutBuilder.setFrom(ISurface ffrom)
Sets the face or datum plane from which the cutout begins.
|
void |
NormalCutoutBuilder.setTo(ISurface to)
Sets the face or datum plane at which the cutout ends.
|
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.