public static class TBSObjectives.ObjectiveType extends Enum
Modifier and Type | Field and Description |
---|---|
static int |
_MAX_MIN
Target is the MINMAX formulation of the list of design responses
|
static int |
_MAXIMUM
Target is to maximize the list of design response
|
static int |
_MINIMUM
Target is to minimize the list of design response
|
static TBSObjectives.ObjectiveType |
MAX_MIN
Target is the MINMAX formulation of the list of design responses
|
static TBSObjectives.ObjectiveType |
MAXIMUM
Target is to maximize the list of design response
|
static TBSObjectives.ObjectiveType |
MINIMUM
Target is to minimize the list of design response
|
Modifier and Type | Method and Description |
---|---|
static TBSObjectives.ObjectiveType |
valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static TBSObjectives.ObjectiveType |
valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static TBSObjectives.ObjectiveType[] |
values()
Returns an array that contains the values for this enum.
|
public static final TBSObjectives.ObjectiveType MINIMUM
public static final TBSObjectives.ObjectiveType MAXIMUM
public static final TBSObjectives.ObjectiveType MAX_MIN
public static final int _MINIMUM
public static final int _MAXIMUM
public static final int _MAX_MIN
public static TBSObjectives.ObjectiveType valueOf(int value)
public static TBSObjectives.ObjectiveType valueOf(String name)
public static TBSObjectives.ObjectiveType[] values()
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.