See: Description
Interface | Description |
---|---|
DAOConstraint |
Represents a
DAOConstraint . |
DAOConstraintBuilder |
Represents a
DAOConstraintBuilder . |
DAOConstraintCollection |
Represents the collection of optimization solution design constraint
To obtain an instance of this class, refer to DAOSolution Created in NX8.0.0 |
DAODesignVariable |
Represents a
DAODesignVariable . |
DAODesignVariableBuilder |
Represents a
DAODesignVariableBuilder . |
DAODesignVariableCollection |
Represents the collection of optimization solution design variable
To obtain an instance of this class, refer to DAOSolution Created in NX8.0.0 |
DAOObjective |
Represents a
DAOObjective . |
DAOOptimizationManager |
Represents the Design and Analysis optimization manager that contains all optimization objects.
|
DAOSolution |
Represents a
DAOSolution . |
DAOSolutionBuilder |
Represents a
DAOSolutionBuilder . |
DAOSolutionCollection |
Represents the collection of optimization solution
To obtain an instance of this class, refer to DAOOptimizationManager Created in NX8.0.0 |
DAOStopCondition |
Represents a
DAOStopCondition . |
NameDescription |
.
|
TBSBaseDesignVariableBuilder |
Represents the builder of
TBSDesignVariable This is an abstract class, and cannot be created. |
TBSCastCondition | |
TBSCheckDOF |
Represents the restriction of dispacement in the coordinate direction of the referenced coordinate system .
|
TBSConstraint |
Represents the design constraint, which is defined with
TBSDesignVariable To create or edit an instance of this class, use TBSConstraintBuilder Created in NX8.0.0 |
TBSConstraintBuilder |
Represents the builder of
TBSConstraint To create a new instance of this class, use TBSOptimizationManager.createResponseConstraintBuilder(nxopen.cae.optimization.TBSConstraint) Created in NX8.0.0 |
TBSConstraintCollection |
Represents a collection of
TBSConstraint To obtain an instance of this class, refer to TBSOptimizationSolution Created in NX8.0.0 |
TBSDesignArea |
Represents the design area .
|
TBSDesignResponse |
Represents the design response referenced by
TBSConstraint and
TBSObjectives To create or edit an instance of this class, use TBSDesignResponseBuilder Created in NX8.0.0 |
TBSDesignResponseBuilder |
Represents the builder of
TBSDesignResponse To create a new instance of this class, use TBSOptimizationManager.createDesignResponseBuilder(nxopen.cae.optimization.TBSDesignResponse) Created in NX8.0.0 |
TBSDesignVariable |
Represents the design variable referenced by
TBSConstraint and
TBSObjectives To create or edit an instance of this class, use TBSDesignVariableBuilder Created in NX8.0.0 |
TBSDesignVariableBuilder |
Represents the builder of
TBSDesignVariable To create a new instance of this class, use TBSOptimizationManager.createDesignVariableBuilder(nxopen.cae.optimization.TBSDesignVariable) Created in NX8.0.0 |
TBSDesignVariableCollection |
Represents a collection of
CAE.Optimization.TBSDesignVariable To obtain an instance of this class, refer to TBSOptimizationSolution Created in NX8.0.0 |
TBSEigenvalueOptimizationParameters |
Represents the parameters to control an eigenvalue optimization .
|
TBSGroupDefinition |
Represents a group of nodes or elements .
|
TBSIOptimizationTest |
Represents an interface to perform optimization test .
|
TBSLoadCase |
Represents the load case
To create a new instance of this class, use TBSOptimizationManager.createLoadCase() Created in NX8.0.0 |
TBSLoadCaseManager |
Managers load cases .
|
TBSMeshSmooth |
Represents the mesh smooth .
|
TBSObjectives |
Represents the objective functions of an optimization .
|
TBSOptimizationManager |
Represents the optimization manager to contain the optimization solutions and take charge of
creating optimization objects
To obtain an instance of this class, refer to SimSimulation Created in NX8.0.0 |
TBSOptimizationParameters |
Represents the parameters to control an optimization
This is an abstract class, and cannot be created. |
TBSOptimizationSolution |
Represents the solution to contain optimization setting
This is an abstract class, and cannot be created. |
TBSOptimizationSolutionBuilder |
Represents the abstract builder of
TBSOptimizationSolution . |
TBSOptimizationSolutionCollection |
Represents a collection of
TBSOptimizationSolution To obtain an instance of this class, refer to TBSOptimizationManager Created in NX8.0.0 |
TBSOutputControlOptions |
Represents the output result control options of the optimization .
|
TBSRestrictArea |
Represents the restrictions for the design variable in an optimization
To create or edit an instance of this class, use TBSRestrictAreaBuilder Created in NX8.0.0 |
TBSRestrictAreaBuilder |
Represents the builder of
TBSRestrictArea This is an abstract class, and cannot be created. |
TBSRestrictAreaCollection |
Represents a collection of
TBSRestrictArea To obtain an instance of this class, refer to TBSOptimizationSolution Created in NX8.0.0 |
TBSShapeLinkCondition |
Represents the definition of link condition for shape restriction .
|
TBSShapeOptimizationParameters |
Represents the control parameters of shape optimization .
|
TBSShapeOptimizationSolution |
Represents a shape optimization solution
To create or edit an instance of this class, use TBSShapeOptimizationSolutionBuilder Created in NX8.5.0 |
TBSShapeOptimizationSolutionBuilder |
Represents the builder of
TBSShapeOptimizationSolution . |
TBSShapeRestrictArea |
Represents the restrictions of the design variable in Shape optimization
To create or edit an instance of this class, use TBSShapeRestrictAreaBuilder Created in NX8.5.0 |
TBSShapeRestrictAreaBuilder |
Represents the builder of
TBSShapeRestrictArea To create a new instance of this class, use TBSOptimizationManager.createShapeRestrictAreaBuilder(nxopen.cae.optimization.TBSShapeRestrictArea) Created in NX8.5.0 |
TBSSingleObjective |
Represents a single objective
To create a new instance of this class, use TBSOptimizationManager.createSingleObjective(nxopen.cae.optimization.TBSDesignResponse, double, double) Created in NX8.0.0 |
TBSSmooth |
Represents the parameters that control the generation of surfaces by optimization
To create or edit an instance of this class, use TBSSmoothBuilder Created in NX8.0.0 |
TBSSmoothBuilder |
Represents the builder of
TBSSmooth . |
TBSSmoothCollection |
Represents a collection of
TBSSmooth To obtain an instance of this class, refer to TBSOptimizationSolution Created in NX8.0.0 |
TBSStopCondition |
Represents the condtion to end an optimization .
|
TBSTestFunction |
Represents a test displacement for shape optimization or bead optimization .
|
TBSTopologyControllerOptimizationParameters |
Represents the parameters to control an optimization in controller strategy .
|
TBSTopologyLinkCondition |
Represents the definition of symmetry and link conditions for topology optimization .
|
TBSTopologyOptimizationSolution |
Represents the topology optimization solution
To create or edit an instance of this class, use TBSTopologyOptimizationSolutionBuilder Created in NX8.0.0 |
TBSTopologyOptimizationSolutionBuilder |
Represents the builder of
TBSTopologyOptimizationSolution . |
TBSTopologyRestrictArea |
Represents the restrictions of the design variable in topology optimization
To create or edit an instance of this class, use TBSTopologyRestrictAreaBuilder Created in NX8.0.0 |
TBSTopologyRestrictAreaBuilder |
Represents the builder of
TBSTopologyRestrictArea To create a new instance of this class, use TBSOptimizationManager.createTopologyRestrictAreaBuilder(nxopen.cae.optimization.TBSTopologyRestrictArea) Created in NX8.0.0 |
TBSTopologySensitivityOptimizationParameters |
Represents the parameters to control an optimization in sensitivity strategy .
|
Class | Description |
---|---|
Category |
Represents the category type
|
DAODesignVariableBuilder.Variable |
Represents the design variable type
|
DAODesignVariableBuilder.VariableData |
This class holds the data returned from
DAODesignVariableBuilder.getVariable() |
Geometry |
Represents the geometry type
|
Goal |
Represents the goal type
|
Hookes | Deprecated
Deprecated in NX10.0.0.
|
Limit |
Represents the limit type
|
Response |
Represents the specific variable
|
Solver |
Represents the optimization solution solver type
|
TBSBaseDesignVariableBuilder.GroupOperator |
Defines the operator type to determine the design variable that used within the selection area
|
TBSCastCondition.MiddlePlaneType |
Defines the middle plane type
|
TBSCheckDOF.CheckDofOption |
Represents the status of displacement restriction
|
TBSCheckDOF.DofSettings |
the displacement restriction settings on three axial directions of referenced coordinate system
|
TBSConstraintBuilder.ConstraintOption |
Defines the constraint type
|
TBSConstraintBuilder.MagnitudeType |
Defines the type of constraint value
|
TBSDesignResponseBuilder.Response |
Defines the design response type
|
TBSGroupDefinition.DefinitionType |
Represents the definition method of a group
|
TBSGroupDefinition.GroupElementType |
Represents the type of group elements
|
TBSLoadCase.LayerOption |
Defines the location for calcuating shell stresses
|
TBSLoadCase.SubcaseData |
This class holds the data returned from
TBSLoadCase.getSubcase() |
TBSLoadCase.SubstepData |
This class holds the data returned from
TBSLoadCase.getSubstep() |
TBSLoadCaseManager.SelectionType |
Defines the selection of the loadcase
|
TBSMeshSmooth.Strategy |
Specify the strategy of mesh smooth
|
TBSObjectives.ObjectiveType |
Defines the target type of the design objective
|
TBSOptimizationSolution.JA_CAE_OPT_SOL_get_result |
This class holds the data returned from
TBSOptimizationSolution.getPostResult(int) |
TBSOptimizationSolution.ResultStatus |
Define the status of optimization result
|
TBSOptimizationSolutionBuilder.StrategyType |
Defines the optimization strategy
|
TBSOutputControlOptions.Op2Option |
Defines the op2 output option
|
TBSShapeLinkCondition.ManufacturingOption |
Defines the type of link condition
|
TBSShapeOptimizationParameters.DisplacementStepsize |
the step size option for incrementing the displacement during the optimization operation
|
TBSSmoothBuilder.Format |
Defines the output file format of surface representation
|
TBSSmoothBuilder.IsoType |
Specifies the content saved to the output files
|
TBSSmoothBuilder.OriginalSurfaceSmoothingOption |
Defines if the original surface is to be smoothed or remain unchanged
|
TBSSmoothBuilder.ResultFiltering |
Defines if the element material values are to be filtered before the isocut
|
TBSSmoothBuilder.SelfIntersectionCheckingOption |
Defines if the self-itersection checks are to be performed during the isocut, smoothing and data reduction
|
TBSSmoothBuilder.SliceFormatOption |
Defines how to save slices
|
TBSTestFunction.Direction |
the direction of test displacements
|
TBSTopologyControllerOptimizationParameters.AutoFrozen |
Defines the automatic fromzen strategy
|
TBSTopologyControllerOptimizationParameters.Speed |
Specifies the step size of increment
|
TBSTopologyControllerOptimizationParameters.VolumeDefinitionMethod |
Represents the definition of volume that can be removed immediatedly in the first design cycle
|
TBSTopologyLinkCondition.AxisType |
Represents the axis of the symmetry coordinate system
|
TBSTopologyLinkCondition.SymmetryOption |
Defines the type of link condition
|
TBSTopologyRestrictAreaBuilder.CheckTypeOption |
Defines the type of restriction
|
TBSTopologySensitivityOptimizationParameters.DensityUpdate |
the method defines how the densities are updated in the method of moving asymptotes
|
TBSTopologySensitivityOptimizationParameters.MaterialInterpolation |
the relationshp between relative density and relative element stiffness
|
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.