Package | Description |
---|---|
nxopen.cae.optimization |
Provides classes and interfaces relating to Optimization.
|
Modifier and Type | Field and Description |
---|---|
static TBSObjectives.ObjectiveType |
TBSObjectives.ObjectiveType.MAX_MIN
Target is the MINMAX formulation of the list of design responses
|
static TBSObjectives.ObjectiveType |
TBSObjectives.ObjectiveType.MAXIMUM
Target is to maximize the list of design response
|
static TBSObjectives.ObjectiveType |
TBSObjectives.ObjectiveType.MINIMUM
Target is to minimize the list of design response
|
Modifier and Type | Method and Description |
---|---|
TBSObjectives.ObjectiveType |
TBSObjectives.targetObjective()
Returns the target objective type
License requirements: None. |
static TBSObjectives.ObjectiveType |
TBSObjectives.ObjectiveType.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static TBSObjectives.ObjectiveType |
TBSObjectives.ObjectiveType.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static TBSObjectives.ObjectiveType[] |
TBSObjectives.ObjectiveType.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
TBSObjectives.setTargetObjective(TBSObjectives.ObjectiveType target)
License requirements: cae_opt_topo ("NX Topology Optimization") OR cae_opt_topobead ("NX Bead Optimization") OR cae_opt_toposhape ("NX Shape Optimization") . |
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.