ConnectorDevice Class¶
-
class
NXOpen.Routing.Electrical.
ConnectorDevice
¶ Bases:
NXOpen.Routing.SingleDevice
The Electrical ConnectorDevice corresponds to a connector instance of
NXOpen.Routing.SingleDevice
.To create a new instance of this class, use
NXOpen.Routing.Electrical.ConnectorDeviceCollection.CreateConnectorDevice
New in version NX4.0.2.
Properties¶
Property | Description |
---|---|
ComponentName | Returns or sets the component name. |
ConnectorType | Returns or sets the connector type. |
Guid | Returns or sets the object’s Global Unique Identifier (GUID). |
IsOccurrence | Returns whether this object is an occurrence or not. |
JournalIdentifier | Returns the identifier that would be recorded in a journal for this object. |
Name | Returns the custom name of the object. |
NxEquivalent | Returns or sets the NX equivalent object. |
OwningComponent | Returns the owning component, if this object is an occurrence. |
OwningPart | Returns the owning part of this object |
PartName | Returns or sets the part name |
PartNumber | Returns or sets the part number |
Prototype | Returns the prototype of this object if it is an occurrence. |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
DeleteAllAttributesByType | Deletes all attributes of a specific type. |
DeleteAttributeByTypeAndTitle | Deletes an attribute by type and title. |
DeleteCharacterstics | Removes the input list of characteristics from this object. |
DeleteUserAttribute | Deletes the first attribute encountered with the given Type, Title. |
DeleteUserAttributes | Deletes the attributes encountered with the given Type with option to update or not. |
FindConnections | Find connections. |
FindMatchingParts | Find parts matching the connector device. |
FindNearestCableDevice | Get the nearest NXOpen.Routing.Electrical.CableDevice encountered up the parent-child hierarchy. |
FindNearestHarnessDevice | Get the nearest NXOpen.Routing.Electrical.HarnessDevice encountered up the parent-child hierarchy. |
FindObject | Finds the NXOpen.NXObject with the given identifier as recorded in a journal. |
FindPlacer | Searches for a placement port for the connector device. |
FindRoutedStockDevices | Find routed stock devices. |
FindStockDevices | Find stock devices. |
GetAssignMethod | Get assign method. |
GetAttributeTitlesByType | Gets all the attribute titles of a specific type. |
GetBooleanUserAttribute | Gets a boolean attribute by Title and array Index. |
GetCharacteristics | Get all of the characteristics values on the this object. |
GetComputationalTimeUserAttribute | Gets a time attribute by Title and array Index. |
GetDestinationCharacteristics | Returns the destination characteristics from the input object. |
GetImplementedConnections | Gets connections implemented on single device. |
GetIntegerAttribute | Gets an integer attribute by title. |
GetIntegerCharacteristic | Get the value of an integer characteristic associated with the input name. |
GetIntegerUserAttribute | Gets an integer attribute by Title and array Index. |
GetItemDefinition | Get item definition. |
GetPartDefinition | Get part definition. |
GetRealAttribute | Gets a real attribute by title. |
GetRealCharacteristic | Get the value of a real characteristic associated with the input name. |
GetRealUserAttribute | Gets a real attribute by Title and array Index. |
GetReferenceAttribute | Gets the reference string (not the calculated value) of a string attribute that uses a reference string. |
GetReferencingDeviceRelshps | Gets referencing device relationships. |
GetRelatedSingleDevices | Assuming this single device to be the relating single device in a NXOpen.Routing.DeviceRelationship , get associated related single devices. |
GetRelatingSingleDevice | Assuming this single device to be the related single device in a NXOpen.Routing.DeviceRelationship , get associated relating single device. |
GetStringAttribute | Gets a string attribute value by title. |
GetStringCharacteristic | Get the value of a string characteristic associated with the input name. |
GetStringUserAttribute | Gets a string attribute by Title and array Index. |
GetTerminal | Get NXOpen.Routing.LogicalTerminal given the name of the terminal. |
GetTerminals | Get terminals. |
GetTimeAttribute | Gets a time attribute by title. |
GetTimeUserAttribute | Gets a time attribute by Title and array Index. |
GetUserAttribute | Gets the first attribute encountered on the object, if any, with a given Title, Type and array Index. |
GetUserAttributeAsString | Gets the first attribute encountered on the object, if any, with a given title, type and array index. |
GetUserAttributeCount | Gets the count of set attributes on the object, if any, of the given type. |
GetUserAttributeLock | Determine the lock of the given attribute. |
GetUserAttributeSize | Gets the size of the first attribute encountered on the object, if any, with a given Title and Type. |
GetUserAttributeSourceObjects | Returns an array of objects from which this object presents attributes. |
GetUserAttributes | Gets all the attributes that have been set on the given object. |
GetUserAttributesAsStrings | Gets all the attributes that have been set on the given object. |
HasUserAttribute | Determines if an attribute with the given Title, Type and array Index is present on the object Unset attributes will not be detected by this function, as its purpose is to test for the actual presence of the attribute on the object. |
IsAssigned | Get status of a connector device (assigned or not). |
IsNxConnector | Is the device a connector? @return |
IsNxDevice | Is the device a NX device? @return |
IsUsedInRoutedConnection | Is the device used in a routed connection? @return |
ManuallyAssignConnector | Assign a connector manually. |
ManuallyDelete | Deletes the single device. |
PlaceConnectorOnPort | Loads the parts based on the NXOpen.Routing.CharacteristicList adds the instance of the part to the current work part and places the instance on the placer. |
Prints a representation of this object to the system log file. | |
ProxyAssignConnector | Assign a connector to a proxy port. |
RemoveTerminal | Remove a terminal. |
SetAttribute | Creates or modifies an integer attribute. |
SetBooleanUserAttribute | Creates or modifies a boolean attribute with the option to update or not. |
SetCharacteristic | Set the value of an integer characteristic associated with the input name, adds a new characteristic to the list if one doesn’t exist already. |
SetCharacteristics | Set all of the characteristics values on this object. |
SetName | Sets the custom name of the object. |
SetPartDefinition | Sets part definition. |
SetReferenceAttribute | Creates or modifies a string attribute which uses a reference string. |
SetTimeAttribute | Creates or modifies a time attribute. |
SetTimeUserAttribute | Creates or modifies a time attribute with the option to update or not. |
SetUserAttribute | Creates or modifies an attribute with the option to update or not. |
SetUserAttributeLock | Lock or unlock the given attribute. |
UnassignConnector | Unassign connector. |
Enumerations¶
ConnectorDeviceAssign Enumeration | Assignment method |
ConnectorDeviceComponentType Enumeration | Component type |
Property Detail¶
ComponentName¶
-
ConnectorDevice.
ComponentName
¶ Returns or sets the component name.
-------------------------------------
Getter Method
Signature
ComponentName()
Returns: Return type: str New in version NX4.0.2.
License requirements: routing_advanced (“Routing Advanced”), routing_base (“Routing Basic”)
-------------------------------------
Setter Method
Signature
ComponentName(componentName)
Parameters: componentName (str) – New in version NX4.0.2.
License requirements: routing_advanced (“Routing Advanced”), routing_base (“Routing Basic”)
ConnectorType¶
-
ConnectorDevice.
ConnectorType
¶ Returns or sets the connector type.
-------------------------------------
Getter Method
Signature
ConnectorType()
Returns: Return type: NXOpen.Routing.Electrical.ConnectorDeviceComponentType
New in version NX4.0.2.
License requirements: routing_advanced (“Routing Advanced”), routing_base (“Routing Basic”)
-------------------------------------
Setter Method
Signature
ConnectorType(elecRlistComponent)
Parameters: elecRlistComponent ( NXOpen.Routing.Electrical.ConnectorDeviceComponentType
) –New in version NX4.0.2.
License requirements: routing_advanced (“Routing Advanced”), routing_base (“Routing Basic”)
IsOccurrence¶
-
ConnectorDevice.
IsOccurrence
¶ Returns whether this object is an occurrence or not.
-------------------------------------
Getter Method
Signature
IsOccurrence()
Returns: This object is an occurrence Return type: bool New in version NX3.0.0.
License requirements: None.
JournalIdentifier¶
-
ConnectorDevice.
JournalIdentifier
¶ Returns the identifier that would be recorded in a journal for this object.
This may not be the same across different releases of the software.
-------------------------------------
Getter Method
Signature
JournalIdentifier()
Returns: Return type: str New in version NX3.0.0.
License requirements: None.
Name¶
-
ConnectorDevice.
Name
¶ Returns the custom name of the object.
-------------------------------------
Getter Method
Signature
Name()
Returns: Return type: str New in version NX3.0.0.
License requirements: None.
OwningComponent¶
-
ConnectorDevice.
OwningComponent
¶ Returns the owning component, if this object is an occurrence.
-------------------------------------
Getter Method
Signature
OwningComponent()
Returns: Return type: NXOpen.Assemblies.Component
New in version NX3.0.0.
License requirements: None.
OwningPart¶
-
ConnectorDevice.
OwningPart
¶ Returns the owning part of this object
-------------------------------------
Getter Method
Signature
OwningPart()
Returns: The owning part of this object or null if it does not have an owner Return type: NXOpen.BasePart
New in version NX3.0.0.
License requirements: None.
Prototype¶
-
ConnectorDevice.
Prototype
¶ Returns the prototype of this object if it is an occurrence.
-------------------------------------
Getter Method
Signature
Prototype()
Returns: The prototype of this object or null if this object is not an occurrence Return type: NXOpen.INXObject
New in version NX3.0.0.
License requirements: None.
Method Detail¶
DeleteCharacterstics¶
-
ConnectorDevice.
DeleteCharacterstics
¶ Removes the input list of characteristics from this object.
Signature
DeleteCharacterstics(values)
Parameters: values ( NXOpen.Routing.CharacteristicList
) –New in version NX4.0.0.
License requirements: routing_base (“Routing Basic”)
FindConnections¶
-
ConnectorDevice.
FindConnections
¶ Find connections.
Signature
FindConnections()
Returns: Return type: list of NXOpen.Routing.Electrical.Connection
New in version NX4.0.2.
License requirements: routing_advanced (“Routing Advanced”), routing_base (“Routing Basic”)
FindMatchingParts¶
-
ConnectorDevice.
FindMatchingParts
¶ Find parts matching the connector device.
Searches for “PART_NAME” property on connector device to search for matches in the part tables Returns all matching rows from the part tables.
Signature
FindMatchingParts()
Returns: Return type: list of NXOpen.Routing.CharacteristicList
New in version NX6.0.0.
License requirements: routing_advanced (“Routing Advanced”), routing_base (“Routing Basic”)
FindNearestCableDevice¶
-
ConnectorDevice.
FindNearestCableDevice
¶ Get the nearest
NXOpen.Routing.Electrical.CableDevice
encountered up the parent-child hierarchy.Signature
FindNearestCableDevice()
Returns: Return type: NXOpen.Routing.Electrical.CableDevice
New in version NX4.0.2.
License requirements: routing_advanced (“Routing Advanced”), routing_base (“Routing Basic”)
FindNearestHarnessDevice¶
-
ConnectorDevice.
FindNearestHarnessDevice
¶ Get the nearest
NXOpen.Routing.Electrical.HarnessDevice
encountered up the parent-child hierarchy.Signature
FindNearestHarnessDevice()
Returns: Return type: NXOpen.Routing.Electrical.HarnessDevice
New in version NX4.0.2.
License requirements: routing_advanced (“Routing Advanced”), routing_base (“Routing Basic”)
FindObject¶
-
ConnectorDevice.
FindObject
¶ Finds the
NXOpen.NXObject
with the given identifier as recorded in a journal.An object may not return the same value as its JournalIdentifier in different versions of the software. However newer versions of the software should find the same object when FindObject is passed older versions of its journal identifier. In general, this method should not be used in handwritten code and exists to support record and playback of journals.
An exception will be thrown if no object can be found with the given journal identifier.
Signature
FindObject(journalIdentifier)
Parameters: journalIdentifier (str) – Journal identifier of the object Returns: Return type: NXOpen.INXObject
New in version NX3.0.0.
License requirements: None.
FindPlacer¶
-
ConnectorDevice.
FindPlacer
¶ Searches for a placement port for the connector device.
The placement port is defined in the component list by attribute “DEVICE_PIN” or “EQUIPMENT_PIN”. If the attribute is not defined, searches for the first available port on the relating device.
Signature
FindPlacer()
Returns: a tuple Return type: A tuple consisting of (placer, placerPos). placer is a NXOpen.Routing.Port
. placerPos is a float.New in version NX6.0.0.
License requirements: routing_advanced (“Routing Advanced”), routing_base (“Routing Basic”)
FindRoutedStockDevices¶
-
ConnectorDevice.
FindRoutedStockDevices
¶ Find routed stock devices.
Signature
FindRoutedStockDevices()
Returns: Return type: list of NXOpen.Routing.Electrical.ElectricalStockDevice
New in version NX4.0.2.
License requirements: routing_advanced (“Routing Advanced”), routing_base (“Routing Basic”)
FindStockDevices¶
-
ConnectorDevice.
FindStockDevices
¶ Find stock devices.
Signature
FindStockDevices()
Returns: Return type: list of NXOpen.Routing.Electrical.ElectricalStockDevice
New in version NX4.0.2.
License requirements: routing_advanced (“Routing Advanced”), routing_base (“Routing Basic”)
GetAssignMethod¶
-
ConnectorDevice.
GetAssignMethod
¶ Get assign method.
Signature
GetAssignMethod()
Returns: Return type: NXOpen.Routing.Electrical.ConnectorDeviceAssign
New in version NX4.0.2.
License requirements: routing_advanced (“Routing Advanced”), routing_base (“Routing Basic”)
GetCharacteristics¶
-
ConnectorDevice.
GetCharacteristics
¶ Get all of the characteristics values on the this object.
Signature
GetCharacteristics()
Returns: Return type: NXOpen.Routing.CharacteristicList
New in version NX4.0.0.
License requirements: routing_base (“Routing Basic”)
GetDestinationCharacteristics¶
-
ConnectorDevice.
GetDestinationCharacteristics
¶ Returns the destination characteristics from the input object.
Retrieves the description of which destination characteristics to read from the application view and then reads those destination characteristics from the object
- Ports: Reads characteristics from the port.
- RCPs: Attempts to find a port at the RCP, reads characteristics from
the port if it exists, otherwise reads from the stock associated with the rcp.
- Segments: Reads characteristics from the stock associated with the segment.
- Components: Reads characteristics directly from the component.
- Stock: Reads characteristics from the stock or from the stock’s data.
Signature
GetDestinationCharacteristics()
Returns: Return type: NXOpen.Routing.CharacteristicList
New in version NX4.0.0.
License requirements: routing_base (“Routing Basic”)
GetIntegerCharacteristic¶
-
ConnectorDevice.
GetIntegerCharacteristic
¶ Get the value of an integer characteristic associated with the input name.
Signature
GetIntegerCharacteristic(name)
Parameters: name (str) – NOTE: The full Unicode character set is not supported for this parameter. Returns: Return type: int New in version NX4.0.0.
License requirements: routing_base (“Routing Basic”)
GetPartDefinition¶
-
ConnectorDevice.
GetPartDefinition
¶ Get part definition.
Signature
GetPartDefinition()
Returns: Return type: NXOpen.Routing.Electrical.ElectricalPartDefinitionShadow
New in version NX4.0.2.
License requirements: routing_advanced (“Routing Advanced”), routing_base (“Routing Basic”)
GetRealCharacteristic¶
-
ConnectorDevice.
GetRealCharacteristic
¶ Get the value of a real characteristic associated with the input name.
Signature
GetRealCharacteristic(name)
Parameters: name (str) – NOTE: The full Unicode character set is not supported for this parameter. Returns: Return type: float New in version NX4.0.0.
License requirements: routing_base (“Routing Basic”)
GetStringCharacteristic¶
-
ConnectorDevice.
GetStringCharacteristic
¶ Get the value of a string characteristic associated with the input name.
Signature
GetStringCharacteristic(name)
Parameters: name (str) – NOTE: The full Unicode character set is not supported for this parameter. Returns: Return type: str New in version NX4.0.0.
License requirements: routing_base (“Routing Basic”)
GetTerminal¶
-
ConnectorDevice.
GetTerminal
¶ Get
NXOpen.Routing.LogicalTerminal
given the name of the terminal.If a terminal does not exists creates a terminal
Signature
GetTerminal(terminalName, createTerminal)
Parameters: - terminalName (str) – NOTE: The full Unicode character set is not supported for this parameter.
- createTerminal (bool) – TRUE - creates a new terminal if one does not exist with given name
Returns: Return type: New in version NX5.0.0.
License requirements: routing_advanced (“Routing Advanced”), routing_base (“Routing Basic”)
GetTerminals¶
-
ConnectorDevice.
GetTerminals
¶ Get terminals.
Signature
GetTerminals()
Returns: Return type: list of NXOpen.Routing.LogicalTerminal
New in version NX4.0.2.
License requirements: routing_advanced (“Routing Advanced”), routing_base (“Routing Basic”)
IsAssigned¶
-
ConnectorDevice.
IsAssigned
¶ Get status of a connector device (assigned or not).
Signature
IsAssigned()
Returns: Return type: bool New in version NX4.0.2.
License requirements: routing_advanced (“Routing Advanced”), routing_base (“Routing Basic”)
IsNxConnector¶
-
ConnectorDevice.
IsNxConnector
¶ Is the device a connector?
Signature
IsNxConnector(elecHarnessDevice)
Parameters: elecHarnessDevice ( NXOpen.Routing.Electrical.HarnessDevice
) –Returns: Return type: bool New in version NX4.0.2.
License requirements: routing_advanced (“Routing Advanced”), routing_base (“Routing Basic”)
IsNxDevice¶
-
ConnectorDevice.
IsNxDevice
¶ Is the device a NX device?
Signature
IsNxDevice(elecHarnessDevice)
Parameters: elecHarnessDevice ( NXOpen.Routing.Electrical.HarnessDevice
) –Returns: Return type: bool New in version NX4.0.2.
License requirements: routing_advanced (“Routing Advanced”), routing_base (“Routing Basic”)
IsUsedInRoutedConnection¶
-
ConnectorDevice.
IsUsedInRoutedConnection
¶ Is the device used in a routed connection?
Signature
IsUsedInRoutedConnection(elecHarnessDevice)
Parameters: elecHarnessDevice ( NXOpen.Routing.Electrical.HarnessDevice
) –Returns: Return type: bool New in version NX4.0.2.
License requirements: routing_advanced (“Routing Advanced”), routing_base (“Routing Basic”)
ManuallyAssignConnector¶
-
ConnectorDevice.
ManuallyAssignConnector
¶ Assign a connector manually.
Signature
ManuallyAssignConnector(elecConnectorPartOccurrence)
Parameters: elecConnectorPartOccurrence ( NXOpen.Assemblies.Component
) – Component to assign.New in version NX4.0.2.
License requirements: routing_advanced (“Routing Advanced”), routing_base (“Routing Basic”)
PlaceConnectorOnPort¶
-
ConnectorDevice.
PlaceConnectorOnPort
¶ Loads the parts based on the
NXOpen.Routing.CharacteristicList
adds the instance of the part to the current work part and places the instance on the placer.Signature
PlaceConnectorOnPort(match, placer)
Parameters: - match (
NXOpen.Routing.CharacteristicList
) – - placer (
NXOpen.Routing.Port
) –
Returns: Return type: New in version NX6.0.0.
License requirements: routing_advanced (“Routing Advanced”), routing_base (“Routing Basic”)
- match (
Print¶
-
ConnectorDevice.
Print
¶ Prints a representation of this object to the system log file.
Signature
Print()
New in version NX3.0.0.
License requirements: None.
ProxyAssignConnector¶
-
ConnectorDevice.
ProxyAssignConnector
¶ Assign a connector to a proxy port.
Signature
ProxyAssignConnector(proxy)
Parameters: proxy ( NXOpen.Routing.Port
) – Assigned port.New in version NX8.0.0.
License requirements: routing_advanced (“Routing Advanced”), routing_base (“Routing Basic”)
RemoveTerminal¶
-
ConnectorDevice.
RemoveTerminal
¶ Remove a terminal.
Signature
RemoveTerminal(routeTerminalToRemove)
Parameters: routeTerminalToRemove ( NXOpen.Routing.LogicalTerminal
) –Returns: Return type: bool New in version NX4.0.2.
License requirements: routing_advanced (“Routing Advanced”), routing_base (“Routing Basic”)
SetCharacteristic¶
-
ConnectorDevice.
SetCharacteristic
¶ Overloaded method SetCharacteristic
SetCharacteristic(name, value)
SetCharacteristic(name, value)
SetCharacteristic(name, value)
-------------------------------------
Set the value of an integer characteristic associated with the input name, adds a new characteristic to the list if one doesn’t exist already. Converts the type of an existing characteristic with the same name to integer if it’s type is not integer.
Signature
SetCharacteristic(name, value)
Parameters: - name (str) – NOTE: The full Unicode character set is not supported for this parameter.
- value (int) –
New in version NX4.0.0.
License requirements: routing_base (“Routing Basic”)
-------------------------------------
Set the value of an real characteristic associated with the input name, adds a new characteristic to the list if one doesn’t exist already. Converts the type of an existing characteristic with the same name to real if it’s type is not real.
Signature
SetCharacteristic(name, value)
Parameters: - name (str) – NOTE: The full Unicode character set is not supported for this parameter.
- value (float) –
New in version NX4.0.0.
License requirements: routing_base (“Routing Basic”)
-------------------------------------
Set the value of an string characteristic associated with the input name, adds a new characteristic to the list if one doesn’t exist already. Converts the type of an existing characteristic with the same name to string if it’s type is not string.
Signature
SetCharacteristic(name, value)
Parameters: - name (str) – NOTE: The full Unicode character set is not supported for this parameter.
- value (str) – NOTE: The full Unicode character set is not supported for this parameter.
New in version NX4.0.0.
License requirements: routing_base (“Routing Basic”)
-------------------------------------
SetCharacteristics¶
-
ConnectorDevice.
SetCharacteristics
¶ Set all of the characteristics values on this object.
Signature
SetCharacteristics(values)
Parameters: values ( NXOpen.Routing.CharacteristicList
) –New in version NX4.0.0.
License requirements: routing_base (“Routing Basic”)
SetName¶
-
ConnectorDevice.
SetName
¶ Sets the custom name of the object.
NOTE: This method should not be used to edit a read-only object such as a Mirrored PMI object. If it is, the changes will be overridden when the part is updated.
Signature
SetName(name)
Parameters: name (str) – New in version NX3.0.0.
License requirements: None.
SetPartDefinition¶
-
ConnectorDevice.
SetPartDefinition
¶ Sets part definition.
Signature
SetPartDefinition(elecPartDefinitionShadow)
Parameters: elecPartDefinitionShadow ( NXOpen.Routing.Electrical.ElectricalPartDefinitionShadow
) –New in version NX4.0.2.
License requirements: routing_advanced (“Routing Advanced”), routing_base (“Routing Basic”)