CableDevice Class¶
-
class
NXOpen.Routing.Electrical.
CableDevice
¶ Bases:
NXOpen.Routing.Electrical.ElectricalStockDevice
Corresponds to a cable instance of an
NXOpen.Routing.Electrical.ElectricalStockDevice
.A cable consists of both a
NXOpen.Routing.Electrical.CableDevice
and aNXOpen.Routing.Electrical.CableDefinition
. ANXOpen.Routing.Electrical.CableDevice
object uses aNXOpen.Routing.Electrical.CableDefinition
to hold a collection ofNXOpen.Routing.Electrical.WireDevice
objects and/orNXOpen.Routing.Electrical.CableDevice
objects contained by the cable.See the NX Routing help for detailed information on the Connection data model.
Creator not available in KF.
New in version NX4.0.2.
Properties¶
Property | Description |
---|---|
ColorName | Returns or sets the color name. |
CutLength | Returns or sets the cut length. |
Guid | Returns or sets the object’s Global Unique Identifier (GUID). |
IsOccurrence | Returns whether this object is an occurrence or not. |
JournalIdentifier | Returns the identifier that would be recorded in a journal for this object. |
Name | Returns the custom name of the object. |
NxColorValue | Returns or sets the NX color value. |
NxEquivalent | Returns or sets the NX equivalent object. |
OwningComponent | Returns the owning component, if this object is an occurrence. |
OwningPart | Returns the owning part of this object |
PartName | Returns or sets the part name |
PartNumber | Returns or sets the part number |
Prototype | Returns the prototype of this object if it is an occurrence. |
StockDefinition | Returns or sets the stock definition. |
StockLength | Returns or sets the stock length. |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
CalculateCutLength | Calculates and sets cut length on object. |
ChangeHarness | Adds this stockdevice as child of given HarnessDevice. |
DeleteAllAttributesByType | Deletes all attributes of a specific type. |
DeleteAttributeByTypeAndTitle | Deletes an attribute by type and title. |
DeleteCharacterstics | Removes the input list of characteristics from this object. |
DeleteUserAttribute | Deletes the first attribute encountered with the given Type, Title. |
DeleteUserAttributes | Deletes the attributes encountered with the given Type with option to update or not. |
FindFromConnector | Find the from connector for this stock device. |
FindImplementedConnection | Find the NXOpen.Routing.Electrical.Connection implemented by this device. |
FindNearestHarnessDefinition | Get nearest NXOpen.Routing.Electrical.HarnessDefinition encountered up the parent-child hierarchy. |
FindNearestHarnessDevice | Find the nearest NXOpen.Routing.Electrical.HarnessDevice encountered up the parent-child hierarchy. |
FindObject | Finds the NXOpen.NXObject with the given identifier as recorded in a journal. |
FindToConnector | Find the to connector for this stock device. |
FindTopmostCableDefinition | Get topmost NXOpen.Routing.Electrical.CableDefinition encountered up the parent-child hierarchy. |
GetAssemblyDefinition | Returns the associated NXOpen.Routing.Electrical.CableDefinition . |
GetAttributeTitlesByType | Gets all the attribute titles of a specific type. |
GetBooleanUserAttribute | Gets a boolean attribute by Title and array Index. |
GetCharacteristics | Get all of the characteristics values on the this object. |
GetComputationalTimeUserAttribute | Gets a time attribute by Title and array Index. |
GetConduitPartNumber | Returns the part number of the conduit applied over this NXOpen.Routing.Electrical.CableDevice object. |
GetDestinationCharacteristics | Returns the destination characteristics from the input object. |
GetImplementedConnections | Gets connections implemented on single device. |
GetIntegerAttribute | Gets an integer attribute by title. |
GetIntegerCharacteristic | Get the value of an integer characteristic associated with the input name. |
GetIntegerUserAttribute | Gets an integer attribute by Title and array Index. |
GetIntermediateComponents | Get intermediate components @return |
GetIntermediateTerminals | Get the intermediate terminals associated to this stock device. |
GetItemDefinition | Get item definition. |
GetRealAttribute | Gets a real attribute by title. |
GetRealCharacteristic | Get the value of a real characteristic associated with the input name. |
GetRealUserAttribute | Gets a real attribute by Title and array Index. |
GetReferenceAttribute | Gets the reference string (not the calculated value) of a string attribute that uses a reference string. |
GetReferencingDeviceRelshps | Gets referencing device relationships. |
GetRelatedSingleDevices | Assuming this single device to be the relating single device in a NXOpen.Routing.DeviceRelationship , get associated related single devices. |
GetRelatingSingleDevice | Assuming this single device to be the related single device in a NXOpen.Routing.DeviceRelationship , get associated relating single device. |
GetStringAttribute | Gets a string attribute value by title. |
GetStringCharacteristic | Get the value of a string characteristic associated with the input name. |
GetStringUserAttribute | Gets a string attribute by Title and array Index. |
GetTimeAttribute | Gets a time attribute by title. |
GetTimeUserAttribute | Gets a time attribute by Title and array Index. |
GetUserAttribute | Gets the first attribute encountered on the object, if any, with a given Title, Type and array Index. |
GetUserAttributeAsString | Gets the first attribute encountered on the object, if any, with a given title, type and array index. |
GetUserAttributeCount | Gets the count of set attributes on the object, if any, of the given type. |
GetUserAttributeLock | Determine the lock of the given attribute. |
GetUserAttributeSize | Gets the size of the first attribute encountered on the object, if any, with a given Title and Type. |
GetUserAttributeSourceObjects | Returns an array of objects from which this object presents attributes. |
GetUserAttributes | Gets all the attributes that have been set on the given object. |
GetUserAttributesAsStrings | Gets all the attributes that have been set on the given object. |
HasIntermediateComponents | Does this stock device have intermediate components? @return |
HasUserAttribute | Determines if an attribute with the given Title, Type and array Index is present on the object Unset attributes will not be detected by this function, as its purpose is to test for the actual presence of the attribute on the object. |
ImportCablePart | Loads the given cable part and imports the connections from given part and adds them as children to the NXOpen.Routing.Electrical.CableDevice . |
ManuallyDelete | Deletes the single device. |
ManuallyRoute | Manually routes a NXOpen.Routing.Electrical.ElectricalStockDevice . |
Prints a representation of this object to the system log file. | |
SetAttribute | Creates or modifies an integer attribute. |
SetBooleanUserAttribute | Creates or modifies a boolean attribute with the option to update or not. |
SetCharacteristic | Set the value of an integer characteristic associated with the input name, adds a new characteristic to the list if one doesn’t exist already. |
SetCharacteristics | Set all of the characteristics values on this object. |
SetConduitPartNumber | Sets the part number of the conduit to be applied over this NXOpen.Routing.Electrical.CableDevice object. |
SetName | Sets the custom name of the object. |
SetReferenceAttribute | Creates or modifies a string attribute which uses a reference string. |
SetTimeAttribute | Creates or modifies a time attribute. |
SetTimeUserAttribute | Creates or modifies a time attribute with the option to update or not. |
SetUserAttribute | Creates or modifies an attribute with the option to update or not. |
SetUserAttributeLock | Lock or unlock the given attribute. |
Property Detail¶
IsOccurrence¶
-
CableDevice.
IsOccurrence
¶ Returns whether this object is an occurrence or not.
-------------------------------------
Getter Method
Signature
IsOccurrence()
Returns: This object is an occurrence Return type: bool New in version NX3.0.0.
License requirements: None.
JournalIdentifier¶
-
CableDevice.
JournalIdentifier
¶ Returns the identifier that would be recorded in a journal for this object.
This may not be the same across different releases of the software.
-------------------------------------
Getter Method
Signature
JournalIdentifier()
Returns: Return type: str New in version NX3.0.0.
License requirements: None.
Name¶
-
CableDevice.
Name
¶ Returns the custom name of the object.
-------------------------------------
Getter Method
Signature
Name()
Returns: Return type: str New in version NX3.0.0.
License requirements: None.
OwningComponent¶
-
CableDevice.
OwningComponent
¶ Returns the owning component, if this object is an occurrence.
-------------------------------------
Getter Method
Signature
OwningComponent()
Returns: Return type: NXOpen.Assemblies.Component
New in version NX3.0.0.
License requirements: None.
OwningPart¶
-
CableDevice.
OwningPart
¶ Returns the owning part of this object
-------------------------------------
Getter Method
Signature
OwningPart()
Returns: The owning part of this object or null if it does not have an owner Return type: NXOpen.BasePart
New in version NX3.0.0.
License requirements: None.
Prototype¶
-
CableDevice.
Prototype
¶ Returns the prototype of this object if it is an occurrence.
-------------------------------------
Getter Method
Signature
Prototype()
Returns: The prototype of this object or null if this object is not an occurrence Return type: NXOpen.INXObject
New in version NX3.0.0.
License requirements: None.
Method Detail¶
DeleteCharacterstics¶
-
CableDevice.
DeleteCharacterstics
¶ Removes the input list of characteristics from this object.
Signature
DeleteCharacterstics(values)
Parameters: values ( NXOpen.Routing.CharacteristicList
) –New in version NX4.0.0.
License requirements: routing_base (“Routing Basic”)
FindObject¶
-
CableDevice.
FindObject
¶ Finds the
NXOpen.NXObject
with the given identifier as recorded in a journal.An object may not return the same value as its JournalIdentifier in different versions of the software. However newer versions of the software should find the same object when FindObject is passed older versions of its journal identifier. In general, this method should not be used in handwritten code and exists to support record and playback of journals.
An exception will be thrown if no object can be found with the given journal identifier.
Signature
FindObject(journalIdentifier)
Parameters: journalIdentifier (str) – Journal identifier of the object Returns: Return type: NXOpen.INXObject
New in version NX3.0.0.
License requirements: None.
GetAssemblyDefinition¶
-
CableDevice.
GetAssemblyDefinition
¶ Returns the associated
NXOpen.Routing.Electrical.CableDefinition
.Signature
GetAssemblyDefinition()
Returns: Return type: NXOpen.Routing.Electrical.CableDefinition
New in version NX4.0.2.
License requirements: routing_advanced (“Routing Advanced”), routing_base (“Routing Basic”)
GetCharacteristics¶
-
CableDevice.
GetCharacteristics
¶ Get all of the characteristics values on the this object.
Signature
GetCharacteristics()
Returns: Return type: NXOpen.Routing.CharacteristicList
New in version NX4.0.0.
License requirements: routing_base (“Routing Basic”)
GetConduitPartNumber¶
-
CableDevice.
GetConduitPartNumber
¶ Returns the part number of the conduit applied over this
NXOpen.Routing.Electrical.CableDevice
object.Signature
GetConduitPartNumber()
Returns: Return type: str New in version NX7.5.0.
License requirements: routing_advanced (“Routing Advanced”), routing_base (“Routing Basic”)
GetDestinationCharacteristics¶
-
CableDevice.
GetDestinationCharacteristics
¶ Returns the destination characteristics from the input object.
Retrieves the description of which destination characteristics to read from the application view and then reads those destination characteristics from the object
- Ports: Reads characteristics from the port.
- RCPs: Attempts to find a port at the RCP, reads characteristics from
the port if it exists, otherwise reads from the stock associated with the rcp.
- Segments: Reads characteristics from the stock associated with the segment.
- Components: Reads characteristics directly from the component.
- Stock: Reads characteristics from the stock or from the stock’s data.
Signature
GetDestinationCharacteristics()
Returns: Return type: NXOpen.Routing.CharacteristicList
New in version NX4.0.0.
License requirements: routing_base (“Routing Basic”)
GetIntegerCharacteristic¶
-
CableDevice.
GetIntegerCharacteristic
¶ Get the value of an integer characteristic associated with the input name.
Signature
GetIntegerCharacteristic(name)
Parameters: name (str) – NOTE: The full Unicode character set is not supported for this parameter. Returns: Return type: int New in version NX4.0.0.
License requirements: routing_base (“Routing Basic”)
GetRealCharacteristic¶
-
CableDevice.
GetRealCharacteristic
¶ Get the value of a real characteristic associated with the input name.
Signature
GetRealCharacteristic(name)
Parameters: name (str) – NOTE: The full Unicode character set is not supported for this parameter. Returns: Return type: float New in version NX4.0.0.
License requirements: routing_base (“Routing Basic”)
GetStringCharacteristic¶
-
CableDevice.
GetStringCharacteristic
¶ Get the value of a string characteristic associated with the input name.
Signature
GetStringCharacteristic(name)
Parameters: name (str) – NOTE: The full Unicode character set is not supported for this parameter. Returns: Return type: str New in version NX4.0.0.
License requirements: routing_base (“Routing Basic”)
ImportCablePart¶
-
CableDevice.
ImportCablePart
¶ Loads the given cable part and imports the connections from given part and adds them as children to the
NXOpen.Routing.Electrical.CableDevice
.Signature
ImportCablePart(partName)
Parameters: partName (str) – Must be fullpath and PART_NAME for a regular part and PART_NAME for part family or part table parts NOTE: The full Unicode character set is not supported for this parameter. New in version NX6.0.1.
License requirements: routing_advanced (“Routing Advanced”), routing_base (“Routing Basic”)
Print¶
-
CableDevice.
Print
¶ Prints a representation of this object to the system log file.
Signature
Print()
New in version NX3.0.0.
License requirements: None.
SetCharacteristic¶
-
CableDevice.
SetCharacteristic
¶ Overloaded method SetCharacteristic
SetCharacteristic(name, value)
SetCharacteristic(name, value)
SetCharacteristic(name, value)
-------------------------------------
Set the value of an integer characteristic associated with the input name, adds a new characteristic to the list if one doesn’t exist already. Converts the type of an existing characteristic with the same name to integer if it’s type is not integer.
Signature
SetCharacteristic(name, value)
Parameters: - name (str) – NOTE: The full Unicode character set is not supported for this parameter.
- value (int) –
New in version NX4.0.0.
License requirements: routing_base (“Routing Basic”)
-------------------------------------
Set the value of an real characteristic associated with the input name, adds a new characteristic to the list if one doesn’t exist already. Converts the type of an existing characteristic with the same name to real if it’s type is not real.
Signature
SetCharacteristic(name, value)
Parameters: - name (str) – NOTE: The full Unicode character set is not supported for this parameter.
- value (float) –
New in version NX4.0.0.
License requirements: routing_base (“Routing Basic”)
-------------------------------------
Set the value of an string characteristic associated with the input name, adds a new characteristic to the list if one doesn’t exist already. Converts the type of an existing characteristic with the same name to string if it’s type is not string.
Signature
SetCharacteristic(name, value)
Parameters: - name (str) – NOTE: The full Unicode character set is not supported for this parameter.
- value (str) – NOTE: The full Unicode character set is not supported for this parameter.
New in version NX4.0.0.
License requirements: routing_base (“Routing Basic”)
-------------------------------------
SetCharacteristics¶
-
CableDevice.
SetCharacteristics
¶ Set all of the characteristics values on this object.
Signature
SetCharacteristics(values)
Parameters: values ( NXOpen.Routing.CharacteristicList
) –New in version NX4.0.0.
License requirements: routing_base (“Routing Basic”)
SetConduitPartNumber¶
-
CableDevice.
SetConduitPartNumber
¶ Sets the part number of the conduit to be applied over this
NXOpen.Routing.Electrical.CableDevice
object.Signature
SetConduitPartNumber(conduitPartNumber)
Parameters: conduitPartNumber (str) – NOTE: The full Unicode character set is not supported for this parameter. New in version NX7.5.0.
License requirements: routing_advanced (“Routing Advanced”), routing_base (“Routing Basic”)
SetName¶
-
CableDevice.
SetName
¶ Sets the custom name of the object.
NOTE: This method should not be used to edit a read-only object such as a Mirrored PMI object. If it is, the changes will be overridden when the part is updated.
Signature
SetName(name)
Parameters: name (str) – New in version NX3.0.0.
License requirements: None.