ConnectorDeviceCollection Class¶
-
class
NXOpen.Routing.Electrical.
ConnectorDeviceCollection
¶ Bases:
object
Represents a collection of
NXOpen.Routing.Electrical.ConnectorDevice
(CD) objects.To obtain an instance of this class, refer to
NXOpen.Routing.RouteManager
New in version NX4.0.2.
Methods¶
Method | Description |
---|---|
AutoAssignConnectors | Auto assignment is done using one of the three matching methods, Part Name, Component Name or Attribute. |
CreateConnectorDevice | Creates a NXOpen.Routing.Electrical.ConnectorDevice . |
GetConnectorSingleDevices | Get connectors from the work part. |
GetEquipmentSingleDevices | Get equipment from the work part. |
Method Detail¶
AutoAssignConnectors¶
-
ConnectorDeviceCollection.
AutoAssignConnectors
¶ Auto assignment is done using one of the three matching methods, Part Name, Component Name or Attribute.
Signature
AutoAssignConnectors(connectors)
Parameters: connectors (list of NXOpen.Routing.Electrical.ConnectorDevice
) –New in version NX4.0.2.
License requirements: routing_advanced (“Routing Advanced”), routing_base (“Routing Basic”)
CreateConnectorDevice¶
-
ConnectorDeviceCollection.
CreateConnectorDevice
¶ Overloaded method CreateConnectorDevice
CreateConnectorDevice(connectorType, componentName)
CreateConnectorDevice(harnessDevice, equipmentName, connectorName, connectorType)
-------------------------------------
Creates a
NXOpen.Routing.Electrical.ConnectorDevice
.Signature
CreateConnectorDevice(connectorType, componentName)
Parameters: - connectorType (
NXOpen.Routing.Electrical.ConnectorDeviceComponentType
) – - componentName (str) – NOTE: The full Unicode character set is not supported for this parameter.
Returns: Return type: New in version NX4.0.2.
License requirements: routing_advanced (“Routing Advanced”), routing_base (“Routing Basic”)
-------------------------------------
Finds or Creates a
NXOpen.Routing.Electrical.ConnectorDevice
for given equipmentName and or connectorName. BuildsNXOpen.Routing.Electrical.ElectricalDeviceRelationship
between equipment and connector, if equipmentName and connectorName are not None. Adds connector to harnessDevice, if connectorName and harnessDevice are not None.Signature
CreateConnectorDevice(harnessDevice, equipmentName, connectorName, connectorType)
Parameters: - harnessDevice (
NXOpen.Routing.Electrical.HarnessDevice
) – can be None - equipmentName (str) – can be None if connectorName is not None NOTE: The full Unicode character set is not supported for this parameter.
- connectorName (str) – can be None if equipmentName is not None NOTE: The full Unicode character set is not supported for this parameter.
- connectorType (
NXOpen.Routing.Electrical.ConnectorDeviceComponentType
) –
Returns: Return type: New in version NX5.0.0.
License requirements: routing_advanced (“Routing Advanced”), routing_base (“Routing Basic”)
-------------------------------------
GetConnectorSingleDevices¶
-
ConnectorDeviceCollection.
GetConnectorSingleDevices
¶ Get connectors from the work part.
Signature
GetConnectorSingleDevices()
Returns: Return type: list of NXOpen.Routing.Electrical.ConnectorDevice
New in version NX4.0.2.
License requirements: routing_advanced (“Routing Advanced”), routing_base (“Routing Basic”)
GetEquipmentSingleDevices¶
-
ConnectorDeviceCollection.
GetEquipmentSingleDevices
¶ Get equipment from the work part.
Signature
GetEquipmentSingleDevices()
Returns: Return type: list of NXOpen.Routing.Electrical.ConnectorDevice
New in version NX4.0.2.
License requirements: routing_advanced (“Routing Advanced”), routing_base (“Routing Basic”)