PartVisualizationShade Class¶
-
class
NXOpen.Preferences.
PartVisualizationShade
¶ Bases:
object
Represents the set of shade visualization preferences applicable to entire part
To obtain an instance of this class, refer to
NXOpen.Preferences.PartPreferences
New in version NX3.0.0.
Properties¶
Property | Description |
---|---|
AdvVisFacetScaleRatio | Returns or sets the facet to view scale ratio for Advanced Visualization views as specified by the user |
AdvVisFacetToViewScale | Returns or sets whether the facet to view scale for Advanced Visualization views should be computed automatically or should be defined by the user |
AdvancedVisViewAngleTolerance | Returns or sets the angle tolerance for advanced visualization views. |
AdvancedVisViewEdgeTolerance | Returns or sets the edge tolerance for advanced visualization views. |
AdvancedVisViewFaceTolerance | Returns or sets the face tolerance for advanced visualization views. |
AdvancedVisViewTolerance | Returns or sets the tolerance for advanced visualization views. |
AdvancedVisViewUpdateMode | Returns or sets the update mode for advanced visualization views. |
AdvancedVisViewWidthTolerance | Returns or sets the width tolerance for advanced Visualization Views. |
AlignAdvVisViewFacetsAlongEdges | Returns or sets the state of whether facets should be aligned along common edges for Advanced Visualization Views |
AlignShadedViewFacetsAlongEdges | Returns or sets the state of whether facets should be aligned along common edges for Shaded Views |
HiddenGeometryColor | Returns or sets the shade hidden geometry color. |
ShadedFacetScaleRatio | Returns or sets the facet to view scale ratio for Shaded views as specified by the user |
ShadedFacetToViewScale | Returns or sets whether the facet to view scale for Shaded views should be computed automatically or should be defined by the user |
ShadedViewAngleTolerance | Returns or sets the angle tolerance for shaded views. |
ShadedViewEdgeTolerance | Returns or sets the edge tolerance for shaded views. |
ShadedViewFaceTolerance | Returns or sets the face tolerance for shaded views. |
ShadedViewTolerance | Returns or sets the tolerance for shaded views. |
ShadedViewUpdateMode | Returns or sets the update mode for shaded views. |
Methods¶
Method | Description |
---|---|
GetAdvVisViewFacetTolerances | Returns the edge, face, angle and width tolerances to be used with the specified tolerance set for Advanced Visualization views. |
GetShadedViewFacetTolerances | Returns the edge, face and angle tolerances to be used with the specified tolerance set for shaded views. |
SetAdvVisViewFacetTolerances | Sets the edge, face, angle and width tolerances to be used with the specified tolerance set for Advanced Visualization views. |
SetShadedViewFacetTolerances | Sets the edge, face and angle tolerances to be used with the specified tolerance set for shaded views. |
Enumerations¶
PartVisualizationShadeAdvViewToleranceType Enumeration | Describes the available tolerance types for Advanced View. |
PartVisualizationShadeHiddenShadedFaceEdges Enumeration | Describes whether the shaded face edges are invisible or dashed visible or with a color to depict the hidden geometry |
PartVisualizationShadeShadedFaceEdge Enumeration | Describes whether the shaded face edges are having no color or body color or user defined color. |
PartVisualizationShadeShadedViewToleranceType Enumeration | Describes the available tolerance types for Shaded View. |
PartVisualizationShadeViewUpdateModeType Enumeration | Describes whether the applied changes are applicable to visible object or all object or no object |
Property Detail¶
AdvVisFacetScaleRatio¶
-
PartVisualizationShade.
AdvVisFacetScaleRatio
¶ Returns or sets the facet to view scale ratio for Advanced Visualization views as specified by the user
-------------------------------------
Getter Method
Signature
AdvVisFacetScaleRatio()
Returns: Return type: float New in version NX8.0.0.
Deprecated since version NX9.0.0: Refer to
Display.FacetSettingsBuilder.AdvVisRefinementFactor
insteadLicense requirements: None.
-------------------------------------
Setter Method
Signature
AdvVisFacetScaleRatio(advVisViewFacetScaleRatio)
Parameters: advVisViewFacetScaleRatio (float) – New in version NX8.0.0.
Deprecated since version NX9.0.0: Refer to
Display.FacetSettingsBuilder.AdvVisRefinementFactor
insteadLicense requirements: None.
AdvVisFacetToViewScale¶
-
PartVisualizationShade.
AdvVisFacetToViewScale
¶ Returns or sets whether the facet to view scale for Advanced Visualization views should be computed automatically or should be defined by the user
-------------------------------------
Getter Method
Signature
AdvVisFacetToViewScale()
Returns: Return type: bool New in version NX8.0.0.
Deprecated since version NX9.0.0: Refer to
Display.FacetSettingsBuilder.AdvVisFacetScale
insteadLicense requirements: None.
-------------------------------------
Setter Method
Signature
AdvVisFacetToViewScale(advVisViewFacetToViewScale)
Parameters: advVisViewFacetToViewScale (bool) – New in version NX8.0.0.
Deprecated since version NX9.0.0: Refer to
Display.FacetSettingsBuilder.AdvVisFacetScale
insteadLicense requirements: None.
AdvancedVisViewAngleTolerance¶
-
PartVisualizationShade.
AdvancedVisViewAngleTolerance
¶ Returns or sets the angle tolerance for advanced visualization views.
-------------------------------------
Getter Method
Signature
AdvancedVisViewAngleTolerance()
Returns: Return type: float New in version NX3.0.0.
Deprecated since version NX8.0.0: Use
NXOpen.Preferences.PartVisualizationShade.GetAdvVisViewFacetTolerances
andNXOpen.Preferences.PartVisualizationShade.SetAdvVisViewFacetTolerances
instead.License requirements: None.
-------------------------------------
Setter Method
Signature
AdvancedVisViewAngleTolerance(advancedVisViewAngleTolerance)
Parameters: advancedVisViewAngleTolerance (float) – New in version NX3.0.0.
Deprecated since version NX8.0.0: Use
NXOpen.Preferences.PartVisualizationShade.GetAdvVisViewFacetTolerances
andNXOpen.Preferences.PartVisualizationShade.SetAdvVisViewFacetTolerances
instead.License requirements: None.
AdvancedVisViewEdgeTolerance¶
-
PartVisualizationShade.
AdvancedVisViewEdgeTolerance
¶ Returns or sets the edge tolerance for advanced visualization views.
-------------------------------------
Getter Method
Signature
AdvancedVisViewEdgeTolerance()
Returns: Return type: float New in version NX3.0.0.
Deprecated since version NX8.0.0: Use
NXOpen.Preferences.PartVisualizationShade.GetAdvVisViewFacetTolerances
andNXOpen.Preferences.PartVisualizationShade.SetAdvVisViewFacetTolerances
instead.License requirements: None.
-------------------------------------
Setter Method
Signature
AdvancedVisViewEdgeTolerance(advancedVisViewEdgeTolerance)
Parameters: advancedVisViewEdgeTolerance (float) – New in version NX3.0.0.
Deprecated since version NX8.0.0: Use
NXOpen.Preferences.PartVisualizationShade.GetAdvVisViewFacetTolerances
andNXOpen.Preferences.PartVisualizationShade.SetAdvVisViewFacetTolerances
instead.License requirements: None.
AdvancedVisViewFaceTolerance¶
-
PartVisualizationShade.
AdvancedVisViewFaceTolerance
¶ Returns or sets the face tolerance for advanced visualization views.
-------------------------------------
Getter Method
Signature
AdvancedVisViewFaceTolerance()
Returns: Return type: float New in version NX3.0.0.
Deprecated since version NX8.0.0: Use
NXOpen.Preferences.PartVisualizationShade.GetAdvVisViewFacetTolerances
andNXOpen.Preferences.PartVisualizationShade.SetAdvVisViewFacetTolerances
instead.License requirements: None.
-------------------------------------
Setter Method
Signature
AdvancedVisViewFaceTolerance(advancedVisViewFaceTolerance)
Parameters: advancedVisViewFaceTolerance (float) – New in version NX3.0.0.
Deprecated since version NX8.0.0: Use
NXOpen.Preferences.PartVisualizationShade.GetAdvVisViewFacetTolerances
andNXOpen.Preferences.PartVisualizationShade.SetAdvVisViewFacetTolerances
instead.License requirements: None.
AdvancedVisViewTolerance¶
-
PartVisualizationShade.
AdvancedVisViewTolerance
¶ Returns or sets the tolerance for advanced visualization views.
-------------------------------------
Getter Method
Signature
AdvancedVisViewTolerance()
Returns: Return type: NXOpen.Preferences.PartVisualizationShadeAdvViewToleranceType
New in version NX3.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
AdvancedVisViewTolerance(advancedVisViewTolerance)
Parameters: advancedVisViewTolerance ( NXOpen.Preferences.PartVisualizationShadeAdvViewToleranceType
) –New in version NX3.0.0.
License requirements: None.
AdvancedVisViewUpdateMode¶
-
PartVisualizationShade.
AdvancedVisViewUpdateMode
¶ Returns or sets the update mode for advanced visualization views.
-------------------------------------
Getter Method
Signature
AdvancedVisViewUpdateMode()
Returns: Return type: NXOpen.Preferences.PartVisualizationShadeViewUpdateModeType
New in version NX3.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
AdvancedVisViewUpdateMode(advancedVisViewUpdateMode)
Parameters: advancedVisViewUpdateMode ( NXOpen.Preferences.PartVisualizationShadeViewUpdateModeType
) –New in version NX3.0.0.
License requirements: None.
AdvancedVisViewWidthTolerance¶
-
PartVisualizationShade.
AdvancedVisViewWidthTolerance
¶ Returns or sets the width tolerance for advanced Visualization Views.
-------------------------------------
Getter Method
Signature
AdvancedVisViewWidthTolerance()
Returns: Return type: float New in version NX3.0.0.
Deprecated since version NX8.0.0: Use
NXOpen.Preferences.PartVisualizationShade.GetAdvVisViewFacetTolerances
andNXOpen.Preferences.PartVisualizationShade.SetAdvVisViewFacetTolerances
instead.License requirements: None.
-------------------------------------
Setter Method
Signature
AdvancedVisViewWidthTolerance(advancedVisViewWidthTolerance)
Parameters: advancedVisViewWidthTolerance (float) – New in version NX3.0.0.
Deprecated since version NX8.0.0: Use
NXOpen.Preferences.PartVisualizationShade.GetAdvVisViewFacetTolerances
andNXOpen.Preferences.PartVisualizationShade.SetAdvVisViewFacetTolerances
instead.License requirements: None.
AlignAdvVisViewFacetsAlongEdges¶
-
PartVisualizationShade.
AlignAdvVisViewFacetsAlongEdges
¶ Returns or sets the state of whether facets should be aligned along common edges for Advanced Visualization Views
-------------------------------------
Getter Method
Signature
AlignAdvVisViewFacetsAlongEdges()
Returns: Return type: bool New in version NX8.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
AlignAdvVisViewFacetsAlongEdges(alignAdvVisViewFacetsAlongEdges)
Parameters: alignAdvVisViewFacetsAlongEdges (bool) – New in version NX8.5.0.
License requirements: None.
AlignShadedViewFacetsAlongEdges¶
-
PartVisualizationShade.
AlignShadedViewFacetsAlongEdges
¶ Returns or sets the state of whether facets should be aligned along common edges for Shaded Views
-------------------------------------
Getter Method
Signature
AlignShadedViewFacetsAlongEdges()
Returns: Return type: bool New in version NX8.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
AlignShadedViewFacetsAlongEdges(alignShadedViewFacetsAlongEdges)
Parameters: alignShadedViewFacetsAlongEdges (bool) – New in version NX8.5.0.
License requirements: None.
ShadedFacetScaleRatio¶
-
PartVisualizationShade.
ShadedFacetScaleRatio
¶ Returns or sets the facet to view scale ratio for Shaded views as specified by the user
-------------------------------------
Getter Method
Signature
ShadedFacetScaleRatio()
Returns: Return type: float New in version NX8.0.0.
Deprecated since version NX9.0.0: Refer to
Display.FacetSettingsBuilder.ShadedRefinementFactor
insteadLicense requirements: None.
-------------------------------------
Setter Method
Signature
ShadedFacetScaleRatio(shadedViewFacetScaleRatio)
Parameters: shadedViewFacetScaleRatio (float) – New in version NX8.0.0.
Deprecated since version NX9.0.0: Refer to
Display.FacetSettingsBuilder.ShadedRefinementFactor
insteadLicense requirements: None.
ShadedFacetToViewScale¶
-
PartVisualizationShade.
ShadedFacetToViewScale
¶ Returns or sets whether the facet to view scale for Shaded views should be computed automatically or should be defined by the user
-------------------------------------
Getter Method
Signature
ShadedFacetToViewScale()
Returns: Return type: bool New in version NX8.0.0.
Deprecated since version NX9.0.0: Refer to
Display.FacetSettingsBuilder.ShadedFacetScale
insteadLicense requirements: None.
-------------------------------------
Setter Method
Signature
ShadedFacetToViewScale(shadedViewFacetToViewScale)
Parameters: shadedViewFacetToViewScale (bool) – New in version NX8.0.0.
Deprecated since version NX9.0.0: Refer to
Display.FacetSettingsBuilder.ShadedFacetScale
insteadLicense requirements: None.
ShadedViewAngleTolerance¶
-
PartVisualizationShade.
ShadedViewAngleTolerance
¶ Returns or sets the angle tolerance for shaded views.
-------------------------------------
Getter Method
Signature
ShadedViewAngleTolerance()
Returns: Return type: float New in version NX3.0.0.
Deprecated since version NX8.0.0: Use
NXOpen.Preferences.PartVisualizationShade.GetShadedViewFacetTolerances
andNXOpen.Preferences.PartVisualizationShade.SetShadedViewFacetTolerances
instead.License requirements: None.
-------------------------------------
Setter Method
Signature
ShadedViewAngleTolerance(shadedViewAngleTolerance)
Parameters: shadedViewAngleTolerance (float) – New in version NX3.0.0.
Deprecated since version NX8.0.0: Use
NXOpen.Preferences.PartVisualizationShade.GetShadedViewFacetTolerances
andNXOpen.Preferences.PartVisualizationShade.SetShadedViewFacetTolerances
instead.License requirements: None.
ShadedViewEdgeTolerance¶
-
PartVisualizationShade.
ShadedViewEdgeTolerance
¶ Returns or sets the edge tolerance for shaded views.
-------------------------------------
Getter Method
Signature
ShadedViewEdgeTolerance()
Returns: Return type: float New in version NX3.0.0.
Deprecated since version NX8.0.0: Use
NXOpen.Preferences.PartVisualizationShade.GetShadedViewFacetTolerances
andNXOpen.Preferences.PartVisualizationShade.SetShadedViewFacetTolerances
instead.License requirements: None.
-------------------------------------
Setter Method
Signature
ShadedViewEdgeTolerance(shadedViewEdgeTolerance)
Parameters: shadedViewEdgeTolerance (float) – New in version NX3.0.0.
Deprecated since version NX8.0.0: Use
NXOpen.Preferences.PartVisualizationShade.GetShadedViewFacetTolerances
andNXOpen.Preferences.PartVisualizationShade.SetShadedViewFacetTolerances
instead.License requirements: None.
ShadedViewFaceTolerance¶
-
PartVisualizationShade.
ShadedViewFaceTolerance
¶ Returns or sets the face tolerance for shaded views.
-------------------------------------
Getter Method
Signature
ShadedViewFaceTolerance()
Returns: Return type: float New in version NX3.0.0.
Deprecated since version NX8.0.0: Use
NXOpen.Preferences.PartVisualizationShade.GetShadedViewFacetTolerances
andNXOpen.Preferences.PartVisualizationShade.SetShadedViewFacetTolerances
instead.License requirements: None.
-------------------------------------
Setter Method
Signature
ShadedViewFaceTolerance(shadedViewFaceTolerance)
Parameters: shadedViewFaceTolerance (float) – New in version NX3.0.0.
Deprecated since version NX8.0.0: Use
NXOpen.Preferences.PartVisualizationShade.GetShadedViewFacetTolerances
andNXOpen.Preferences.PartVisualizationShade.SetShadedViewFacetTolerances
instead.License requirements: None.
ShadedViewTolerance¶
-
PartVisualizationShade.
ShadedViewTolerance
¶ Returns or sets the tolerance for shaded views.
-------------------------------------
Getter Method
Signature
ShadedViewTolerance()
Returns: Return type: NXOpen.Preferences.PartVisualizationShadeShadedViewToleranceType
New in version NX3.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ShadedViewTolerance(shadedViewTolerance)
Parameters: shadedViewTolerance ( NXOpen.Preferences.PartVisualizationShadeShadedViewToleranceType
) –New in version NX3.0.0.
License requirements: None.
ShadedViewUpdateMode¶
-
PartVisualizationShade.
ShadedViewUpdateMode
¶ Returns or sets the update mode for shaded views.
-------------------------------------
Getter Method
Signature
ShadedViewUpdateMode()
Returns: Return type: NXOpen.Preferences.PartVisualizationShadeViewUpdateModeType
New in version NX3.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ShadedViewUpdateMode(shadedViewUpdateMode)
Parameters: shadedViewUpdateMode ( NXOpen.Preferences.PartVisualizationShadeViewUpdateModeType
) –New in version NX3.0.0.
License requirements: None.
Method Detail¶
GetAdvVisViewFacetTolerances¶
-
PartVisualizationShade.
GetAdvVisViewFacetTolerances
¶ Returns the edge, face, angle and width tolerances to be used with the specified tolerance set for Advanced Visualization views.
Signature
GetAdvVisViewFacetTolerances(advVisViewToleranceSet)
Parameters: advVisViewToleranceSet ( NXOpen.Preferences.PartVisualizationShadeAdvViewToleranceType
) –Returns: a tuple Return type: A tuple consisting of (edgeTolerance, faceTolerance, angleTolerance, widthTolerance). edgeTolerance is a float. faceTolerance is a float. angleTolerance is a float. widthTolerance is a float. New in version NX8.0.0.
License requirements: None.
GetShadedViewFacetTolerances¶
-
PartVisualizationShade.
GetShadedViewFacetTolerances
¶ Returns the edge, face and angle tolerances to be used with the specified tolerance set for shaded views.
Signature
GetShadedViewFacetTolerances(shadedViewToleranceSet)
Parameters: shadedViewToleranceSet ( NXOpen.Preferences.PartVisualizationShadeShadedViewToleranceType
) –Returns: a tuple Return type: A tuple consisting of (edgeTolerance, faceTolerance, angleTolerance). edgeTolerance is a float. faceTolerance is a float. angleTolerance is a float. New in version NX8.0.0.
License requirements: None.
SetAdvVisViewFacetTolerances¶
-
PartVisualizationShade.
SetAdvVisViewFacetTolerances
¶ Sets the edge, face, angle and width tolerances to be used with the specified tolerance set for Advanced Visualization views.
Signature
SetAdvVisViewFacetTolerances(advVisViewToleranceSet, edgeTolerance, faceTolerance, angleTolerance, widthTolerance)
Parameters: - advVisViewToleranceSet (
NXOpen.Preferences.PartVisualizationShadeAdvViewToleranceType
) – - edgeTolerance (float) –
- faceTolerance (float) –
- angleTolerance (float) –
- widthTolerance (float) –
New in version NX8.0.0.
License requirements: None.
- advVisViewToleranceSet (
SetShadedViewFacetTolerances¶
-
PartVisualizationShade.
SetShadedViewFacetTolerances
¶ Sets the edge, face and angle tolerances to be used with the specified tolerance set for shaded views.
Signature
SetShadedViewFacetTolerances(shadedViewToleranceSet, edgeTolerance, faceTolerance, angleTolerance)
Parameters: - shadedViewToleranceSet (
NXOpen.Preferences.PartVisualizationShadeShadedViewToleranceType
) – - edgeTolerance (float) –
- faceTolerance (float) –
- angleTolerance (float) –
New in version NX8.0.0.
License requirements: None.
- shadedViewToleranceSet (