PartVisualizationShadeShadedFaceEdge Enumeration¶
NXOpen.Preferences.PartVisualizationShade.ShadedFaceEdge is an alias for NXOpen.Preferences.PartVisualizationShadeShadedFaceEdge
-
class
NXOpen.Preferences.
PartVisualizationShadeShadedFaceEdge
¶ Bases:
object
Describes whether the shaded face edges are having no color or body color or user defined color.
Enum Members
Enum Member Enum Member Description Off Option is offBodyColor Body ColorSpecifyColor Specified Color-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-