PartVisualizationShadeShadedViewToleranceType Enumeration¶
NXOpen.Preferences.PartVisualizationShade.ShadedViewToleranceType is an alias for NXOpen.Preferences.PartVisualizationShadeShadedViewToleranceType
-
class
NXOpen.Preferences.
PartVisualizationShadeShadedViewToleranceType
¶ Bases:
object
Describes the available tolerance types for Shaded View.
Each of these options maps tolerance values to three specific faceting operations: Facet Edge Tolerance, Facet Chord Tolerance, and Angular Tolerance.
Enum Members
- Chord Tolerance is 0.01, and Angular Tolerance is 0.0 “
- “Standard”, ” For Standard: Facet Edge Tolerance is 0.005, Facet
- Chord Tolerance is 0.005 , and Angular Tolerance is 15 “
- “Fine”, ” For Fine: Facet Edge Tolerance is 0.0005, Facet
- Chord Tolerance is 0.0025, and Angular Tolerance is 6 “
- “Extrafine”, ” For Extrafine: Facet Edge Tolerance is 0.005, Facet
- Chord Tolerance is 0.001, and Angular Tolerance is 6 “
- “Ultrafine”, ” For Ultrafine: Facet Edge Tolerance is 0.0005, Facet
- Chord Tolerance is 0.0005, and Angular Tolerance is 3 “
- “Customize”, ” Customize. User can specify the Edge Tolerance,
Face Tolerance and Angle Tolerance specifically. “
-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.