PartVisualizationShadeHiddenShadedFaceEdges Enumeration¶
NXOpen.Preferences.PartVisualizationShade.HiddenShadedFaceEdges is an alias for NXOpen.Preferences.PartVisualizationShadeHiddenShadedFaceEdges
-
class
NXOpen.Preferences.
PartVisualizationShadeHiddenShadedFaceEdges
¶ Bases:
object
Describes whether the shaded face edges are invisible or dashed visible or with a color to depict the hidden geometry
Enum Members
- hidden are not displayed “
- “Dashed”, ” If selected, hidden shaded face edges are
displayed in the body color with a dashed line font. “
“HiddenColor”, ” If any color is selected, hidden shaded faceedges are displayed in that color.”
-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.