LayerManager Class¶
-
class
NXOpen.Layer.
LayerManager
¶ Bases:
object
Represents an object that manages layers
To obtain an instance of this class, refer to
NXOpen.BasePart
New in version NX3.0.0.
Methods¶
Method | Description |
---|---|
ApplyMoveToLayerToOwningParts | Move the selected objects to the specified layer in their Owning Parts. |
ChangeStates | Changes the states of the specified layers in the part. |
CopyObjects | Copies objects to the specified layer |
GetAllObjectsOnLayer | Returns all objects on the specified layer. |
GetState | Gets the state of the specified layer. |
GetStates | Gets the states for all layers in the part. |
GetVisibilitiesInView | Gets the visibility of all layers in a specified view. |
MoveDisplayableObjects | Moves displayable objects to the specified layer. |
ResetViewVisibilityToGlobal | Resets a view’s layer visibility to the global states. |
SetObjectsVisibilityOnLayer | Sets specified layer(s) visibility in a specified view. |
SetState | Sets the state of the specified layer. |
SetStates | Sets the states for all layers in the part. |
Property Detail¶
WorkLayer¶
-
LayerManager.
WorkLayer
¶ Returns or sets the work layer.
If you change the work layer, the old work layer is changed to Selectable. The part must be the displayed part.
-------------------------------------
Getter Method
Signature
WorkLayer()
Returns: Layer number of the work layer Return type: int New in version NX3.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
WorkLayer(newWorkLayer)
Parameters: newWorkLayer (int) – Layer number for the new work layer New in version NX3.0.0.
License requirements: None.
Method Detail¶
ApplyMoveToLayerToOwningParts¶
-
LayerManager.
ApplyMoveToLayerToOwningParts
¶ Move the selected objects to the specified layer in their Owning Parts.
This only works when a single layer has been selected on the Layer Settings dialog.
The owning parts will be fully loaded if they are not already.
Objects of class
NXOpen.CAE.CAEEdge
,NXOpen.CAE.CAEFace
,NXOpen.CAE.CAEVertex
,NXOpen.Edge
,NXOpen.Face
orNXOpen.View
may not be moved.Signature
ApplyMoveToLayerToOwningParts(newLayer, objectArray)
Parameters: - newLayer (int) – The layer in the owning parts to move the objects to
- objectArray (list of
NXOpen.DisplayableObject
) – The objects to be moved
New in version NX7.5.0.
License requirements: solid_modeling (“SOLIDS MODELING”) OR drafting (“DRAFTING”)
ChangeStates¶
-
LayerManager.
ChangeStates
¶ Overloaded method ChangeStates
ChangeStates(stateArray, fitAll)
ChangeStates(stateArray)
-------------------------------------
Changes the states of the specified layers in the part. Note: there must be exactly one work layer. If you change the work layer, you must specify a new work layer. If you set the work layer, the old work layer will be changed to Selectable, unless you specify otherwise. The part must be the displayed part.
Signature
ChangeStates(stateArray, fitAll)
Parameters: - stateArray (list of
NXOpen.Layer.StateInfo
) – Indicates the new states for the layers. - fitAll (bool) – Whether to refit the view to what is visible after the layer states have been changed
New in version NX3.0.0.
License requirements: None.
-------------------------------------
Changes the states of the specified layers in the part. Note: there must be exactly one work layer. If you change the work layer, you must specify a new work layer. If you set the work layer, the old work layer will be changed to Selectable, unless you specify otherwise. The part must be the displayed part.
Signature
ChangeStates(stateArray)
Parameters: stateArray (list of NXOpen.Layer.StateInfo
) – Indicates the new states for the layers.New in version NX3.0.0.
License requirements: None.
-------------------------------------
CopyObjects¶
-
LayerManager.
CopyObjects
¶ Copies objects to the specified layer
Objects of class
NXOpen.Assemblies.Component
,NXOpen.DatumAxis
,NXOpen.DatumPlane
NXOpen.Edge
,NXOpen.Face
,NXOpen.Features.Feature
orNXOpen.View
, may not be copied.Objects of type UF_cs2_vertex_type may not be copied.
The part must be the work part.
Signature
CopyObjects(newLayer, objectArray)
Parameters: - newLayer (int) – The layer to move the objects to
- objectArray (list of
NXOpen.NXObject
) – The objects to be copied
New in version NX4.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”) OR drafting (“DRAFTING”)
GetAllObjectsOnLayer¶
-
LayerManager.
GetAllObjectsOnLayer
¶ Returns all objects on the specified layer.
The part must be the displayed part.
Signature
GetAllObjectsOnLayer(layer)
Parameters: layer (int) – Returns: All the objects on the specified layer Return type: list of NXOpen.NXObject
New in version NX3.0.0.
License requirements: None.
GetState¶
-
LayerManager.
GetState
¶ Gets the state of the specified layer.
The part must be the displayed part.
Signature
GetState(layer)
Parameters: layer (int) – Returns: Return type: NXOpen.Layer.State
New in version NX3.0.0.
License requirements: None.
GetStates¶
-
LayerManager.
GetStates
¶ Gets the states for all layers in the part.
The part must be the displayed part.
Signature
GetStates()
Returns: Indicates the states for all layers in the part. Return type: NXOpen.Layer.StateCollection
New in version NX3.0.0.
License requirements: None.
GetVisibilitiesInView¶
-
LayerManager.
GetVisibilitiesInView
¶ Gets the visibility of all layers in a specified view.
The part must be the displayed part.
Signature
GetVisibilitiesInView(view)
Parameters: view ( NXOpen.View
) – The view object being queriedReturns: The current states for the layers. The returned states can only be
LayerState.Visible
andLayerState.Hidden
. state_array[i] is for layer i+1 :rtype: list ofNXOpen.Layer.StateInfo
New in version NX4.0.3.
License requirements: None.
MoveDisplayableObjects¶
-
LayerManager.
MoveDisplayableObjects
¶ Moves displayable objects to the specified layer.
The specified part may be the displayed part or the work part. If it is the work part but not the displayed part, then none of the objects to be moved may be currently displayed.
This method is the preferred way to change the layer of one or more objects, because
NXOpen.DisplayableObject.Layer
does not correct the display of the objects and does not work as expected for sketches and components, because it does not move the members of the sketch or component.Objects of class
NXOpen.CAE.CAEEdge
,NXOpen.CAE.CAEFace
,NXOpen.CAE.CAEVertex
,NXOpen.Edge
,NXOpen.Face
orNXOpen.View
may not be moved.Signature
MoveDisplayableObjects(newLayer, objectArray)
Parameters: - newLayer (int) – The layer to move the objects to
- objectArray (list of
NXOpen.DisplayableObject
) – The objects to be moved
New in version NX5.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”) OR drafting (“DRAFTING”)
ResetViewVisibilityToGlobal¶
-
LayerManager.
ResetViewVisibilityToGlobal
¶ Resets a view’s layer visibility to the global states.
The part must be the displayed part.
Signature
ResetViewVisibilityToGlobal(view)
Parameters: view ( NXOpen.View
) – The view objectNew in version NX4.0.0.
License requirements: None.
SetObjectsVisibilityOnLayer¶
-
LayerManager.
SetObjectsVisibilityOnLayer
¶ Sets specified layer(s) visibility in a specified view.
The part must be the displayed part.
Signature
SetObjectsVisibilityOnLayer(view, stateArray, doUpdate)
Parameters: - view (
NXOpen.View
) – The view object being modified - stateArray (list of
NXOpen.Layer.StateInfo
) – The new states for the layers. The given states may only beLayerState.Visible
andLayerState.Hidden
. - doUpdate (bool) – Whether to update the view(s) after the layer states have been changed
New in version NX4.0.0.
License requirements: None.
- view (
SetState¶
-
LayerManager.
SetState
¶ Overloaded method SetState
SetState(layer, state)
SetState(layer, state, fitAll)
-------------------------------------
Sets the state of the specified layer. The specified layer must not be the work layer. If you are changing the state of the layer to Work, the old work layer will be changed to Selectable. The part must be the displayed part.
Signature
SetState(layer, state)
Parameters: - layer (int) –
- state (
NXOpen.Layer.State
) –
New in version NX3.0.0.
License requirements: None.
-------------------------------------
Sets the state of the specified layer. The specified layer must not be the work layer. If you are changing the state of the layer to Work, the old work layer will be changed to Selectable. The part must be the displayed part.
Signature
SetState(layer, state, fitAll)
Parameters: - layer (int) –
- state (
NXOpen.Layer.State
) – - fitAll (bool) – Whether to refit the view to what is visible after the layer state has been changed
New in version NX3.0.0.
License requirements: None.
-------------------------------------
SetStates¶
-
LayerManager.
SetStates
¶ Overloaded method SetStates
SetStates(stateCollection, fitAll)
SetStates(stateCollection)
-------------------------------------
Sets the states for all layers in the part. The part must be the displayed part. Note: there must be exactly one work layer.
Signature
SetStates(stateCollection, fitAll)
Parameters: - stateCollection (
NXOpen.Layer.StateCollection
) – The states for all layers in the part. - fitAll (bool) – Whether to refit the view to what is visible after the layer states have been changed
New in version NX3.0.0.
License requirements: None.
-------------------------------------
Sets the states for all layers in the part. The part must be the displayed part. Note: there must be exactly one work layer.
Signature
SetStates(stateCollection)
Parameters: stateCollection ( NXOpen.Layer.StateCollection
) – The states for all layers in the part.New in version NX3.0.0.
License requirements: None.
-------------------------------------