StateInfo Struct¶
-
class
NXOpen.Layer.
StateInfo
¶ Bases:
object
Used in several methods that get or set the state of a layer
Fields¶
Field | Description |
---|---|
Layer | Layer number |
State | The state of the layer |
Layer¶
-
StateInfo.
Layer
¶ Layer number
-------------------------------------
Getter Method Signature
Layer()
Returns: Return type: int -------------------------------------
Setter Method
Signature
Layer(value)
Parameters: value (int) –
State¶
-
StateInfo.
State
¶ The state of the layer
-------------------------------------
Getter Method Signature
State()
Returns: Return type: NXOpen.Layer.State
-------------------------------------
Setter Method
Signature
State(value)
Parameters: value ( NXOpen.Layer.State
) –