NXOpen.Formboard Package¶
Classes¶
NXOpen.Formboard.FaceAnnotationBuilder |
Builder for Face Annotation functionality used in formboard. |
NXOpen.Formboard.FlipComponentBuilder |
Builder for flip component operation used in formboard. |
NXOpen.Formboard.FormboardLayoutBuilder |
Class that performs the “layout” of Formboard geometry. |
NXOpen.Formboard.FormboardManager |
Contains information about flattened harness drawing and drafting data for harness manufacturing drawings (Formboard Drawings). |
NXOpen.Formboard.LayoutLengthOptions |
Defines the various options for determining the rounded lengths of formboard geometry during the layout or update process. |
NXOpen.Formboard.ObjectAttributeReferenceBuilder |
Builder for “object attribute” used in formboard which enbles user to create annotation in drafting functionality. |
NXOpen.Formboard.OrientBranchBuilder |
Builder for “Orient Branch” operation used in formboard. |
NXOpen.Formboard.PathLengthAnnotationBuilder |
TODO Class documentation |
NXOpen.Formboard.ShapeSegmentBuilder |
Builder for Face Annotation functionality used in formboard. |
NXOpen.Formboard.UpdateDiscrepancy |
Defines a discrepancy object which contains information about a specific difference between the formboard drawing and the 3D harness model. |
NXOpen.Formboard.UpdateFormboardBuilder |
Class that performs the “update” of Formboard geometry. |
Enumerations¶
FaceAnnotationBuilderDrwDestination Enumeration | Enum which defines where the geometry is to be placed. |
FaceAnnotationBuilderTypes Enumeration | Enum which defines the type to import CGM/Pattern file |
FlipComponentBuilderAxisType Enumeration | Enum for the selection of axis type for flipping formboard component |
FormboardLayoutBuilderBranchAngle Enumeration | Methods for determining which angles to apply at each branch of the Formboard. |
FormboardLayoutBuilderBranchShape Enumeration | Shape option for the branches. |
FormboardLayoutBuilderMainRunType Enumeration | Selection method for the set of segments that define the main run of the formboard geometry. |
LayoutLengthOptionsRoundingMethod Enumeration | Methods of rounding lengths for Formboard geometry. |
ObjectAttributeReferenceBuilderLeaderType Enumeration | Enum which defines types of leader user wants to associate with the annotation. |
OrientBranchBuilderBranchAngleMethod Enumeration | Enum to define the type of method to orient branch. |
PathLengthAnnotationBuilderTypes Enumeration | TODO: Document the whole type |
UpdateDiscrepancyObjectType Enumeration | Specifies the type of objects involved in the discrepancy. |
UpdateDiscrepancyType Enumeration | The general type of the discrepancy. |