ObjectAttributeReferenceBuilderLeaderType Enumeration¶
NXOpen.Formboard.ObjectAttributeReferenceBuilder.LeaderType is an alias for NXOpen.Formboard.ObjectAttributeReferenceBuilderLeaderType
-
class
NXOpen.Formboard.
ObjectAttributeReferenceBuilderLeaderType
¶ Bases:
object
Enum which defines types of leader user wants to associate with the annotation.
User can either create no leader or one or two leader for the annotation when picking the associated object.
Enum Members
Enum Member Enum Member Description None No leader for annotation of selected object.SingleLocation Single leader for the annotation of selected object.StartandEndLocations Two leaders for annotation with start and end location.-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-