OrientBranchBuilder Class¶
-
class
NXOpen.Formboard.
OrientBranchBuilder
¶ Bases:
NXOpen.Builder
Builder for “Orient Branch” operation used in formboard.
Allows user to orient the branch by different methods.
To create a new instance of this class, use
NXOpen.Formboard.FormboardManager.CreateOrientBranchBuilder
Default values.
Property Value BranchAngleType AnglefromReferenceVector RotationAngle.Value 0 New in version NX7.5.0.
Properties¶
Property | Description |
---|---|
BranchAngleType | Returns or sets the user selected NXOpen.Formboard.OrientBranchBuilderBranchAngleMethod |
FromPoint | Returns or sets the user selected from point when NXOpen.Formboard.OrientBranchBuilderBranchAngleMethod is :py:class:` NXOpen.Formboard.OrientBranchBuilderBranchAngleMethod.TwoPoints < NXOpen.Formboard.OrientBranchBuilderBranchAngleMethod>`. |
FromVector | Returns or sets the user selected from vector when NXOpen.Formboard.OrientBranchBuilderBranchAngleMethod is :py:class:` NXOpen.Formboard.OrientBranchBuilderBranchAngleMethod.AlignAxisToVector < NXOpen.Formboard.OrientBranchBuilderBranchAngleMethod>`. |
RefRotationAngle | Returns the angle for the rotation of branch when NXOpen.Formboard.OrientBranchBuilderBranchAngleMethod is :py:class:` NXOpen.Formboard.OrientBranchBuilderBranchAngleMethod.AnglefromReferenceVector < NXOpen.Formboard.OrientBranchBuilderBranchAngleMethod>`. |
ReferenceVector | Returns or sets the user selected reference vector when NXOpen.Formboard.OrientBranchBuilderBranchAngleMethod is :py:class:` NXOpen.Formboard.OrientBranchBuilderBranchAngleMethod.AnglefromReferenceVector < NXOpen.Formboard.OrientBranchBuilderBranchAngleMethod>`. |
RotationAngle | Returns the angle for the rotation of branch when NXOpen.Formboard.OrientBranchBuilderBranchAngleMethod is :py:class:` NXOpen.Formboard.OrientBranchBuilderBranchAngleMethod.Angle < NXOpen.Formboard.OrientBranchBuilderBranchAngleMethod>`. |
SelectBranch | Returns the user selected branch NXOpen.Routing.ISegment for rotation. |
Tag | Returns the Tag for this object. |
ToPoint | Returns or sets the user selected to point when NXOpen.Formboard.OrientBranchBuilderBranchAngleMethod is :py:class:` NXOpen.Formboard.OrientBranchBuilderBranchAngleMethod.TwoPoints < NXOpen.Formboard.OrientBranchBuilderBranchAngleMethod>`. |
ToVector | Returns or sets the user selected to vector when NXOpen.Formboard.OrientBranchBuilderBranchAngleMethod is :py:class:` NXOpen.Formboard.OrientBranchBuilderBranchAngleMethod.AlignAxisToVector < NXOpen.Formboard.OrientBranchBuilderBranchAngleMethod>`. |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetObject | Returns the object currently being edited by this builder. |
InitializeFromSegment | Initializes or resets ( start or stop ) drag operation based on the input branch segment. |
SetBranchSeedObject | Sets the selected branch NXOpen.Routing.ISegment when a branch is selected by branch method by Routing Object Collector. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
StartDrag | Starts the drag operation of selected object. |
StopDrag | Stop the drag operation of selected object. |
UnSuppressConstraints | Suppress the NXOpen.Positioning.Constraint associated with selected branch NXOpen.Routing.ISegment when a branch is selected by branch method by Routing Object Collector. |
UpdateRotationAngle | Rotates the branch by an appropriate rotation and transformation which depends on the NXOpen.Formboard.OrientBranchBuilderBranchAngleMethod selected by user. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Enumerations¶
OrientBranchBuilderBranchAngleMethod Enumeration | Enum to define the type of method to orient branch. |
Property Detail¶
BranchAngleType¶
-
OrientBranchBuilder.
BranchAngleType
¶ Returns or sets the user selected
NXOpen.Formboard.OrientBranchBuilderBranchAngleMethod
-------------------------------------
Getter Method
Signature
BranchAngleType()
Returns: Return type: NXOpen.Formboard.OrientBranchBuilderBranchAngleMethod
New in version NX7.5.0.
License requirements: routing_harness (“Routing Harness”)
-------------------------------------
Setter Method
Signature
BranchAngleType(branchAngleType)
Parameters: branchAngleType ( NXOpen.Formboard.OrientBranchBuilderBranchAngleMethod
) –New in version NX7.5.0.
License requirements: routing_harness (“Routing Harness”)
FromPoint¶
-
OrientBranchBuilder.
FromPoint
¶ Returns or sets the user selected from point when
NXOpen.Formboard.OrientBranchBuilderBranchAngleMethod
is :py:class:` NXOpen.Formboard.OrientBranchBuilderBranchAngleMethod.TwoPoints < NXOpen.Formboard.OrientBranchBuilderBranchAngleMethod>`.-------------------------------------
Getter Method
Signature
FromPoint()
Returns: Return type: NXOpen.Point
New in version NX7.5.0.
Deprecated since version NX8.5.0: This :py:class:` NXOpen.Formboard.OrientBranchBuilderBranchAngleMethod.TwoPoints < NXOpen.Formboard.OrientBranchBuilderBranchAngleMethod>` is no longer supported.
License requirements: routing_harness (“Routing Harness”)
-------------------------------------
Setter Method
Signature
FromPoint(fromPoint)
Parameters: fromPoint ( NXOpen.Point
) –New in version NX7.5.0.
Deprecated since version NX8.5.0: This :py:class:` NXOpen.Formboard.OrientBranchBuilderBranchAngleMethod.TwoPoints < NXOpen.Formboard.OrientBranchBuilderBranchAngleMethod>` is no longer supported.
License requirements: routing_harness (“Routing Harness”)
FromVector¶
-
OrientBranchBuilder.
FromVector
¶ Returns or sets the user selected from vector when
NXOpen.Formboard.OrientBranchBuilderBranchAngleMethod
is :py:class:` NXOpen.Formboard.OrientBranchBuilderBranchAngleMethod.AlignAxisToVector < NXOpen.Formboard.OrientBranchBuilderBranchAngleMethod>`.-------------------------------------
Getter Method
Signature
FromVector()
Returns: Return type: NXOpen.Direction
New in version NX7.5.0.
Deprecated since version NX8.5.0: This builder attribute is no longer required.
License requirements: routing_harness (“Routing Harness”)
-------------------------------------
Setter Method
Signature
FromVector(fromVector)
Parameters: fromVector ( NXOpen.Direction
) –New in version NX7.5.0.
Deprecated since version NX8.5.0: This builder attribute is no longer required.
License requirements: routing_harness (“Routing Harness”)
RefRotationAngle¶
-
OrientBranchBuilder.
RefRotationAngle
¶ Returns the angle for the rotation of branch when
NXOpen.Formboard.OrientBranchBuilderBranchAngleMethod
is :py:class:` NXOpen.Formboard.OrientBranchBuilderBranchAngleMethod.AnglefromReferenceVector < NXOpen.Formboard.OrientBranchBuilderBranchAngleMethod>`.-------------------------------------
Getter Method
Signature
RefRotationAngle()
Returns: Return type: NXOpen.Expression
New in version NX7.5.0.
License requirements: routing_harness (“Routing Harness”)
ReferenceVector¶
-
OrientBranchBuilder.
ReferenceVector
¶ Returns or sets the user selected reference vector when
NXOpen.Formboard.OrientBranchBuilderBranchAngleMethod
is :py:class:` NXOpen.Formboard.OrientBranchBuilderBranchAngleMethod.AnglefromReferenceVector < NXOpen.Formboard.OrientBranchBuilderBranchAngleMethod>`.-------------------------------------
Getter Method
Signature
ReferenceVector()
Returns: Return type: NXOpen.Direction
New in version NX7.5.0.
License requirements: routing_harness (“Routing Harness”)
-------------------------------------
Setter Method
Signature
ReferenceVector(referenceVector)
Parameters: referenceVector ( NXOpen.Direction
) –New in version NX7.5.0.
License requirements: routing_harness (“Routing Harness”)
RotationAngle¶
-
OrientBranchBuilder.
RotationAngle
¶ Returns the angle for the rotation of branch when
NXOpen.Formboard.OrientBranchBuilderBranchAngleMethod
is :py:class:` NXOpen.Formboard.OrientBranchBuilderBranchAngleMethod.Angle < NXOpen.Formboard.OrientBranchBuilderBranchAngleMethod>`.-------------------------------------
Getter Method
Signature
RotationAngle()
Returns: Return type: NXOpen.Expression
New in version NX7.5.0.
License requirements: routing_harness (“Routing Harness”)
SelectBranch¶
-
OrientBranchBuilder.
SelectBranch
¶ Returns the user selected branch
NXOpen.Routing.ISegment
for rotation.-------------------------------------
Getter Method
Signature
SelectBranch()
Returns: Return type: NXOpen.Routing.RouteObjectCollector
New in version NX7.5.0.
License requirements: routing_harness (“Routing Harness”)
ToPoint¶
-
OrientBranchBuilder.
ToPoint
¶ Returns or sets the user selected to point when
NXOpen.Formboard.OrientBranchBuilderBranchAngleMethod
is :py:class:` NXOpen.Formboard.OrientBranchBuilderBranchAngleMethod.TwoPoints < NXOpen.Formboard.OrientBranchBuilderBranchAngleMethod>`.-------------------------------------
Getter Method
Signature
ToPoint()
Returns: Return type: NXOpen.Point
New in version NX7.5.0.
Deprecated since version NX8.5.0: This :py:class:` NXOpen.Formboard.OrientBranchBuilderBranchAngleMethod.TwoPoints < NXOpen.Formboard.OrientBranchBuilderBranchAngleMethod>` is no longer supported.
License requirements: routing_harness (“Routing Harness”)
-------------------------------------
Setter Method
Signature
ToPoint(toPoint)
Parameters: toPoint ( NXOpen.Point
) –New in version NX7.5.0.
Deprecated since version NX8.5.0: This :py:class:` NXOpen.Formboard.OrientBranchBuilderBranchAngleMethod.TwoPoints < NXOpen.Formboard.OrientBranchBuilderBranchAngleMethod>` is no longer supported.
License requirements: routing_harness (“Routing Harness”)
ToVector¶
-
OrientBranchBuilder.
ToVector
¶ Returns or sets the user selected to vector when
NXOpen.Formboard.OrientBranchBuilderBranchAngleMethod
is :py:class:` NXOpen.Formboard.OrientBranchBuilderBranchAngleMethod.AlignAxisToVector < NXOpen.Formboard.OrientBranchBuilderBranchAngleMethod>`.-------------------------------------
Getter Method
Signature
ToVector()
Returns: Return type: NXOpen.Direction
New in version NX7.5.0.
License requirements: routing_harness (“Routing Harness”)
-------------------------------------
Setter Method
Signature
ToVector(toVector)
Parameters: toVector ( NXOpen.Direction
) –New in version NX7.5.0.
License requirements: routing_harness (“Routing Harness”)
Method Detail¶
InitializeFromSegment¶
-
OrientBranchBuilder.
InitializeFromSegment
¶ Initializes or resets ( start or stop ) drag operation based on the input branch segment.
Signature
InitializeFromSegment()
New in version NX7.5.0.
Deprecated since version NX9.0.1: This method is no longer required.
License requirements: routing_harness (“Routing Harness”)
SetBranchSeedObject¶
-
OrientBranchBuilder.
SetBranchSeedObject
¶ Sets the selected branch
NXOpen.Routing.ISegment
when a branch is selected by branch method by Routing Object Collector.Signature
SetBranchSeedObject(segmentTag)
Parameters: segmentTag ( NXOpen.Routing.ISegment
) – selected seed objectNew in version NX7.5.0.
License requirements: routing_harness (“Routing Harness”)
StartDrag¶
-
OrientBranchBuilder.
StartDrag
¶ Starts the drag operation of selected object.
Does nothing if drag has already been started.
Signature
StartDrag()
New in version NX7.5.0.
Deprecated since version NX9.0.1: This method is no longer required.
License requirements: routing_harness (“Routing Harness”)
StopDrag¶
-
OrientBranchBuilder.
StopDrag
¶ Stop the drag operation of selected object.
Does nothing if drag has not been started.
Signature
StopDrag()
New in version NX7.5.0.
Deprecated since version NX9.0.1: This method is no longer required.
License requirements: routing_harness (“Routing Harness”)
UnSuppressConstraints¶
-
OrientBranchBuilder.
UnSuppressConstraints
¶ Suppress the
NXOpen.Positioning.Constraint
associated with selected branchNXOpen.Routing.ISegment
when a branch is selected by branch method by Routing Object Collector.Signature
UnSuppressConstraints()
New in version NX7.5.3.
Deprecated since version NX7.5.3: This method is no longer relevant and calls to this can be safely removed.
License requirements: routing_harness (“Routing Harness”)
UpdateRotationAngle¶
-
OrientBranchBuilder.
UpdateRotationAngle
¶ Rotates the branch by an appropriate rotation and transformation which depends on the
NXOpen.Formboard.OrientBranchBuilderBranchAngleMethod
selected by user.Signature
UpdateRotationAngle(angle)
Parameters: angle (float) – angle for rotation New in version NX7.5.0.
Deprecated since version NX9.0.1: This method is no longer required.
License requirements: routing_harness (“Routing Harness”)
Validate¶
-
OrientBranchBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.