ShapeSegmentBuilder Class¶
-
class
NXOpen.Formboard.
ShapeSegmentBuilder
¶ Bases:
NXOpen.Builder
Builder for Face Annotation functionality used in formboard.
It allows importing CGM or Pattern file geometry and placing it on a drawing sheet or model view. As a result of this a group of dumb geometry is placed such that defined origin is located at the lower left hand of the bounding box containing the group of geometry.
To create a new instance of this class, use
NXOpen.Formboard.FormboardManager.CreateShapeSegmentBuilder
New in version NX7.5.0.
Methods¶
Method | Description |
---|---|
AddRadialPivot | |
AddSplinePoint | Adds a point to the existing spline. |
ChangeType | |
Commit | Commits any edits that have been applied to the builder. |
CommitCurrentOperation | |
CreateNewRadialBend | |
CreateNewSpline | |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetLineData | |
GetObject | Returns the object currently being edited by this builder. |
NewSegment | |
RemoveRadialPivot | |
RemoveSplinePoint | |
SetActiveView | Sets the active view for the shape operation. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
SwapAnchorEnd | |
UpdateLineAngleVec | |
UpdateRadialPivot | |
UpdateSplinePoint | |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Method Detail¶
AddRadialPivot¶
-
ShapeSegmentBuilder.
AddRadialPivot
¶ Signature
AddRadialPivot(pivotLocation, bendMethod, bendValue)
Parameters: - pivotLocation (
NXOpen.Point3d
) – - bendMethod (int) –
- bendValue (float) –
New in version NX7.5.0.
License requirements: routing_harness (“Routing Harness”)
- pivotLocation (
AddSplinePoint¶
-
ShapeSegmentBuilder.
AddSplinePoint
¶ Adds a point to the existing spline.
Signature
AddSplinePoint(pointLocation)
Parameters: pointLocation ( NXOpen.Point3d
) –Returns: Return type: int New in version NX7.5.0.
License requirements: routing_harness (“Routing Harness”)
ChangeType¶
-
ShapeSegmentBuilder.
ChangeType
¶ Signature
ChangeType(newType)
Parameters: newType (int) – New in version NX7.5.0.
License requirements: routing_harness (“Routing Harness”)
CommitCurrentOperation¶
-
ShapeSegmentBuilder.
CommitCurrentOperation
¶ Signature
CommitCurrentOperation()
New in version NX7.5.0.
License requirements: routing_harness (“Routing Harness”)
CreateNewRadialBend¶
-
ShapeSegmentBuilder.
CreateNewRadialBend
¶ Signature
CreateNewRadialBend(firstPivot, firstBendMethod, firstBendValue, secondPivot, secondBendMethod, secondBendValue)
Parameters: - firstPivot (
NXOpen.Point3d
) – - firstBendMethod (int) –
- firstBendValue (float) –
- secondPivot (
NXOpen.Point3d
) – - secondBendMethod (int) –
- secondBendValue (float) –
New in version NX7.5.0.
License requirements: routing_harness (“Routing Harness”)
- firstPivot (
CreateNewSpline¶
-
ShapeSegmentBuilder.
CreateNewSpline
¶ Signature
CreateNewSpline(anchorLocation, firstPoint, secondPoint)
Parameters: - anchorLocation (
NXOpen.Point3d
) – - firstPoint (
NXOpen.Point3d
) – - secondPoint (
NXOpen.Point3d
) –
New in version NX7.5.0.
License requirements: routing_harness (“Routing Harness”)
- anchorLocation (
GetLineData¶
-
ShapeSegmentBuilder.
GetLineData
¶ Signature
GetLineData()
Returns: a tuple Return type: A tuple consisting of (anchorSeg, anchorRcp, angle). anchorSeg is a NXOpen.Routing.ISegment
. anchorRcp is aNXOpen.Routing.ControlPoint
. angle is a float.New in version NX7.5.0.
License requirements: routing_harness (“Routing Harness”)
NewSegment¶
-
ShapeSegmentBuilder.
NewSegment
¶ Signature
NewSegment(newSegment)
Parameters: newSegment ( NXOpen.Routing.ISegment
) –New in version NX7.5.0.
License requirements: routing_harness (“Routing Harness”)
RemoveRadialPivot¶
-
ShapeSegmentBuilder.
RemoveRadialPivot
¶ Signature
RemoveRadialPivot(pivotIndex)
Parameters: pivotIndex (int) – New in version NX7.5.0.
License requirements: routing_harness (“Routing Harness”)
RemoveSplinePoint¶
-
ShapeSegmentBuilder.
RemoveSplinePoint
¶ Signature
RemoveSplinePoint(pointIndex)
Parameters: pointIndex (int) – New in version NX7.5.0.
License requirements: routing_harness (“Routing Harness”)
SetActiveView¶
-
ShapeSegmentBuilder.
SetActiveView
¶ Sets the active view for the shape operation.
Signature
SetActiveView(view)
Parameters: view ( NXOpen.TaggedObject
) –New in version NX7.5.0.
License requirements: routing_harness (“Routing Harness”)
SwapAnchorEnd¶
-
ShapeSegmentBuilder.
SwapAnchorEnd
¶ Signature
SwapAnchorEnd()
New in version NX7.5.0.
License requirements: routing_harness (“Routing Harness”)
UpdateLineAngleVec¶
-
ShapeSegmentBuilder.
UpdateLineAngleVec
¶ Signature
UpdateLineAngleVec(newDir)
Parameters: newDir ( NXOpen.Vector3d
) –New in version NX7.5.0.
License requirements: routing_harness (“Routing Harness”)
UpdateRadialPivot¶
-
ShapeSegmentBuilder.
UpdateRadialPivot
¶ Signature
UpdateRadialPivot(pivotIndex, newLocation, newBendMethod, newBendValue)
Parameters: - pivotIndex (int) –
- newLocation (
NXOpen.Point3d
) – - newBendMethod (int) –
- newBendValue (float) –
New in version NX7.5.0.
License requirements: routing_harness (“Routing Harness”)
UpdateSplinePoint¶
-
ShapeSegmentBuilder.
UpdateSplinePoint
¶ Signature
UpdateSplinePoint(pointIndex, pointLocation, inDrag)
Parameters: - pointIndex (int) –
- pointLocation (
NXOpen.Point3d
) – - inDrag (bool) –
New in version NX7.5.0.
License requirements: routing_harness (“Routing Harness”)
Validate¶
-
ShapeSegmentBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.