TextBuilder Class¶
-
class
NXOpen.Features.
TextBuilder
¶ Bases:
NXOpen.Features.FeatureBuilder
Represents a
NXOpen.Features.Text
builderTo create a new instance of this class, use
NXOpen.Features.FeatureCollection.CreateTextBuilder
Default values.
Property Value CanCreateBoundingBox 0 CanJoinCurves 1 CanProjectCurves 0 CanReferenceText 0 CanUseKerningSpaces 1 FontStyle Regular FrameOnPath.AnchorLocation Center FrameOnPath.Height.Value 10 (millimeters part), 1 (inches part) FrameOnPath.Offset.Value 0 (millimeters part), 0 (inches part) FrameOnPath.WScale 100 IsAssociative 1 OnFacePlacementMethod CurvesOnFaces OrientationMethod Natural PlanarFrame.AnchorLocation BottomCenter PlanarFrame.Height.Value 10 (millimeters part), 1 (inches part) PlanarFrame.Shear.Value 0 PlanarFrame.WScale 100 New in version NX7.5.1.
Properties¶
Property | Description |
---|---|
CanCreateBoundingBox | Returns or sets the flag indicating if bounding box can be created |
CanJoinCurves | Returns or sets the flag indicating if curves can be joined |
CanProjectCurves | Returns or sets the flag indicating if curves can be projected |
CanReferenceText | Returns or sets the flag indicating if text feature can reference a string expression |
CanReverseIntersectionCurve | Returns or sets the flag indicating if intersection curve can be reversed |
CanUseKerningSpaces | Returns or sets the flag indicating if kerning spaces can be used |
Font | Returns the font |
FontStyle | Returns or sets the font style |
FrameOnPath | Returns the frame on path |
IsAssociative | Returns or sets the flag indicating if operation is associative |
OnCurvePlacementProfile | Returns the placement profile for NXOpen.Features.TextBuilderTypes.OnCurve type |
OnFacePlacementMethod | Returns or sets the placement method for NXOpen.Features.TextBuilderTypes.OnFace type |
OnFacePlacementProfile | Returns the placement profile for NXOpen.Features.TextBuilderTypes.OnFace type |
OrientationMethod | Returns or sets the orientation method for NXOpen.Features.TextBuilderTypes.OnCurve type |
OrientationVector | Returns or sets the orientation vector |
ParentFeatureInternal | Returns or sets whether or not the latest timestamped parent feature of this feature should be made internal |
PatchSolutionFlag | Returns or sets the patch solution flag |
PatchSurfaceFilename | Returns or sets the patch surface filename |
PlacementFaces | Returns the placement faces for NXOpen.Features.TextBuilderTypes.OnFace type |
PlanarFrame | Returns the planar frame |
Script | Returns or sets the script |
SectionPlane | Returns or sets the section plane for NXOpen.Features.TextBuilderTypes.OnFace type |
SurroundingPatchSurfaceFilename | Returns or sets the surrounding patch surface filename |
Tag | Returns the Tag for this object. |
Text | Returns the string expression representing the text |
TextString | Returns or sets the string to be rendered |
Type | Returns or sets the type |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
CommitFeature | Commits the feature parameters and creates the feature @return |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetFeature | Returns the feature currently being edited by this builder. |
GetObject | Returns the object currently being edited by this builder. |
HideInternalParentFeatureAfterEdit | Re-suppress an internal parent feature (a slave feature) after it has been edited. |
SelectFont | Selects the font along with appropriate character set |
SetParentFeatureInternal | Set the parent features which would be internal or slaves to the feature being created or commited |
ShowInternalParentFeatureForEdit | Unsuppress an internal parent feature (a slave feature) so it can be edited. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
UnsetParentFeatureInternal | Set the internal parent feature of the feature being edited to external |
UpdateOnOrientationVectorReversal | Updates the builder based on orientation vector sense |
UpdateOnSectionPlane | Updates the builder based on section plane |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Enumerations¶
TextBuilderFontStyleOptions Enumeration | Font style options |
TextBuilderOnFacePlacementMethodOptions Enumeration | The placement options for NXOpen.Features.TextBuilderTypes.OnFace type |
TextBuilderOrientationMethodOptions Enumeration | The orientation options for NXOpen.Features.TextBuilderTypes.OnCurve type |
TextBuilderScriptOptions Enumeration | Script or character set options |
TextBuilderTypes Enumeration | Text placement type |
Property Detail¶
CanCreateBoundingBox¶
-
TextBuilder.
CanCreateBoundingBox
¶ Returns or sets the flag indicating if bounding box can be created
-------------------------------------
Getter Method
Signature
CanCreateBoundingBox()
Returns: Return type: bool New in version NX7.5.1.
License requirements: None.
-------------------------------------
Setter Method
Signature
CanCreateBoundingBox(canCreateBoundingBox)
Parameters: canCreateBoundingBox (bool) – New in version NX7.5.1.
License requirements: solid_modeling (“SOLIDS MODELING”)
CanJoinCurves¶
-
TextBuilder.
CanJoinCurves
¶ Returns or sets the flag indicating if curves can be joined
-------------------------------------
Getter Method
Signature
CanJoinCurves()
Returns: Return type: bool New in version NX7.5.1.
License requirements: None.
-------------------------------------
Setter Method
Signature
CanJoinCurves(canJoinCurves)
Parameters: canJoinCurves (bool) – New in version NX7.5.1.
License requirements: solid_modeling (“SOLIDS MODELING”)
CanProjectCurves¶
-
TextBuilder.
CanProjectCurves
¶ Returns or sets the flag indicating if curves can be projected
-------------------------------------
Getter Method
Signature
CanProjectCurves()
Returns: Return type: bool New in version NX7.5.1.
License requirements: None.
-------------------------------------
Setter Method
Signature
CanProjectCurves(canProjectCurves)
Parameters: canProjectCurves (bool) – New in version NX7.5.1.
License requirements: solid_modeling (“SOLIDS MODELING”)
CanReferenceText¶
-
TextBuilder.
CanReferenceText
¶ Returns or sets the flag indicating if text feature can reference a string expression
-------------------------------------
Getter Method
Signature
CanReferenceText()
Returns: Return type: bool New in version NX7.5.1.
License requirements: None.
-------------------------------------
Setter Method
Signature
CanReferenceText(canReferenceText)
Parameters: canReferenceText (bool) – New in version NX7.5.1.
License requirements: solid_modeling (“SOLIDS MODELING”)
CanReverseIntersectionCurve¶
-
TextBuilder.
CanReverseIntersectionCurve
¶ Returns or sets the flag indicating if intersection curve can be reversed
-------------------------------------
Getter Method
Signature
CanReverseIntersectionCurve()
Returns: Return type: bool New in version NX7.5.1.
License requirements: None.
-------------------------------------
Setter Method
Signature
CanReverseIntersectionCurve(canReverse)
Parameters: canReverse (bool) – New in version NX7.5.1.
License requirements: solid_modeling (“SOLIDS MODELING”)
CanUseKerningSpaces¶
-
TextBuilder.
CanUseKerningSpaces
¶ Returns or sets the flag indicating if kerning spaces can be used
-------------------------------------
Getter Method
Signature
CanUseKerningSpaces()
Returns: Return type: bool New in version NX7.5.1.
License requirements: None.
-------------------------------------
Setter Method
Signature
CanUseKerningSpaces(canUseKerningSpaces)
Parameters: canUseKerningSpaces (bool) – New in version NX7.5.1.
License requirements: solid_modeling (“SOLIDS MODELING”)
Font¶
-
TextBuilder.
Font
¶ Returns the font
-------------------------------------
Getter Method
Signature
Font()
Returns: Return type: str New in version NX7.5.1.
License requirements: None.
FontStyle¶
-
TextBuilder.
FontStyle
¶ Returns or sets the font style
-------------------------------------
Getter Method
Signature
FontStyle()
Returns: Return type: NXOpen.Features.TextBuilderFontStyleOptions
New in version NX7.5.1.
License requirements: None.
-------------------------------------
Setter Method
Signature
FontStyle(fontStyle)
Parameters: fontStyle ( NXOpen.Features.TextBuilderFontStyleOptions
) –New in version NX7.5.1.
License requirements: solid_modeling (“SOLIDS MODELING”)
FrameOnPath¶
-
TextBuilder.
FrameOnPath
¶ Returns the frame on path
-------------------------------------
Getter Method
Signature
FrameOnPath()
Returns: Return type: NXOpen.GeometricUtilities.FrameOnPathBuilder
New in version NX7.5.1.
License requirements: None.
IsAssociative¶
-
TextBuilder.
IsAssociative
¶ Returns or sets the flag indicating if operation is associative
-------------------------------------
Getter Method
Signature
IsAssociative()
Returns: Return type: bool New in version NX7.5.1.
License requirements: None.
-------------------------------------
Setter Method
Signature
IsAssociative(isAssociative)
Parameters: isAssociative (bool) – New in version NX7.5.1.
License requirements: solid_modeling (“SOLIDS MODELING”)
OnCurvePlacementProfile¶
-
TextBuilder.
OnCurvePlacementProfile
¶ Returns the placement profile for
NXOpen.Features.TextBuilderTypes.OnCurve
type-------------------------------------
Getter Method
Signature
OnCurvePlacementProfile()
Returns: Return type: NXOpen.Section
New in version NX7.5.1.
License requirements: None.
OnFacePlacementMethod¶
-
TextBuilder.
OnFacePlacementMethod
¶ Returns or sets the placement method for
NXOpen.Features.TextBuilderTypes.OnFace
type-------------------------------------
Getter Method
Signature
OnFacePlacementMethod()
Returns: Return type: NXOpen.Features.TextBuilderOnFacePlacementMethodOptions
New in version NX7.5.1.
License requirements: None.
-------------------------------------
Setter Method
Signature
OnFacePlacementMethod(placementMethod)
Parameters: placementMethod ( NXOpen.Features.TextBuilderOnFacePlacementMethodOptions
) –New in version NX7.5.1.
License requirements: solid_modeling (“SOLIDS MODELING”)
OnFacePlacementProfile¶
-
TextBuilder.
OnFacePlacementProfile
¶ Returns the placement profile for
NXOpen.Features.TextBuilderTypes.OnFace
type-------------------------------------
Getter Method
Signature
OnFacePlacementProfile()
Returns: Return type: NXOpen.Section
New in version NX7.5.1.
License requirements: None.
OrientationMethod¶
-
TextBuilder.
OrientationMethod
¶ Returns or sets the orientation method for
NXOpen.Features.TextBuilderTypes.OnCurve
type-------------------------------------
Getter Method
Signature
OrientationMethod()
Returns: Return type: NXOpen.Features.TextBuilderOrientationMethodOptions
New in version NX7.5.1.
License requirements: None.
-------------------------------------
Setter Method
Signature
OrientationMethod(orientationMethod)
Parameters: orientationMethod ( NXOpen.Features.TextBuilderOrientationMethodOptions
) –New in version NX7.5.1.
License requirements: solid_modeling (“SOLIDS MODELING”)
OrientationVector¶
-
TextBuilder.
OrientationVector
¶ Returns or sets the orientation vector
-------------------------------------
Getter Method
Signature
OrientationVector()
Returns: Return type: NXOpen.Direction
New in version NX7.5.1.
License requirements: None.
-------------------------------------
Setter Method
Signature
OrientationVector(orientationVector)
Parameters: orientationVector ( NXOpen.Direction
) –New in version NX7.5.1.
License requirements: solid_modeling (“SOLIDS MODELING”)
PlacementFaces¶
-
TextBuilder.
PlacementFaces
¶ Returns the placement faces for
NXOpen.Features.TextBuilderTypes.OnFace
type-------------------------------------
Getter Method
Signature
PlacementFaces()
Returns: Return type: NXOpen.ScCollector
New in version NX7.5.1.
License requirements: None.
PlanarFrame¶
-
TextBuilder.
PlanarFrame
¶ Returns the planar frame
-------------------------------------
Getter Method
Signature
PlanarFrame()
Returns: Return type: NXOpen.GeometricUtilities.RectangularFrameBuilder
New in version NX7.5.1.
License requirements: None.
Script¶
-
TextBuilder.
Script
¶ Returns or sets the script
-------------------------------------
Getter Method
Signature
Script()
Returns: Return type: NXOpen.Features.TextBuilderScriptOptions
New in version NX7.5.1.
License requirements: None.
-------------------------------------
Setter Method
Signature
Script(script)
Parameters: script ( NXOpen.Features.TextBuilderScriptOptions
) –New in version NX7.5.1.
License requirements: solid_modeling (“SOLIDS MODELING”)
SectionPlane¶
-
TextBuilder.
SectionPlane
¶ Returns or sets the section plane for
NXOpen.Features.TextBuilderTypes.OnFace
type-------------------------------------
Getter Method
Signature
SectionPlane()
Returns: Return type: NXOpen.Plane
New in version NX7.5.1.
License requirements: None.
-------------------------------------
Setter Method
Signature
SectionPlane(sectionPlane)
Parameters: sectionPlane ( NXOpen.Plane
) –New in version NX7.5.1.
License requirements: solid_modeling (“SOLIDS MODELING”)
Text¶
-
TextBuilder.
Text
¶ Returns the string expression representing the text
-------------------------------------
Getter Method
Signature
Text()
Returns: Return type: NXOpen.Expression
New in version NX7.5.1.
License requirements: None.
TextString¶
-
TextBuilder.
TextString
¶ Returns or sets the string to be rendered
-------------------------------------
Getter Method
Signature
TextString()
Returns: Copy of the text referenced by the builder Return type: str New in version NX7.5.3.
License requirements: None.
-------------------------------------
Setter Method
Signature
TextString(textString)
Parameters: textString (str) – Text to be rendered New in version NX7.5.3.
License requirements: solid_modeling (“SOLIDS MODELING”)
Type¶
-
TextBuilder.
Type
¶ Returns or sets the type
-------------------------------------
Getter Method
Signature
Type()
Returns: Return type: NXOpen.Features.TextBuilderTypes
New in version NX7.5.1.
License requirements: None.
-------------------------------------
Setter Method
Signature
Type(type)
Parameters: type ( NXOpen.Features.TextBuilderTypes
) –New in version NX7.5.1.
License requirements: solid_modeling (“SOLIDS MODELING”)
Method Detail¶
SelectFont¶
-
TextBuilder.
SelectFont
¶ Selects the font along with appropriate character set
Signature
SelectFont(fontName, script)
Parameters: - fontName (str) – Font
- script (
NXOpen.Features.TextBuilderScriptOptions
) – Character set
New in version NX7.5.1.
License requirements: solid_modeling (“SOLIDS MODELING”)
UpdateOnOrientationVectorReversal¶
-
TextBuilder.
UpdateOnOrientationVectorReversal
¶ Updates the builder based on orientation vector sense
Signature
UpdateOnOrientationVectorReversal()
New in version NX7.5.1.
License requirements: solid_modeling (“SOLIDS MODELING”)
UpdateOnSectionPlane¶
-
TextBuilder.
UpdateOnSectionPlane
¶ Updates the builder based on section plane
Signature
UpdateOnSectionPlane()
New in version NX7.5.1.
License requirements: solid_modeling (“SOLIDS MODELING”)
Validate¶
-
TextBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.