FrameOnPathBuilder Class¶
-
class
NXOpen.GeometricUtilities.
FrameOnPathBuilder
¶ Bases:
NXOpen.TaggedObject
,NXOpen.GeometricUtilities.IComponentBuilder
Frame on path builder
New in version NX7.5.1.
Properties¶
Property | Description |
---|---|
AnchorLocation | Returns or sets the anchor location |
AnchorPosition | Returns the anchor position |
Height | Returns the height |
IsApexReversed | Returns or sets the value indicating if apex point is reversed |
Length | Returns the length |
Offset | Returns the offset |
Tag | Returns the Tag for this object. |
WScale | Returns or sets the width scale |
Methods¶
Method | Description |
---|---|
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Enumerations¶
FrameOnPathBuilderAnchorLocationType Enumeration | Anchor location types |
Property Detail¶
AnchorLocation¶
-
FrameOnPathBuilder.
AnchorLocation
¶ Returns or sets the anchor location
-------------------------------------
Getter Method
Signature
AnchorLocation()
Returns: Return type: NXOpen.GeometricUtilities.FrameOnPathBuilderAnchorLocationType
New in version NX7.5.1.
License requirements: None.
-------------------------------------
Setter Method
Signature
AnchorLocation(anchorLocation)
Parameters: anchorLocation ( NXOpen.GeometricUtilities.FrameOnPathBuilderAnchorLocationType
) –New in version NX7.5.1.
License requirements: solid_modeling (“SOLIDS MODELING”)
AnchorPosition¶
-
FrameOnPathBuilder.
AnchorPosition
¶ Returns the anchor position
-------------------------------------
Getter Method
Signature
AnchorPosition()
Returns: Return type: NXOpen.GeometricUtilities.OnPathDimensionBuilder
New in version NX7.5.1.
License requirements: None.
Height¶
-
FrameOnPathBuilder.
Height
¶ Returns the height
-------------------------------------
Getter Method
Signature
Height()
Returns: Return type: NXOpen.Expression
New in version NX7.5.1.
License requirements: None.
IsApexReversed¶
-
FrameOnPathBuilder.
IsApexReversed
¶ Returns or sets the value indicating if apex point is reversed
-------------------------------------
Getter Method
Signature
IsApexReversed()
Returns: Return type: bool New in version NX7.5.1.
License requirements: None.
-------------------------------------
Setter Method
Signature
IsApexReversed(isReversed)
Parameters: isReversed (bool) – New in version NX7.5.1.
License requirements: solid_modeling (“SOLIDS MODELING”)
Length¶
-
FrameOnPathBuilder.
Length
¶ Returns the length
-------------------------------------
Getter Method
Signature
Length()
Returns: Return type: NXOpen.Expression
New in version NX7.5.1.
License requirements: None.
Offset¶
-
FrameOnPathBuilder.
Offset
¶ Returns the offset
-------------------------------------
Getter Method
Signature
Offset()
Returns: Return type: NXOpen.Expression
New in version NX7.5.1.
License requirements: None.
WScale¶
-
FrameOnPathBuilder.
WScale
¶ Returns or sets the width scale
-------------------------------------
Getter Method
Signature
WScale()
Returns: Return type: float New in version NX7.5.1.
License requirements: None.
-------------------------------------
Setter Method
Signature
WScale(wScale)
Parameters: wScale (float) – New in version NX7.5.1.
License requirements: None.
Method Detail¶
Validate¶
-
FrameOnPathBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.