SnipSurfaceBuilder Class¶
-
class
NXOpen.Features.
SnipSurfaceBuilder
¶ Bases:
NXOpen.Features.FeatureBuilder
Represents a
NXOpen.Features.SnipSurface
builderTo create a new instance of this class, use
NXOpen.Features.FeatureCollection.CreateSnipSurfaceBuilder
Default values.
Property Value RefitControl.DegreesAndSegmentsOrPatches.Degree 3 RefitControl.DegreesAndSegmentsOrPatches.SegmentsOrPatches 1 RefitControl.DegreesAndSegmentsOrPatches.UDegree 5 RefitControl.DegreesAndSegmentsOrPatches.UPatches 1 RefitControl.DegreesAndSegmentsOrPatches.VDegree 5 RefitControl.DegreesAndSegmentsOrPatches.VPatches 1 New in version NX6.0.0.
Properties¶
Property | Description |
---|---|
CutType | Returns or sets the cutting type |
DivideSurface | Returns or sets a value indicating whether to divide the surface |
EditCopy | Returns or sets a value indicating whether to keep the original surface intact |
IsoparametricPosition | Returns the isoparametric position |
KeepOppositeSurface | Returns or sets a value indicating whether to keep the opposite surface. |
ParentFeatureInternal | Returns or sets whether or not the latest timestamped parent feature of this feature should be made internal |
PatchSolutionFlag | Returns or sets the patch solution flag |
PatchSurfaceFilename | Returns or sets the patch surface filename |
ProjectDirection | Returns the project direction |
RefitControl | Returns the refit control |
RegionPickPoint | Returns or sets the 3D point picked on surface in Select Face |
SelectUV | Returns or sets the UV flag |
SnippingCurve | Returns the snipping curve |
SnippingObject | Returns the snipping object |
SnippingPlane | Returns or sets the snipping plane |
SurfacePointUV | Returns or sets the UV values of the picked point on surface |
SurroundingPatchSurfaceFilename | Returns or sets the surrounding patch surface filename |
Tag | Returns the Tag for this object. |
TargetFace | Returns the target face |
Type | Returns or sets the snipping method accessor |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
CommitFeature | Commits the feature parameters and creates the feature @return |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetCreateNewCopy | Returns the indicator for creating a new copy @return |
GetFeature | Returns the feature currently being edited by this builder. |
GetObject | Returns the object currently being edited by this builder. |
HideInternalParentFeatureAfterEdit | Re-suppress an internal parent feature (a slave feature) after it has been edited. |
SetCreateNewCopy | Sets the indicator for creating a new copy |
SetParentFeatureInternal | Set the parent features which would be internal or slaves to the feature being created or commited |
ShowInternalParentFeatureForEdit | Unsuppress an internal parent feature (a slave feature) so it can be edited. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
UnsetParentFeatureInternal | Set the internal parent feature of the feature being edited to external |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Enumerations¶
SnipSurfaceBuilderTypes Enumeration | Snip method added in v 7. |
Property Detail¶
CutType¶
-
SnipSurfaceBuilder.
CutType
¶ Returns or sets the cutting type
-------------------------------------
Getter Method
Signature
CutType()
Returns: Return type: int New in version NX6.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”) OR studio_free_form (“STUDIO FREE FORM”)
-------------------------------------
Setter Method
Signature
CutType(cutType)
Parameters: cutType (int) – New in version NX6.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”) OR studio_free_form (“STUDIO FREE FORM”)
DivideSurface¶
-
SnipSurfaceBuilder.
DivideSurface
¶ Returns or sets a value indicating whether to divide the surface
-------------------------------------
Getter Method
Signature
DivideSurface()
Returns: Return type: bool New in version NX6.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”) OR studio_free_form (“STUDIO FREE FORM”)
-------------------------------------
Setter Method
Signature
DivideSurface(divide)
Parameters: divide (bool) – New in version NX6.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”) OR studio_free_form (“STUDIO FREE FORM”)
EditCopy¶
-
SnipSurfaceBuilder.
EditCopy
¶ Returns or sets a value indicating whether to keep the original surface intact
-------------------------------------
Getter Method
Signature
EditCopy()
Returns: Return type: bool New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
EditCopy(editCopy)
Parameters: editCopy (bool) – New in version NX7.5.0.
License requirements: None.
IsoparametricPosition¶
-
SnipSurfaceBuilder.
IsoparametricPosition
¶ Returns the isoparametric position
-------------------------------------
Getter Method
Signature
IsoparametricPosition()
Returns: Return type: NXOpen.Expression
New in version NX7.5.0.
License requirements: None.
KeepOppositeSurface¶
-
SnipSurfaceBuilder.
KeepOppositeSurface
¶ Returns or sets a value indicating whether to keep the opposite surface.
This is applicable only when DivideSurface is false
-------------------------------------
Getter Method
Signature
KeepOppositeSurface()
Returns: Return type: bool New in version NX6.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”) OR studio_free_form (“STUDIO FREE FORM”)
-------------------------------------
Setter Method
Signature
KeepOppositeSurface(switchRegion)
Parameters: switchRegion (bool) – New in version NX6.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”) OR studio_free_form (“STUDIO FREE FORM”)
ProjectDirection¶
-
SnipSurfaceBuilder.
ProjectDirection
¶ Returns the project direction
-------------------------------------
Getter Method
Signature
ProjectDirection()
Returns: Projection Options data Return type: NXOpen.GeometricUtilities.ProjectionOptions
New in version NX6.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”) OR studio_free_form (“STUDIO FREE FORM”)
RefitControl¶
-
SnipSurfaceBuilder.
RefitControl
¶ Returns the refit control
-------------------------------------
Getter Method
Signature
RefitControl()
Returns: Return type: NXOpen.GeometricUtilities.RefitControlBuilder
New in version NX6.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”) OR studio_free_form (“STUDIO FREE FORM”)
RegionPickPoint¶
-
SnipSurfaceBuilder.
RegionPickPoint
¶ Returns or sets the 3D point picked on surface in Select Face
-------------------------------------
Getter Method
Signature
RegionPickPoint()
Returns: Return type: NXOpen.Point3d
New in version NX6.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”) OR studio_free_form (“STUDIO FREE FORM”)
-------------------------------------
Setter Method
Signature
RegionPickPoint(pnt)
Parameters: pnt ( NXOpen.Point3d
) –New in version NX6.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”) OR studio_free_form (“STUDIO FREE FORM”)
SelectUV¶
-
SnipSurfaceBuilder.
SelectUV
¶ Returns or sets the UV flag
-------------------------------------
Getter Method
Signature
SelectUV()
Returns: Return type: int New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
SelectUV(selectUV)
Parameters: selectUV (int) – New in version NX7.5.0.
License requirements: None.
SnippingCurve¶
-
SnipSurfaceBuilder.
SnippingCurve
¶ Returns the snipping curve
-------------------------------------
Getter Method
Signature
SnippingCurve()
Returns: Return type: NXOpen.Section
New in version NX6.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”) OR studio_free_form (“STUDIO FREE FORM”)
SnippingObject¶
-
SnipSurfaceBuilder.
SnippingObject
¶ Returns the snipping object
-------------------------------------
Getter Method
Signature
SnippingObject()
Returns: Return type: NXOpen.SelectTaggedObject
New in version NX7.5.0.
License requirements: solid_modeling (“SOLIDS MODELING”) OR studio_free_form (“STUDIO FREE FORM”)
SnippingPlane¶
-
SnipSurfaceBuilder.
SnippingPlane
¶ Returns or sets the snipping plane
-------------------------------------
Getter Method
Signature
SnippingPlane()
Returns: Return type: NXOpen.Plane
New in version NX6.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”) OR studio_free_form (“STUDIO FREE FORM”)
-------------------------------------
Setter Method
Signature
SnippingPlane(plane)
Parameters: plane ( NXOpen.Plane
) –New in version NX6.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”) OR studio_free_form (“STUDIO FREE FORM”)
SurfacePointUV¶
-
SnipSurfaceBuilder.
SurfacePointUV
¶ Returns or sets the UV values of the picked point on surface
-------------------------------------
Getter Method
Signature
SurfacePointUV()
Returns: Return type: NXOpen.Point3d
New in version NX6.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”) OR studio_free_form (“STUDIO FREE FORM”)
-------------------------------------
Setter Method
Signature
SurfacePointUV(surfacePointUV)
Parameters: surfacePointUV ( NXOpen.Point3d
) –New in version NX6.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”) OR studio_free_form (“STUDIO FREE FORM”)
TargetFace¶
-
SnipSurfaceBuilder.
TargetFace
¶ Returns the target face
-------------------------------------
Getter Method
Signature
TargetFace()
Returns: Return type: NXOpen.SelectFace
New in version NX6.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”) OR studio_free_form (“STUDIO FREE FORM”)
Type¶
-
SnipSurfaceBuilder.
Type
¶ Returns or sets the snipping method accessor
-------------------------------------
Getter Method
Signature
Type()
Returns: Return type: NXOpen.Features.SnipSurfaceBuilderTypes
New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Type(type)
Parameters: type ( NXOpen.Features.SnipSurfaceBuilderTypes
) –New in version NX7.5.0.
License requirements: None.
Method Detail¶
GetCreateNewCopy¶
-
SnipSurfaceBuilder.
GetCreateNewCopy
¶ Returns the indicator for creating a new copy
Signature
GetCreateNewCopy()
Returns: Return type: bool New in version NX6.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”) OR studio_free_form (“STUDIO FREE FORM”)
SetCreateNewCopy¶
-
SnipSurfaceBuilder.
SetCreateNewCopy
¶ Sets the indicator for creating a new copy
Signature
SetCreateNewCopy(createNewCopy)
Parameters: createNewCopy (bool) – New in version NX6.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”) OR studio_free_form (“STUDIO FREE FORM”)
Validate¶
-
SnipSurfaceBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.