SectionSurfaceBuilderEx Class¶
-
class
NXOpen.Features.
SectionSurfaceBuilderEx
¶ Bases:
NXOpen.Features.FeatureBuilder
Represents a
NXOpen.Features.SectionSurface
builder.Use
NXOpen.Features.SectionSurfaceBuilderEx
to create section surface. For more details see the NX documentation for Section Surface.To create a new instance of this class, use
NXOpen.Features.FeatureCollection.CreateSectionSurfaceBuilderEx
Default values.
Property Value AngleLaw.EndValue.Value 1 AngleLaw.Function ft AngleLaw.LawType Constant AngleLaw.Parameter t AngleLaw.StartValue.Value 1 AngleLaw.Value.Value 0.0 CircularTypeMode ThreePoint ConicTypeMode Shoulder ControlRegion Entire CubicTypeMode TwoSlopes EndContinuity.ContinuityType G1 RadiusLaw.EndValue.Value 1.0 (millimeters part), 0.05 (inches part) RadiusLaw.StartValue.Value 1.0 (millimeters part), 0.05 (inches part) RadiusLaw.Value.Value 1.0 (millimeters part), 0.05 (inches part) RhoLaw.EndValue.Value 0.5 RhoLaw.StartValue.Value 0.5 RhoLaw.Value.Value 0.5 SectionMethodCircleTangent FilletArc SectionMethodFilletBridge Continuity SectionMethodRho Rho SlopeControl ByApex SpineEndFlowDirection NotSpecified SpineStartFlowDirection NotSpecified SpineType ByVector StartContinuity.ContinuityType G1 New in version NX9.0.0.
Properties¶
Property | Description |
---|---|
AlternateSolutions | Returns or sets the alternate method. |
AngleLaw | Returns the angle law. |
ApexCurve | Returns the apex curve. |
BodyTypePreference | Returns or sets the body preference type. |
CircularTypeMode | Returns or sets the circular type mode. |
ConicTypeMode | Returns or sets the conic type mode. |
ControlRegion | Returns or sets the control region. |
CreateApexCurve | Returns or sets whether an apex curve should be created. |
CubicTypeMode | Returns or sets the cubic type mode. |
EndContinuity | Returns the end continuity. |
EndDepthSkew | Returns the end depth skew. |
EndDirection | Returns or sets the end direction. |
EndFace | Returns the end face. |
EndHighlightCurve | Returns the end highlight curve. |
EndShapeCurve | Returns the end shape curve. |
EndSlopeCurve | Returns the end slope curve. |
EntireDepthSkew | Returns the entire depth skew. |
G0Tolerance | Returns or sets the g0 tolerance. |
G1Tolerance | Returns or sets the g1 tolerance. |
G2Tolerance | Returns or sets the g2 tolerance. |
ParentFeatureInternal | Returns or sets whether or not the latest timestamped parent feature of this feature should be made internal |
PatchSolutionFlag | Returns or sets the patch solution flag |
PatchSurfaceFilename | Returns or sets the patch surface filename |
RadiusLaw | Returns the radius law. |
Rebuild | Returns the rebuild. |
RhoLaw | Returns the rho law. |
SectionEndGuide | Returns the section end guide. |
SectionInteriorGuide1 | Returns the interior guide1. |
SectionInteriorGuide2 | Returns the section interior guide2. |
SectionInteriorGuide3 | Returns the section interior guide3. |
SectionMethodCircleTangent | Returns or sets the section method circle tangent. |
SectionMethodFilletBridge | Returns or sets the section method fillet bridge. |
SectionMethodRho | Returns or sets the section method rho. |
SectionOrientationGuide | Returns the section orientation guide. |
SectionStartGuide | Returns the section start guide. |
ShoulderCurve | Returns the shoulder curve. |
SlopeControl | Returns or sets the slope control. |
SpineEndFlowDirection | Returns or sets the spine end flow direction. |
SpineSection | Returns the spine section. |
SpineStartFlowDirection | Returns or sets the spine start flow direction. |
SpineType | Returns or sets the spine. |
SpineVector | Returns or sets the spine vector. |
StartContinuity | Returns the start continuity. |
StartDepthSkew | Returns the start depth skew. |
StartDirection | Returns or sets the start direction. |
StartFace | Returns the start face. |
StartHighlightCurve | Returns the start highlight curve. |
StartShapeCurve | Returns the start shape curve. |
StartSlopeCurve | Returns the start slope curve. |
SurroundingPatchSurfaceFilename | Returns or sets the surrounding patch surface filename |
Tag | Returns the Tag for this object. |
Type | Returns or sets the type. |
UDegree | Returns or sets the u degree. |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
CommitFeature | Commits the feature parameters and creates the feature @return |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetFeature | Returns the feature currently being edited by this builder. |
GetObject | Returns the object currently being edited by this builder. |
HideInternalParentFeatureAfterEdit | Re-suppress an internal parent feature (a slave feature) after it has been edited. |
SetParentFeatureInternal | Set the parent features which would be internal or slaves to the feature being created or commited |
ShowInternalParentFeatureForEdit | Unsuppress an internal parent feature (a slave feature) so it can be edited. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
UnsetParentFeatureInternal | Set the internal parent feature of the feature being edited to external |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Enumerations¶
Property Detail¶
AlternateSolutions¶
-
SectionSurfaceBuilderEx.
AlternateSolutions
¶ Returns or sets the alternate method.
This api only applies to the follow section surface methods, circle_tangent and linear-tangent
-------------------------------------
Getter Method
Signature
AlternateSolutions()
Returns: Return type: int New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
AlternateSolutions(alternateSolutions)
Parameters: alternateSolutions (int) – New in version NX9.0.0.
License requirements: None.
AngleLaw¶
-
SectionSurfaceBuilderEx.
AngleLaw
¶ Returns the angle law.
-------------------------------------
Getter Method
Signature
AngleLaw()
Returns: Return type: NXOpen.GeometricUtilities.LawBuilder
New in version NX9.0.0.
License requirements: None.
ApexCurve¶
-
SectionSurfaceBuilderEx.
ApexCurve
¶ Returns the apex curve.
Only applies to the follow section surface types:
NXOpen.Features.SectionSurfaceBuilderExConicType.Shoulder
,NXOpen.Features.SectionSurfaceBuilderExConicType.Rho
, andNXOpen.Features.SectionSurfaceBuilderExConicType.Hilite
-------------------------------------
Getter Method
Signature
ApexCurve()
Returns: Return type: NXOpen.Section
New in version NX9.0.0.
License requirements: None.
BodyTypePreference¶
-
SectionSurfaceBuilderEx.
BodyTypePreference
¶ Returns or sets the body preference type.
-------------------------------------
Getter Method
Signature
BodyTypePreference()
Returns: Return type: NXOpen.Features.SectionSurfaceBuilderExBodyType
New in version NX10.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
BodyTypePreference(type)
Parameters: type ( NXOpen.Features.SectionSurfaceBuilderExBodyType
) –New in version NX10.0.0.
License requirements: features_modeling (“FEATURES MODELING”), nx_freeform_2 (“advanced freeform modeling”)
CircularTypeMode¶
-
SectionSurfaceBuilderEx.
CircularTypeMode
¶ Returns or sets the circular type mode.
-------------------------------------
Getter Method
Signature
CircularTypeMode()
Returns: Return type: NXOpen.Features.SectionSurfaceBuilderExCircularType
New in version NX9.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
CircularTypeMode(circularTypeMode)
Parameters: circularTypeMode ( NXOpen.Features.SectionSurfaceBuilderExCircularType
) –New in version NX9.0.0.
License requirements: features_modeling (“FEATURES MODELING”), nx_freeform_2 (“advanced freeform modeling”)
ConicTypeMode¶
-
SectionSurfaceBuilderEx.
ConicTypeMode
¶ Returns or sets the conic type mode.
-------------------------------------
Getter Method
Signature
ConicTypeMode()
Returns: Return type: NXOpen.Features.SectionSurfaceBuilderExConicType
New in version NX9.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ConicTypeMode(conicTypeMode)
Parameters: conicTypeMode ( NXOpen.Features.SectionSurfaceBuilderExConicType
) –New in version NX9.0.0.
License requirements: features_modeling (“FEATURES MODELING”), nx_freeform_2 (“advanced freeform modeling”)
ControlRegion¶
-
SectionSurfaceBuilderEx.
ControlRegion
¶ Returns or sets the control region.
-------------------------------------
Getter Method
Signature
ControlRegion()
Returns: Return type: NXOpen.Features.SectionSurfaceBuilderExControlRegionType
New in version NX9.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ControlRegion(controlRegion)
Parameters: controlRegion ( NXOpen.Features.SectionSurfaceBuilderExControlRegionType
) –New in version NX9.0.0.
License requirements: features_modeling (“FEATURES MODELING”), nx_freeform_2 (“advanced freeform modeling”)
CreateApexCurve¶
-
SectionSurfaceBuilderEx.
CreateApexCurve
¶ Returns or sets whether an apex curve should be created.
-------------------------------------
Getter Method
Signature
CreateApexCurve()
Returns: Return type: bool New in version NX9.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
CreateApexCurve(createApexCurve)
Parameters: createApexCurve (bool) – New in version NX9.0.0.
License requirements: features_modeling (“FEATURES MODELING”), nx_freeform_2 (“advanced freeform modeling”)
CubicTypeMode¶
-
SectionSurfaceBuilderEx.
CubicTypeMode
¶ Returns or sets the cubic type mode.
-------------------------------------
Getter Method
Signature
CubicTypeMode()
Returns: Return type: NXOpen.Features.SectionSurfaceBuilderExCubicType
New in version NX9.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
CubicTypeMode(cubicTypeMode)
Parameters: cubicTypeMode ( NXOpen.Features.SectionSurfaceBuilderExCubicType
) –New in version NX9.0.0.
License requirements: features_modeling (“FEATURES MODELING”), nx_freeform_2 (“advanced freeform modeling”)
EndContinuity¶
-
SectionSurfaceBuilderEx.
EndContinuity
¶ Returns the end continuity.
-------------------------------------
Getter Method
Signature
EndContinuity()
Returns: Return type: NXOpen.GeometricUtilities.Continuity
New in version NX9.0.0.
License requirements: None.
EndDepthSkew¶
-
SectionSurfaceBuilderEx.
EndDepthSkew
¶ Returns the end depth skew.
-------------------------------------
Getter Method
Signature
EndDepthSkew()
Returns: Return type: NXOpen.GeometricUtilities.DepthSkewBuilder
New in version NX9.0.0.
License requirements: None.
EndDirection¶
-
SectionSurfaceBuilderEx.
EndDirection
¶ Returns or sets the end direction.
-------------------------------------
Getter Method
Signature
EndDirection()
Returns: Return type: bool New in version NX9.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
EndDirection(endDirection)
Parameters: endDirection (bool) – New in version NX9.0.0.
License requirements: features_modeling (“FEATURES MODELING”), nx_freeform_2 (“advanced freeform modeling”)
EndFace¶
-
SectionSurfaceBuilderEx.
EndFace
¶ Returns the end face.
Only applies to the follow section surface types:
NXOpen.Features.SectionSurfaceBuilderExConicType.Shoulder
,NXOpen.Features.SectionSurfaceBuilderExConicType.Rho
,NXOpen.Features.SectionSurfaceBuilderExConicType.Hilite
andNXOpen.Features.SectionSurfaceBuilderExCubicType.FilletBridge
-------------------------------------
Getter Method
Signature
EndFace()
Returns: Return type: NXOpen.ScCollector
New in version NX9.0.0.
License requirements: None.
EndHighlightCurve¶
-
SectionSurfaceBuilderEx.
EndHighlightCurve
¶ Returns the end highlight curve.
Only applies to the follow section surface type:
NXOpen.Features.SectionSurfaceBuilderExConicType.Hilite
-------------------------------------
Getter Method
Signature
EndHighlightCurve()
Returns: Return type: NXOpen.Section
New in version NX9.0.0.
License requirements: None.
EndShapeCurve¶
-
SectionSurfaceBuilderEx.
EndShapeCurve
¶ Returns the end shape curve.
-------------------------------------
Getter Method
Signature
EndShapeCurve()
Returns: Return type: NXOpen.Section
New in version NX9.0.0.
License requirements: None.
EndSlopeCurve¶
-
SectionSurfaceBuilderEx.
EndSlopeCurve
¶ Returns the end slope curve.
Only applies to the follow section surface types:
NXOpen.Features.SectionSurfaceBuilderExConicType.Shoulder
,NXOpen.Features.SectionSurfaceBuilderExConicType.Rho
,NXOpen.Features.SectionSurfaceBuilderExConicType.Hilite
,NXOpen.Features.SectionSurfaceBuilderExCubicType.TwoSlopes
andNXOpen.Features.SectionSurfaceBuilderExConicType.FourPointSlope
-------------------------------------
Getter Method
Signature
EndSlopeCurve()
Returns: Return type: NXOpen.Section
New in version NX9.0.0.
License requirements: None.
EntireDepthSkew¶
-
SectionSurfaceBuilderEx.
EntireDepthSkew
¶ Returns the entire depth skew.
-------------------------------------
Getter Method
Signature
EntireDepthSkew()
Returns: Return type: NXOpen.GeometricUtilities.DepthSkewBuilder
New in version NX9.0.0.
License requirements: None.
G0Tolerance¶
-
SectionSurfaceBuilderEx.
G0Tolerance
¶ Returns or sets the g0 tolerance.
-------------------------------------
Getter Method
Signature
G0Tolerance()
Returns: Return type: float New in version NX9.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
G0Tolerance(g0Tolerance)
Parameters: g0Tolerance (float) – New in version NX9.0.0.
License requirements: features_modeling (“FEATURES MODELING”), nx_freeform_2 (“advanced freeform modeling”)
G1Tolerance¶
-
SectionSurfaceBuilderEx.
G1Tolerance
¶ Returns or sets the g1 tolerance.
-------------------------------------
Getter Method
Signature
G1Tolerance()
Returns: Return type: float New in version NX9.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
G1Tolerance(g1Tolerance)
Parameters: g1Tolerance (float) – New in version NX9.0.0.
License requirements: features_modeling (“FEATURES MODELING”), nx_freeform_2 (“advanced freeform modeling”)
G2Tolerance¶
-
SectionSurfaceBuilderEx.
G2Tolerance
¶ Returns or sets the g2 tolerance.
-------------------------------------
Getter Method
Signature
G2Tolerance()
Returns: Return type: float New in version NX9.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
G2Tolerance(g2Tolerance)
Parameters: g2Tolerance (float) – New in version NX9.0.0.
License requirements: features_modeling (“FEATURES MODELING”), nx_freeform_2 (“advanced freeform modeling”)
RadiusLaw¶
-
SectionSurfaceBuilderEx.
RadiusLaw
¶ Returns the radius law.
-------------------------------------
Getter Method
Signature
RadiusLaw()
Returns: Return type: NXOpen.GeometricUtilities.LawBuilder
New in version NX9.0.0.
License requirements: None.
Rebuild¶
-
SectionSurfaceBuilderEx.
Rebuild
¶ Returns the rebuild.
-------------------------------------
Getter Method
Signature
Rebuild()
Returns: Return type: NXOpen.GeometricUtilities.Rebuild
New in version NX9.0.0.
License requirements: None.
RhoLaw¶
-
SectionSurfaceBuilderEx.
RhoLaw
¶ Returns the rho law.
-------------------------------------
Getter Method
Signature
RhoLaw()
Returns: Return type: NXOpen.GeometricUtilities.LawBuilder
New in version NX9.0.0.
License requirements: None.
SectionEndGuide¶
-
SectionSurfaceBuilderEx.
SectionEndGuide
¶ Returns the section end guide.
-------------------------------------
Getter Method
Signature
SectionEndGuide()
Returns: Return type: NXOpen.Section
New in version NX9.0.0.
License requirements: None.
SectionInteriorGuide1¶
-
SectionSurfaceBuilderEx.
SectionInteriorGuide1
¶ Returns the interior guide1.
Only applies to the follow section surface types:
NXOpen.Features.SectionSurfaceBuilderExConicType.FourPointSlope
,NXOpen.Features.SectionSurfaceBuilderExConicType.FivePoint
, andNXOpen.Features.SectionSurfaceBuilderExCircularType.ThreePoint
-------------------------------------
Getter Method
Signature
SectionInteriorGuide1()
Returns: Return type: NXOpen.Section
New in version NX9.0.0.
License requirements: None.
SectionInteriorGuide2¶
-
SectionSurfaceBuilderEx.
SectionInteriorGuide2
¶ Returns the section interior guide2.
Only applies to the follow section surface types:
NXOpen.Features.SectionSurfaceBuilderExConicType.FourPointSlope
andNXOpen.Features.SectionSurfaceBuilderExConicType.FivePoint
-------------------------------------
Getter Method
Signature
SectionInteriorGuide2()
Returns: Return type: NXOpen.Section
New in version NX9.0.0.
License requirements: None.
SectionInteriorGuide3¶
-
SectionSurfaceBuilderEx.
SectionInteriorGuide3
¶ Returns the section interior guide3.
Only applies to the follow section surface types:
NXOpen.Features.SectionSurfaceBuilderExConicType.FourPointSlope
andNXOpen.Features.SectionSurfaceBuilderExConicType.FivePoint
-------------------------------------
Getter Method
Signature
SectionInteriorGuide3()
Returns: Return type: NXOpen.Section
New in version NX9.0.0.
License requirements: None.
SectionMethodCircleTangent¶
-
SectionSurfaceBuilderEx.
SectionMethodCircleTangent
¶ Returns or sets the section method circle tangent.
-------------------------------------
Getter Method
Signature
SectionMethodCircleTangent()
Returns: Return type: NXOpen.Features.SectionSurfaceBuilderExSectionMethodCircleTangentType
New in version NX9.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
SectionMethodCircleTangent(sectionMethodCircleTangent)
Parameters: sectionMethodCircleTangent ( NXOpen.Features.SectionSurfaceBuilderExSectionMethodCircleTangentType
) –New in version NX9.0.0.
License requirements: features_modeling (“FEATURES MODELING”), nx_freeform_2 (“advanced freeform modeling”)
SectionMethodFilletBridge¶
-
SectionSurfaceBuilderEx.
SectionMethodFilletBridge
¶ Returns or sets the section method fillet bridge.
-------------------------------------
Getter Method
Signature
SectionMethodFilletBridge()
Returns: Return type: NXOpen.Features.SectionSurfaceBuilderExSectionMethodFilletBridgeType
New in version NX9.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
SectionMethodFilletBridge(sectionMethodFilletBridge)
Parameters: sectionMethodFilletBridge ( NXOpen.Features.SectionSurfaceBuilderExSectionMethodFilletBridgeType
) –New in version NX9.0.0.
License requirements: features_modeling (“FEATURES MODELING”), nx_freeform_2 (“advanced freeform modeling”)
SectionMethodRho¶
-
SectionSurfaceBuilderEx.
SectionMethodRho
¶ Returns or sets the section method rho.
-------------------------------------
Getter Method
Signature
SectionMethodRho()
Returns: Return type: NXOpen.Features.SectionSurfaceBuilderExSectionMethodRhoType
New in version NX9.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
SectionMethodRho(sectionMethodRho)
Parameters: sectionMethodRho ( NXOpen.Features.SectionSurfaceBuilderExSectionMethodRhoType
) –New in version NX9.0.0.
License requirements: features_modeling (“FEATURES MODELING”), nx_freeform_2 (“advanced freeform modeling”)
SectionOrientationGuide¶
-
SectionSurfaceBuilderEx.
SectionOrientationGuide
¶ Returns the section orientation guide.
Only applies to the follow section surface types:
NXOpen.Features.SectionSurfaceBuilderExCircularType.CenterRadius
-------------------------------------
Getter Method
Signature
SectionOrientationGuide()
Returns: Return type: NXOpen.Section
New in version NX9.0.0.
License requirements: None.
SectionStartGuide¶
-
SectionSurfaceBuilderEx.
SectionStartGuide
¶ Returns the section start guide.
-------------------------------------
Getter Method
Signature
SectionStartGuide()
Returns: Return type: NXOpen.Section
New in version NX9.0.0.
License requirements: None.
ShoulderCurve¶
-
SectionSurfaceBuilderEx.
ShoulderCurve
¶ Returns the shoulder curve.
Only applies to the follow section surface types:
NXOpen.Features.SectionSurfaceBuilderExConicType.Shoulder
-------------------------------------
Getter Method
Signature
ShoulderCurve()
Returns: Return type: NXOpen.Section
New in version NX9.0.0.
License requirements: None.
SlopeControl¶
-
SectionSurfaceBuilderEx.
SlopeControl
¶ Returns or sets the slope control.
-------------------------------------
Getter Method
Signature
SlopeControl()
Returns: Return type: NXOpen.Features.SectionSurfaceBuilderExSlopeControlType
New in version NX9.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
SlopeControl(slopeControl)
Parameters: slopeControl ( NXOpen.Features.SectionSurfaceBuilderExSlopeControlType
) –New in version NX9.0.0.
License requirements: features_modeling (“FEATURES MODELING”), nx_freeform_2 (“advanced freeform modeling”)
SpineEndFlowDirection¶
-
SectionSurfaceBuilderEx.
SpineEndFlowDirection
¶ Returns or sets the spine end flow direction.
-------------------------------------
Getter Method
Signature
SpineEndFlowDirection()
Returns: Return type: NXOpen.Features.SectionSurfaceBuilderExSpineEndFlowType
New in version NX9.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
SpineEndFlowDirection(spineEndFlowDirection)
Parameters: spineEndFlowDirection ( NXOpen.Features.SectionSurfaceBuilderExSpineEndFlowType
) –New in version NX9.0.0.
License requirements: features_modeling (“FEATURES MODELING”), nx_freeform_2 (“advanced freeform modeling”)
SpineSection¶
-
SectionSurfaceBuilderEx.
SpineSection
¶ Returns the spine section.
-------------------------------------
Getter Method
Signature
SpineSection()
Returns: Return type: NXOpen.Section
New in version NX9.0.0.
License requirements: None.
SpineStartFlowDirection¶
-
SectionSurfaceBuilderEx.
SpineStartFlowDirection
¶ Returns or sets the spine start flow direction.
-------------------------------------
Getter Method
Signature
SpineStartFlowDirection()
Returns: Return type: NXOpen.Features.SectionSurfaceBuilderExSpineStartFlowType
New in version NX9.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
SpineStartFlowDirection(spineStartFlowDirection)
Parameters: spineStartFlowDirection ( NXOpen.Features.SectionSurfaceBuilderExSpineStartFlowType
) –New in version NX9.0.0.
License requirements: features_modeling (“FEATURES MODELING”), nx_freeform_2 (“advanced freeform modeling”)
SpineType¶
-
SectionSurfaceBuilderEx.
SpineType
¶ Returns or sets the spine.
-------------------------------------
Getter Method
Signature
SpineType()
Returns: Return type: NXOpen.Features.SectionSurfaceBuilderExSpine
New in version NX9.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
SpineType(spineType)
Parameters: spineType ( NXOpen.Features.SectionSurfaceBuilderExSpine
) –New in version NX9.0.0.
License requirements: features_modeling (“FEATURES MODELING”), nx_freeform_2 (“advanced freeform modeling”)
SpineVector¶
-
SectionSurfaceBuilderEx.
SpineVector
¶ Returns or sets the spine vector.
-------------------------------------
Getter Method
Signature
SpineVector()
Returns: Return type: NXOpen.Direction
New in version NX9.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
SpineVector(spineVector)
Parameters: spineVector ( NXOpen.Direction
) –New in version NX9.0.0.
License requirements: features_modeling (“FEATURES MODELING”), nx_freeform_2 (“advanced freeform modeling”)
StartContinuity¶
-
SectionSurfaceBuilderEx.
StartContinuity
¶ Returns the start continuity.
-------------------------------------
Getter Method
Signature
StartContinuity()
Returns: Return type: NXOpen.GeometricUtilities.Continuity
New in version NX9.0.0.
License requirements: None.
StartDepthSkew¶
-
SectionSurfaceBuilderEx.
StartDepthSkew
¶ Returns the start depth skew.
-------------------------------------
Getter Method
Signature
StartDepthSkew()
Returns: Return type: NXOpen.GeometricUtilities.DepthSkewBuilder
New in version NX9.0.0.
License requirements: None.
StartDirection¶
-
SectionSurfaceBuilderEx.
StartDirection
¶ Returns or sets the start direction.
Only applies to the follow section surface types:
NXOpen.Features.SectionSurfaceBuilderExCircularType.RadiusAngleArc
andNXOpen.Features.SectionSurfaceBuilderExCubicType.FilletBridge
-------------------------------------
Getter Method
Signature
StartDirection()
Returns: Return type: bool New in version NX9.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
StartDirection(startDirection)
Parameters: startDirection (bool) – New in version NX9.0.0.
License requirements: features_modeling (“FEATURES MODELING”), nx_freeform_2 (“advanced freeform modeling”)
StartFace¶
-
SectionSurfaceBuilderEx.
StartFace
¶ Returns the start face.
Only applies to the follow section surface types:
NXOpen.Features.SectionSurfaceBuilderExConicType.Shoulder
,NXOpen.Features.SectionSurfaceBuilderExConicType.Rho
,NXOpen.Features.SectionSurfaceBuilderExConicType.Hilite
andNXOpen.Features.SectionSurfaceBuilderExCubicType.FilletBridge
-------------------------------------
Getter Method
Signature
StartFace()
Returns: Return type: NXOpen.ScCollector
New in version NX9.0.0.
License requirements: None.
StartHighlightCurve¶
-
SectionSurfaceBuilderEx.
StartHighlightCurve
¶ Returns the start highlight curve.
Only applies to the follow section surface type:
NXOpen.Features.SectionSurfaceBuilderExConicType.Hilite
-------------------------------------
Getter Method
Signature
StartHighlightCurve()
Returns: Return type: NXOpen.Section
New in version NX9.0.0.
License requirements: None.
StartShapeCurve¶
-
SectionSurfaceBuilderEx.
StartShapeCurve
¶ Returns the start shape curve.
-------------------------------------
Getter Method
Signature
StartShapeCurve()
Returns: Return type: NXOpen.Section
New in version NX9.0.0.
License requirements: None.
StartSlopeCurve¶
-
SectionSurfaceBuilderEx.
StartSlopeCurve
¶ Returns the start slope curve.
Only applies to the follow section surface types:
NXOpen.Features.SectionSurfaceBuilderExConicType.Shoulder
,NXOpen.Features.SectionSurfaceBuilderExConicType.Rho
,NXOpen.Features.SectionSurfaceBuilderExConicType.Hilite
,NXOpen.Features.SectionSurfaceBuilderExCubicType.TwoSlopes
andNXOpen.Features.SectionSurfaceBuilderExConicType.FourPointSlope
-------------------------------------
Getter Method
Signature
StartSlopeCurve()
Returns: Return type: NXOpen.Section
New in version NX9.0.0.
License requirements: None.
Type¶
-
SectionSurfaceBuilderEx.
Type
¶ Returns or sets the type.
-------------------------------------
Getter Method
Signature
Type()
Returns: Return type: NXOpen.Features.SectionSurfaceBuilderExTypes
New in version NX9.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Type(type)
Parameters: type ( NXOpen.Features.SectionSurfaceBuilderExTypes
) –New in version NX9.0.0.
License requirements: features_modeling (“FEATURES MODELING”), nx_freeform_2 (“advanced freeform modeling”)
UDegree¶
-
SectionSurfaceBuilderEx.
UDegree
¶ Returns or sets the u degree.
-------------------------------------
Getter Method
Signature
UDegree()
Returns: Return type: NXOpen.Features.SectionSurfaceBuilderExUDegreeType
New in version NX9.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
UDegree(uDegree)
Parameters: uDegree ( NXOpen.Features.SectionSurfaceBuilderExUDegreeType
) –New in version NX9.0.0.
License requirements: features_modeling (“FEATURES MODELING”), nx_freeform_2 (“advanced freeform modeling”)
Method Detail¶
Validate¶
-
SectionSurfaceBuilderEx.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.