SectionSurfaceBuilderExCircularType Enumeration¶
NXOpen.Features.SectionSurfaceBuilderEx.CircularType is an alias for NXOpen.Features.SectionSurfaceBuilderExCircularType
-
class
NXOpen.Features.
SectionSurfaceBuilderExCircularType
¶ Bases:
object
This enum represents the current modes of circular type section surfaces.
Enum Members
Enum Member Enum Member Description ThreePoint Three Point modeTwoPointRadius Two Point Radius modeTwoPointSlope Two Point Slope modeRadiusAngleArc Radius Angle Arc modeCenterRadius Center Radius modeTangentRadius Tangent Radius mode-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-