DepthSkewBuilder Class¶
-
class
NXOpen.GeometricUtilities.
DepthSkewBuilder
¶ Bases:
NXOpen.TaggedObject
,NXOpen.GeometricUtilities.IComponentBuilder
This class provides ability to specify a depth and a skew value.
New in version NX6.0.0.
Properties¶
Property | Description |
---|---|
Depth | Returns the depth |
Skew | Returns the skew |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Property Detail¶
Depth¶
-
DepthSkewBuilder.
Depth
¶ Returns the depth
-------------------------------------
Getter Method
Signature
Depth()
Returns: Return type: NXOpen.Expression
New in version NX6.0.0.
License requirements: None.
Skew¶
-
DepthSkewBuilder.
Skew
¶ Returns the skew
-------------------------------------
Getter Method
Signature
Skew()
Returns: Return type: NXOpen.Expression
New in version NX6.0.0.
License requirements: None.
Method Detail¶
Validate¶
-
DepthSkewBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.