SectionInertiaAnalysisBuilder Class¶
-
class
NXOpen.Features.
SectionInertiaAnalysisBuilder
¶ Bases:
NXOpen.Features.FeatureBuilder
Represents a
NXOpen.Features.SectionInertiaAnalysis
builderTo create a new instance of this class, use
NXOpen.Features.FeatureCollection.CreateSectionInertiaAnalysisBuilder
Default values.
Property Value AnnoLayer 101 CenterOfGravity True DatumPlaneLayer 101 DatumPlanes False NSection 5 PrincipalAxes False RectangleLayer 101 RectangularSection False SecondPrincipleMi True SectionArea True SectionLayer 101 SectionLength True Sections False ShearCenter False New in version NX5.0.0.
Properties¶
Property | Description |
---|---|
AnnoLayer | Returns or sets the anno layer |
CSys | Returns or sets the c sys |
CenterOfGravity | Returns or sets the center of gravity |
CurveCollector | Returns the curve collector |
DatumPlaneLayer | Returns or sets the datum plane layer |
DatumPlanes | Returns or sets the datum planes |
Distance | Returns the distance |
FaceCollector | Returns the face collector |
MassPropertyType | Returns or sets the mass property type |
NSection | Returns or sets the n section |
ParentFeatureInternal | Returns or sets whether or not the latest timestamped parent feature of this feature should be made internal |
PatchSolutionFlag | Returns or sets the patch solution flag |
PatchSurfaceFilename | Returns or sets the patch surface filename |
PathCollector | Returns the path collector |
PrincipalAxes | Returns or sets the principal axes |
RectangleLayer | Returns or sets the rectangle layer |
RectangularSection | Returns or sets the rectangular section |
SecondPrincipleMi | Returns or sets the second principle mi |
SectionArea | Returns or sets the section area |
SectionLayer | Returns or sets the section layer |
SectionLength | Returns or sets the section length |
SectionNormal | Returns or sets the section normal |
SectioningMethod | Returns or sets the sectioning method |
Sections | Returns or sets the sections |
ShearCenter | Returns or sets the shear center |
SurroundingPatchSurfaceFilename | Returns or sets the surrounding patch surface filename |
Tag | Returns the Tag for this object. |
Thickness | Returns the thickness. |
Type | Returns or sets the analysis |
Units | Returns or sets the units for calculations |
ValidityFlag | Returns or sets the validity flag. |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
CommitFeature | Commits the feature parameters and creates the feature @return |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetAnnotation | The annotations generated can be accessed using this method. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetFeature | Returns the feature currently being edited by this builder. |
GetObject | Returns the object currently being edited by this builder. |
HideInternalParentFeatureAfterEdit | Re-suppress an internal parent feature (a slave feature) after it has been edited. |
IsTempGraphics | The function checks if temporary graphics was generated. |
RefreshScreen | The function refreshes the graphic screen if any temporary graphics was previously generated by this command. |
SetParentFeatureInternal | Set the parent features which would be internal or slaves to the feature being created or commited |
ShowInfo | The function displays the information box with information about the section intertia analysis performed. |
ShowInternalParentFeatureForEdit | Unsuppress an internal parent feature (a slave feature) so it can be edited. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
UnsetParentFeatureInternal | Set the internal parent feature of the feature being edited to external |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Enumerations¶
SectionInertiaAnalysisBuilderCoordSys Enumeration | The coordinate system associated with the analysis. |
SectionInertiaAnalysisBuilderPropertyType Enumeration | Type of Analysis property. |
SectionInertiaAnalysisBuilderSampleMethod Enumeration | Type of sampling method to be used in sections along curve type of analysis. |
SectionInertiaAnalysisBuilderSectionAxisNormal Enumeration | Slice direction in case of parallel section type of analysis. |
SectionInertiaAnalysisBuilderTypes Enumeration | The type of Section Inertia Analysis to be performed. |
Property Detail¶
AnnoLayer¶
-
SectionInertiaAnalysisBuilder.
AnnoLayer
¶ Returns or sets the anno layer
-------------------------------------
Getter Method
Signature
AnnoLayer()
Returns: Return type: int New in version NX5.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
AnnoLayer(annoLayer)
Parameters: annoLayer (int) – New in version NX5.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”)
CSys¶
-
SectionInertiaAnalysisBuilder.
CSys
¶ Returns or sets the c sys
-------------------------------------
Getter Method
Signature
CSys()
Returns: Return type: NXOpen.Features.SectionInertiaAnalysisBuilderCoordSys
New in version NX5.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
CSys(csys)
Parameters: csys ( NXOpen.Features.SectionInertiaAnalysisBuilderCoordSys
) –New in version NX5.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”)
CenterOfGravity¶
-
SectionInertiaAnalysisBuilder.
CenterOfGravity
¶ Returns or sets the center of gravity
-------------------------------------
Getter Method
Signature
CenterOfGravity()
Returns: Return type: bool New in version NX5.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
CenterOfGravity(centerOfGravity)
Parameters: centerOfGravity (bool) – New in version NX5.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”)
CurveCollector¶
-
SectionInertiaAnalysisBuilder.
CurveCollector
¶ Returns the curve collector
-------------------------------------
Getter Method
Signature
CurveCollector()
Returns: Return type: NXOpen.Section
New in version NX5.0.0.
License requirements: None.
DatumPlaneLayer¶
-
SectionInertiaAnalysisBuilder.
DatumPlaneLayer
¶ Returns or sets the datum plane layer
-------------------------------------
Getter Method
Signature
DatumPlaneLayer()
Returns: Return type: int New in version NX5.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
DatumPlaneLayer(datumPlaneLayer)
Parameters: datumPlaneLayer (int) – New in version NX5.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”)
DatumPlanes¶
-
SectionInertiaAnalysisBuilder.
DatumPlanes
¶ Returns or sets the datum planes
-------------------------------------
Getter Method
Signature
DatumPlanes()
Returns: Return type: bool New in version NX5.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
DatumPlanes(datumPlanes)
Parameters: datumPlanes (bool) – New in version NX5.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”)
Distance¶
-
SectionInertiaAnalysisBuilder.
Distance
¶ Returns the distance
-------------------------------------
Getter Method
Signature
Distance()
Returns: Return type: NXOpen.Expression
New in version NX5.0.0.
License requirements: None.
FaceCollector¶
-
SectionInertiaAnalysisBuilder.
FaceCollector
¶ Returns the face collector
-------------------------------------
Getter Method
Signature
FaceCollector()
Returns: Return type: NXOpen.ScCollector
New in version NX5.0.0.
License requirements: None.
MassPropertyType¶
-
SectionInertiaAnalysisBuilder.
MassPropertyType
¶ Returns or sets the mass property type
-------------------------------------
Getter Method
Signature
MassPropertyType()
Returns: Return type: NXOpen.Features.SectionInertiaAnalysisBuilderPropertyType
New in version NX5.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
MassPropertyType(massPropertyType)
Parameters: massPropertyType ( NXOpen.Features.SectionInertiaAnalysisBuilderPropertyType
) –New in version NX5.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”)
NSection¶
-
SectionInertiaAnalysisBuilder.
NSection
¶ Returns or sets the n section
-------------------------------------
Getter Method
Signature
NSection()
Returns: Return type: int New in version NX5.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
NSection(nSection)
Parameters: nSection (int) – New in version NX5.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”)
PathCollector¶
-
SectionInertiaAnalysisBuilder.
PathCollector
¶ Returns the path collector
-------------------------------------
Getter Method
Signature
PathCollector()
Returns: Return type: NXOpen.Section
New in version NX5.0.0.
License requirements: None.
PrincipalAxes¶
-
SectionInertiaAnalysisBuilder.
PrincipalAxes
¶ Returns or sets the principal axes
-------------------------------------
Getter Method
Signature
PrincipalAxes()
Returns: Return type: bool New in version NX5.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
PrincipalAxes(principalAxes)
Parameters: principalAxes (bool) – New in version NX5.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”)
RectangleLayer¶
-
SectionInertiaAnalysisBuilder.
RectangleLayer
¶ Returns or sets the rectangle layer
-------------------------------------
Getter Method
Signature
RectangleLayer()
Returns: Return type: int New in version NX5.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
RectangleLayer(rectangleLayer)
Parameters: rectangleLayer (int) – New in version NX5.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”)
RectangularSection¶
-
SectionInertiaAnalysisBuilder.
RectangularSection
¶ Returns or sets the rectangular section
-------------------------------------
Getter Method
Signature
RectangularSection()
Returns: Return type: bool New in version NX5.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
RectangularSection(rectangularSection)
Parameters: rectangularSection (bool) – New in version NX5.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”)
SecondPrincipleMi¶
-
SectionInertiaAnalysisBuilder.
SecondPrincipleMi
¶ Returns or sets the second principle mi
-------------------------------------
Getter Method
Signature
SecondPrincipleMi()
Returns: Return type: bool New in version NX5.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
SecondPrincipleMi(secondPrincipleMI)
Parameters: secondPrincipleMI (bool) – New in version NX5.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”)
SectionArea¶
-
SectionInertiaAnalysisBuilder.
SectionArea
¶ Returns or sets the section area
-------------------------------------
Getter Method
Signature
SectionArea()
Returns: Return type: bool New in version NX5.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
SectionArea(sectionArea)
Parameters: sectionArea (bool) – New in version NX5.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”)
SectionLayer¶
-
SectionInertiaAnalysisBuilder.
SectionLayer
¶ Returns or sets the section layer
-------------------------------------
Getter Method
Signature
SectionLayer()
Returns: Return type: int New in version NX5.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
SectionLayer(sectionLayer)
Parameters: sectionLayer (int) – New in version NX5.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”)
SectionLength¶
-
SectionInertiaAnalysisBuilder.
SectionLength
¶ Returns or sets the section length
-------------------------------------
Getter Method
Signature
SectionLength()
Returns: Return type: bool New in version NX5.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
SectionLength(sectionLength)
Parameters: sectionLength (bool) – New in version NX5.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”)
SectionNormal¶
-
SectionInertiaAnalysisBuilder.
SectionNormal
¶ Returns or sets the section normal
-------------------------------------
Getter Method
Signature
SectionNormal()
Returns: Return type: NXOpen.Features.SectionInertiaAnalysisBuilderSectionAxisNormal
New in version NX5.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
SectionNormal(sectionNormal)
Parameters: sectionNormal ( NXOpen.Features.SectionInertiaAnalysisBuilderSectionAxisNormal
) –New in version NX5.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”)
SectioningMethod¶
-
SectionInertiaAnalysisBuilder.
SectioningMethod
¶ Returns or sets the sectioning method
-------------------------------------
Getter Method
Signature
SectioningMethod()
Returns: Return type: NXOpen.Features.SectionInertiaAnalysisBuilderSampleMethod
New in version NX5.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
SectioningMethod(sectioningMethod)
Parameters: sectioningMethod ( NXOpen.Features.SectionInertiaAnalysisBuilderSampleMethod
) –New in version NX5.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”)
Sections¶
-
SectionInertiaAnalysisBuilder.
Sections
¶ Returns or sets the sections
-------------------------------------
Getter Method
Signature
Sections()
Returns: Return type: bool New in version NX5.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Sections(sections)
Parameters: sections (bool) – New in version NX5.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”)
ShearCenter¶
-
SectionInertiaAnalysisBuilder.
ShearCenter
¶ Returns or sets the shear center
-------------------------------------
Getter Method
Signature
ShearCenter()
Returns: Return type: bool New in version NX5.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ShearCenter(shearCenter)
Parameters: shearCenter (bool) – New in version NX5.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”)
Thickness¶
-
SectionInertiaAnalysisBuilder.
Thickness
¶ Returns the thickness.
This attribute is always used in hollow analysis while it is used in solid analysis if any of the loops is open.
-------------------------------------
Getter Method
Signature
Thickness()
Returns: Return type: NXOpen.Expression
New in version NX5.0.0.
License requirements: None.
Type¶
-
SectionInertiaAnalysisBuilder.
Type
¶ Returns or sets the analysis
-------------------------------------
Getter Method
Signature
Type()
Returns: Return type: NXOpen.Features.SectionInertiaAnalysisBuilderTypes
New in version NX5.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Type(type)
Parameters: type ( NXOpen.Features.SectionInertiaAnalysisBuilderTypes
) –New in version NX5.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”)
Units¶
-
SectionInertiaAnalysisBuilder.
Units
¶ Returns or sets the units for calculations
-------------------------------------
Getter Method
Signature
Units()
Returns: Return type: int New in version NX5.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Units(units)
Parameters: units (int) – New in version NX5.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”)
ValidityFlag¶
-
SectionInertiaAnalysisBuilder.
ValidityFlag
¶ Returns or sets the validity flag.
If the flag is set to false, properties will be recomputed.
-------------------------------------
Getter Method
Signature
ValidityFlag()
Returns: Return type: bool New in version NX5.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ValidityFlag(validityFlag)
Parameters: validityFlag (bool) – New in version NX5.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”)
Method Detail¶
GetAnnotation¶
-
SectionInertiaAnalysisBuilder.
GetAnnotation
¶ The annotations generated can be accessed using this method.
Signature
GetAnnotation()
Returns: The annotation notes created. Pass NULL to get only the number. Return type: list of NXOpen.Annotations.PmiNote
New in version NX5.0.0.
License requirements: None.
IsTempGraphics¶
-
SectionInertiaAnalysisBuilder.
IsTempGraphics
¶ The function checks if temporary graphics was generated.
Signature
IsTempGraphics()
Returns: Return type: bool New in version NX5.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”)
RefreshScreen¶
-
SectionInertiaAnalysisBuilder.
RefreshScreen
¶ The function refreshes the graphic screen if any temporary graphics was previously generated by this command.
Signature
RefreshScreen()
New in version NX5.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”)
ShowInfo¶
-
SectionInertiaAnalysisBuilder.
ShowInfo
¶ The function displays the information box with information about the section intertia analysis performed.
Signature
ShowInfo()
New in version NX5.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”)
Validate¶
-
SectionInertiaAnalysisBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.