SectionInertiaAnalysisBuilderCoordSys Enumeration¶
NXOpen.Features.SectionInertiaAnalysisBuilder.CoordSys is an alias for NXOpen.Features.SectionInertiaAnalysisBuilderCoordSys
-
class
NXOpen.Features.
SectionInertiaAnalysisBuilderCoordSys
¶ Bases:
object
The coordinate system associated with the analysis.
Enum Members
Enum Member Enum Member Description Absolute Absolute Coordinate System CurrentWCS World Coordinate System -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-