SectionInertiaAnalysisBuilderSampleMethod Enumeration¶
NXOpen.Features.SectionInertiaAnalysisBuilder.SampleMethod is an alias for NXOpen.Features.SectionInertiaAnalysisBuilderSampleMethod
-
class
NXOpen.Features.
SectionInertiaAnalysisBuilderSampleMethod
¶ Bases:
object
Type of sampling method to be used in sections along curve type of analysis.
Enum Members
Enum Member Enum Member Description ByDistance Sample according to Distance ByNumber Sample according to Number of slices -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-