CopyPasteBuilder Class¶
-
class
NXOpen.Features.
CopyPasteBuilder
¶ Bases:
NXOpen.Builder
Represents a
NXOpen.Features.CopyPasteBuilder
To create a new instance of this class, use
NXOpen.Features.FeatureCollection.CreateCopyPasteBuilder2
New in version NX6.0.0.
Properties¶
Property | Description |
---|---|
Associative | Returns or sets the associative toggle |
CopyResolveGeometry | Returns or sets the copy resolving geometry toggle |
ExpressionOption | Returns or sets the expression option |
ParentOption | Returns or sets the parent option |
SelectOption | Returns or sets the parent select option. |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetBuilderVersion | The builder version getting function @return |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetFeatureReferences | Returns the feature references builder @return |
GetObject | Returns the object currently being edited by this builder. |
SetBuilderVersion | The builder version setting function. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
UpdateBuilder | The update builder function, needs to be called after parent select option is reset |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Enumerations¶
CopyPasteBuilderBuilderVersion Enumeration | Types of version number |
CopyPasteBuilderExpressionTransferOption Enumeration | Types of expression transfer mode |
CopyPasteBuilderParentSelectOption Enumeration | Types of parent select option; Specifying smart object or selecting input for original parent |
CopyPasteBuilderParentTransferOption Enumeration | Types of parent transfer mode |
Property Detail¶
Associative¶
-
CopyPasteBuilder.
Associative
¶ Returns or sets the associative toggle
-------------------------------------
Getter Method
Signature
Associative()
Returns: Return type: bool New in version NX8.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Associative(associative)
Parameters: associative (bool) – New in version NX8.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”)
CopyResolveGeometry¶
-
CopyPasteBuilder.
CopyResolveGeometry
¶ Returns or sets the copy resolving geometry toggle
-------------------------------------
Getter Method
Signature
CopyResolveGeometry()
Returns: Return type: bool New in version NX8.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
CopyResolveGeometry(copyResolveGeometry)
Parameters: copyResolveGeometry (bool) – New in version NX8.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”)
ExpressionOption¶
-
CopyPasteBuilder.
ExpressionOption
¶ Returns or sets the expression option
-------------------------------------
Getter Method
Signature
ExpressionOption()
Returns: Return type: NXOpen.Features.CopyPasteBuilderExpressionTransferOption
New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ExpressionOption(expressionOption)
Parameters: expressionOption ( NXOpen.Features.CopyPasteBuilderExpressionTransferOption
) –New in version NX6.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”)
ParentOption¶
-
CopyPasteBuilder.
ParentOption
¶ Returns or sets the parent option
-------------------------------------
Getter Method
Signature
ParentOption()
Returns: Return type: NXOpen.Features.CopyPasteBuilderParentTransferOption
New in version NX6.0.0.
Deprecated since version NX8.0.0: This functionality is no longer supported.
License requirements: None.
-------------------------------------
Setter Method
Signature
ParentOption(parentOption)
Parameters: parentOption ( NXOpen.Features.CopyPasteBuilderParentTransferOption
) –New in version NX6.0.0.
Deprecated since version NX8.0.0: This functionality is no longer supported.
License requirements: solid_modeling (“SOLIDS MODELING”)
SelectOption¶
-
CopyPasteBuilder.
SelectOption
¶ Returns or sets the parent select option.
This option allows the user to control if the input smart objects for the copied feature should have all the input smart object creation methods available from the parent feature or only use the smart object creation method selected on the original parent
-------------------------------------
Getter Method
Signature
SelectOption()
Returns: Return type: NXOpen.Features.CopyPasteBuilderParentSelectOption
New in version NX8.5.1.
License requirements: None.
-------------------------------------
Setter Method
Signature
SelectOption(selectionOption)
Parameters: selectionOption ( NXOpen.Features.CopyPasteBuilderParentSelectOption
) –New in version NX8.5.1.
License requirements: solid_modeling (“SOLIDS MODELING”)
Method Detail¶
GetBuilderVersion¶
-
CopyPasteBuilder.
GetBuilderVersion
¶ The builder version getting function
Signature
GetBuilderVersion()
Returns: Return type: NXOpen.Features.CopyPasteBuilderBuilderVersion
New in version NX8.5.0.
License requirements: solid_modeling (“SOLIDS MODELING”)
GetFeatureReferences¶
-
CopyPasteBuilder.
GetFeatureReferences
¶ Returns the feature references builder
Signature
GetFeatureReferences()
Returns: Return type: NXOpen.Features.FeatureReferencesBuilder
New in version NX6.0.0.
License requirements: None.
SetBuilderVersion¶
-
CopyPasteBuilder.
SetBuilderVersion
¶ The builder version setting function.
This function sets builder version number with value which is treated as bit field. It still uses the enumeration defined in previous releases. In order to set the builder version number to the correct value, the version number could be calculated by a bitwise or operation on previous releases versions number, or by an addition of previous releases versions number.
Signature
SetBuilderVersion(version)
Parameters: version ( NXOpen.Features.CopyPasteBuilderBuilderVersion
) –New in version NX8.5.0.
License requirements: solid_modeling (“SOLIDS MODELING”)
UpdateBuilder¶
-
CopyPasteBuilder.
UpdateBuilder
¶ The update builder function, needs to be called after parent select option is reset
Signature
UpdateBuilder()
New in version NX8.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”)
Validate¶
-
CopyPasteBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.