CopyPasteBuilderBuilderVersion Enumeration¶
NXOpen.Features.CopyPasteBuilder.BuilderVersion is an alias for NXOpen.Features.CopyPasteBuilderBuilderVersion
-
class
NXOpen.Features.
CopyPasteBuilderBuilderVersion
¶ Bases:
object
Types of version number
Enum Members
Enum Member Enum Member Description Original Value of original version; It can be set before NX8.0.ExposeOnflySo Value of version which exposes smart object created on fly as part of the copy operation; It should be set since NX8.0.ExposeBody Value of version which exposes additional target body parent; It should be added since NX8.5.ShowParentSelectOption Value of version which introduces parent select option; It should be added since NX8.5.1.-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-