CopyPasteBuilderParentSelectOption Enumeration¶
NXOpen.Features.CopyPasteBuilder.ParentSelectOption is an alias for NXOpen.Features.CopyPasteBuilderParentSelectOption
-
class
NXOpen.Features.
CopyPasteBuilderParentSelectOption
¶ Bases:
object
Types of parent select option; Specifying smart object or selecting input for original parent
Enum Members
- copied feature may be selected from the creation methods that were available on the original feature. “
- “InputForOriginalParent”, ” Specifying smart object using the same creation method that was used in the original feature. “
-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.