CombinedProjectionBuilder Class¶
-
class
NXOpen.Features.
CombinedProjectionBuilder
¶ Bases:
NXOpen.Features.FeatureBuilder
Represents a
NXOpen.Features.CombinedProjection
builderTo create a new instance of this class, use
NXOpen.Features.FeatureCollection.CreateCombinedProjectionBuilder
Default values.
Property Value CurveFit.FitOption Cubic CurveFit.MaximumDegree 7 CurveFit.MaximumSegments 1 New in version NX6.0.0.
Properties¶
Property | Description |
---|---|
Curve1 | Returns the combined projection curve1 |
Curve2 | Returns the combined projection curve2 |
CurveFit | Returns the combined projection curveFit |
CurveOptions | Returns the combined projection curveOptions |
Direction1 | Returns the combined projection direction1 |
Direction2 | Returns the combined projection direction2 |
ParentFeatureInternal | Returns or sets whether or not the latest timestamped parent feature of this feature should be made internal |
PatchSolutionFlag | Returns or sets the patch solution flag |
PatchSurfaceFilename | Returns or sets the patch surface filename |
SurroundingPatchSurfaceFilename | Returns or sets the surrounding patch surface filename |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
CommitFeature | Commits the feature parameters and creates the feature @return |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetFeature | Returns the feature currently being edited by this builder. |
GetObject | Returns the object currently being edited by this builder. |
HideInternalParentFeatureAfterEdit | Re-suppress an internal parent feature (a slave feature) after it has been edited. |
SetParentFeatureInternal | Set the parent features which would be internal or slaves to the feature being created or commited |
ShowInternalParentFeatureForEdit | Unsuppress an internal parent feature (a slave feature) so it can be edited. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
UnsetParentFeatureInternal | Set the internal parent feature of the feature being edited to external |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Property Detail¶
Curve1¶
-
CombinedProjectionBuilder.
Curve1
¶ Returns the combined projection curve1
-------------------------------------
Getter Method
Signature
Curve1()
Returns: Return type: NXOpen.Section
New in version NX6.0.0.
License requirements: None.
Curve2¶
-
CombinedProjectionBuilder.
Curve2
¶ Returns the combined projection curve2
-------------------------------------
Getter Method
Signature
Curve2()
Returns: Return type: NXOpen.Section
New in version NX6.0.0.
License requirements: None.
CurveFit¶
-
CombinedProjectionBuilder.
CurveFit
¶ Returns the combined projection curveFit
-------------------------------------
Getter Method
Signature
CurveFit()
Returns: Return type: NXOpen.GeometricUtilities.CurveFitOptions
New in version NX6.0.0.
License requirements: None.
CurveOptions¶
-
CombinedProjectionBuilder.
CurveOptions
¶ Returns the combined projection curveOptions
-------------------------------------
Getter Method
Signature
CurveOptions()
Returns: Return type: NXOpen.GeometricUtilities.CurveOptions
New in version NX6.0.0.
License requirements: None.
Direction1¶
-
CombinedProjectionBuilder.
Direction1
¶ Returns the combined projection direction1
-------------------------------------
Getter Method
Signature
Direction1()
Returns: Return type: NXOpen.GeometricUtilities.ProjectionOptions
New in version NX6.0.0.
License requirements: None.
Direction2¶
-
CombinedProjectionBuilder.
Direction2
¶ Returns the combined projection direction2
-------------------------------------
Getter Method
Signature
Direction2()
Returns: Return type: NXOpen.GeometricUtilities.ProjectionOptions
New in version NX6.0.0.
License requirements: None.
Method Detail¶
Validate¶
-
CombinedProjectionBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.