CurveOptions Class¶
-
class
NXOpen.GeometricUtilities.
CurveOptions
¶ Bases:
NXOpen.TaggedObject
,NXOpen.GeometricUtilities.IComponentBuilder
Represents the curve options data
New in version NX5.0.0.
Properties¶
Property | Description |
---|---|
Associative | Returns or sets the associativity option |
InputCurveOption | Returns or sets the curve options |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Enumerations¶
CurveOptionsInputCurve Enumeration | Represents the input curve options |
Property Detail¶
Associative¶
-
CurveOptions.
Associative
¶ Returns or sets the associativity option
-------------------------------------
Getter Method
Signature
Associative()
Returns: associativity Return type: bool New in version NX5.0.0.
License requirements: features_modeling (“FEATURES MODELING”) OR cam_base (“CAM BASE”)
-------------------------------------
Setter Method
Signature
Associative(associative)
Parameters: associative (bool) – associativity New in version NX5.0.0.
License requirements: features_modeling (“FEATURES MODELING”) OR cam_base (“CAM BASE”)
InputCurveOption¶
-
CurveOptions.
InputCurveOption
¶ Returns or sets the curve options
-------------------------------------
Getter Method
Signature
InputCurveOption()
Returns: curve options Return type: NXOpen.GeometricUtilities.CurveOptionsInputCurve
New in version NX5.0.0.
License requirements: features_modeling (“FEATURES MODELING”) OR cam_base (“CAM BASE”)
-------------------------------------
Setter Method
Signature
InputCurveOption(inputCurveOption)
Parameters: inputCurveOption ( NXOpen.GeometricUtilities.CurveOptionsInputCurve
) – curve optionsNew in version NX5.0.0.
License requirements: features_modeling (“FEATURES MODELING”) OR cam_base (“CAM BASE”)
Method Detail¶
Validate¶
-
CurveOptions.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.