SectionLineBuilder Class¶
-
class
NXOpen.Drawings.
SectionLineBuilder
¶ Bases:
NXOpen.Builder
Represents a
NXOpen.Drawings.SectionLineBuilder
.This class is used to create or edit a
NXOpen.Drawings.SectionLine
. To create a new instance of this class, useNXOpen.Drawings.SectionLineCollection.CreateSectionLineBuilder
New in version NX6.0.0.
Deprecated since version NX10.0.0: Use
NXOpen.Drawings.SectionViewBuilder.SectionLineType
Properties¶
Property | Description |
---|---|
ArrowDirection | Returns or sets the arrow direction. |
CutDirection | Returns or sets the cut direction. |
Half | Returns the half section line data. |
HalfPictorial | Returns the half pictorial section line data. |
HingeDirection | Returns or sets the hinge direction. |
Oriented | Returns the simple 3D section line data. |
ParentView | Returns the parent view. |
Pictorial | Returns the pictorial section line data. |
PointAndAngle | Returns the point and angle section line data. |
PointToPoint | Returns the point to point section line data. |
Revolved | Returns the revolved section line data. |
SimpleOrStepped | Returns the simple or stepped section line data. |
Style | Returns the style. |
Tag | Returns the Tag for this object. |
Type | Returns or sets the section line type |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetObject | Returns the object currently being edited by this builder. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Enumerations¶
SectionLineBuilderTypes Enumeration | Section Line type |
Property Detail¶
ArrowDirection¶
-
SectionLineBuilder.
ArrowDirection
¶ Returns or sets the arrow direction.
The arrow direction defines the direction of the section line arrows and must be perpendicular to the cut direction.
The arrow direction is only used for
NXOpen.Drawings.SectionLineBuilderTypes.Pictorial
,NXOpen.Drawings.SectionLineBuilderTypes.HalfPictorial
andNXOpen.Drawings.SectionLineBuilderTypes.Oriented
section lines-------------------------------------
Getter Method
Signature
ArrowDirection()
Returns: Return type: NXOpen.Direction
New in version NX6.0.0.
Deprecated since version NX10.0.0: This API is not supported yet and should not be used.
License requirements: None.
-------------------------------------
Setter Method
Signature
ArrowDirection(arrowDirection)
Parameters: arrowDirection ( NXOpen.Direction
) –New in version NX6.0.0.
Deprecated since version NX10.0.0: This API is not supported yet and should not be used.
License requirements: drafting (“DRAFTING”)
CutDirection¶
-
SectionLineBuilder.
CutDirection
¶ Returns or sets the cut direction.
The cut direction is a vector that specifies the direction of the cutting plane. A vector arrow displays showing the direction of the vector.
The cut direction is only used for
NXOpen.Drawings.SectionLineBuilderTypes.Pictorial
,NXOpen.Drawings.SectionLineBuilderTypes.HalfPictorial
andNXOpen.Drawings.SectionLineBuilderTypes.Oriented
section lines-------------------------------------
Getter Method
Signature
CutDirection()
Returns: Return type: NXOpen.Direction
New in version NX6.0.0.
Deprecated since version NX10.0.0: This API is not supported yet and should not be used.
License requirements: None.
-------------------------------------
Setter Method
Signature
CutDirection(cutDirection)
Parameters: cutDirection ( NXOpen.Direction
) –New in version NX6.0.0.
Deprecated since version NX10.0.0: This API is not supported yet and should not be used.
License requirements: drafting (“DRAFTING”)
Half¶
-
SectionLineBuilder.
Half
¶ Returns the half section line data.
Use the half section line data when the type is set to
NXOpen.Drawings.SectionLineBuilderTypes.Half
-------------------------------------
Getter Method
Signature
Half()
Returns: Return type: NXOpen.Drawings.HalfSectionLineBuilder
New in version NX6.0.0.
Deprecated since version NX10.0.0: Use
Drawings.SectionViewBuilder.SectionViewType
License requirements: None.
HalfPictorial¶
-
SectionLineBuilder.
HalfPictorial
¶ Returns the half pictorial section line data.
Use the half pictorial section line data when the type is set to
NXOpen.Drawings.SectionLineBuilderTypes.HalfPictorial
-------------------------------------
Getter Method
Signature
HalfPictorial()
Returns: Return type: NXOpen.Drawings.HalfSectionLineBuilder
New in version NX6.0.0.
Deprecated since version NX10.0.0: This API is not supported yet and should not be used.
License requirements: None.
HingeDirection¶
-
SectionLineBuilder.
HingeDirection
¶ Returns or sets the hinge direction.
The hinge direction is only used for
NXOpen.Drawings.SectionLineBuilderTypes.SimpleOrStepped
,NXOpen.Drawings.SectionLineBuilderTypes.Half
,NXOpen.Drawings.SectionLineBuilderTypes.Revolved
,NXOpen.Drawings.SectionLineBuilderTypes.PointToPoint
, andNXOpen.Drawings.SectionLineBuilderTypes.PointAndAngle
section lines-------------------------------------
Getter Method
Signature
HingeDirection()
Returns: Return type: NXOpen.Direction
New in version NX6.0.0.
Deprecated since version NX10.0.0: Use
Drawings.ViewStyleOrientationBuilder.HingeLine
License requirements: None.
-------------------------------------
Setter Method
Signature
HingeDirection(hingeDirection)
Parameters: hingeDirection ( NXOpen.Direction
) –New in version NX6.0.0.
Deprecated since version NX10.0.0: Use
Drawings.ViewStyleOrientationBuilder.HingeLine
License requirements: drafting (“DRAFTING”)
Oriented¶
-
SectionLineBuilder.
Oriented
¶ Returns the simple 3D section line data.
Use the simple 3D section line data when the type is set to
NXOpen.Drawings.SectionLineBuilderTypes.Oriented
-------------------------------------
Getter Method
Signature
Oriented()
Returns: Return type: NXOpen.Drawings.OrientedSectionLineBuilder
New in version NX6.0.0.
Deprecated since version NX10.0.0: This API is not supported yet and should not be used.
License requirements: None.
ParentView¶
-
SectionLineBuilder.
ParentView
¶ Returns the parent view.
The view that the section line will cut.
-------------------------------------
Getter Method
Signature
ParentView()
Returns: Return type: NXOpen.Drawings.ParentViewBuilder
New in version NX6.0.0.
Deprecated since version NX10.0.0: Use
Drawings.SectionViewBuilder.ParentView
License requirements: None.
Pictorial¶
-
SectionLineBuilder.
Pictorial
¶ Returns the pictorial section line data.
Use the pictorial section line data when the type is set to
NXOpen.Drawings.SectionLineBuilderTypes.Pictorial
-------------------------------------
Getter Method
Signature
Pictorial()
Returns: Return type: NXOpen.Drawings.SteppedSectionLineBuilder
New in version NX6.0.0.
Deprecated since version NX10.0.0: This API is not supported yet and should not be used.
License requirements: None.
PointAndAngle¶
-
SectionLineBuilder.
PointAndAngle
¶ Returns the point and angle section line data.
Use the point and angle section line data when the type is set to
NXOpen.Drawings.SectionLineBuilderTypes.PointAndAngle
-------------------------------------
Getter Method
Signature
PointAndAngle()
Returns: Return type: NXOpen.Drawings.PointAndAngleSectionLineBuilder
New in version NX6.0.0.
Deprecated since version NX10.0.0: This API is not supported yet and should not be used.
License requirements: None.
PointToPoint¶
-
SectionLineBuilder.
PointToPoint
¶ Returns the point to point section line data.
Use the point to point section line data when the type is set to
NXOpen.Drawings.SectionLineBuilderTypes.PointToPoint
-------------------------------------
Getter Method
Signature
PointToPoint()
Returns: Return type: NXOpen.Drawings.PointToPointSectionLineBuilder
New in version NX6.0.0.
Deprecated since version NX10.0.0: Use
Drawings.SectionViewBuilder.SectionViewType
License requirements: None.
Revolved¶
-
SectionLineBuilder.
Revolved
¶ Returns the revolved section line data.
Use the revolved section line data when the type is set to
NXOpen.Drawings.SectionLineBuilderTypes.Revolved
-------------------------------------
Getter Method
Signature
Revolved()
Returns: Return type: NXOpen.Drawings.RevolvedSectionLineBuilder
New in version NX6.0.0.
Deprecated since version NX10.0.0: Use
Drawings.SectionViewBuilder.SectionViewType
License requirements: None.
SimpleOrStepped¶
-
SectionLineBuilder.
SimpleOrStepped
¶ Returns the simple or stepped section line data.
Use the simple or stepped section line data when the type is set to
NXOpen.Drawings.SectionLineBuilderTypes.SimpleOrStepped
-------------------------------------
Getter Method
Signature
SimpleOrStepped()
Returns: Return type: NXOpen.Drawings.SteppedSectionLineBuilder
New in version NX6.0.0.
Deprecated since version NX10.0.0: Use
Drawings.SectionViewBuilder.SectionViewType
License requirements: None.
Style¶
-
SectionLineBuilder.
Style
¶ Returns the style.
The preferences of a section line.
-------------------------------------
Getter Method
Signature
Style()
Returns: Return type: NXOpen.Drawings.SectionLineStyleBuilder
New in version NX6.0.0.
Deprecated since version NX10.0.0: Use
Drawings.SectionViewBuilder.ViewStyle
License requirements: None.
Type¶
-
SectionLineBuilder.
Type
¶ Returns or sets the section line type
-------------------------------------
Getter Method
Signature
Type()
Returns: Return type: NXOpen.Drawings.SectionLineBuilderTypes
New in version NX6.0.0.
Deprecated since version NX10.0.0: Use
Drawings.SectionViewBuilder.SectionViewType
License requirements: None.
-------------------------------------
Setter Method
Signature
Type(type)
Parameters: type ( NXOpen.Drawings.SectionLineBuilderTypes
) –New in version NX6.0.0.
Deprecated since version NX10.0.0: Use
Drawings.SectionViewBuilder.SectionViewType
License requirements: drafting (“DRAFTING”)
Method Detail¶
Validate¶
-
SectionLineBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.