SectionLineBuilderTypes Enumeration¶
NXOpen.Drawings.SectionLineBuilder.Types is an alias for NXOpen.Drawings.SectionLineBuilderTypes
-
class
NXOpen.Drawings.
SectionLineBuilderTypes
¶ Bases:
object
Section Line type
Enum Members
Enum Member Enum Member Description SimpleOrStepped Creates or edits aNXOpen.Drawings.SteppedSectionLine
Half Creates or edits aNXOpen.Drawings.HalfSectionLine
Revolved Creates or edits aNXOpen.Drawings.RevolvedSectionLine
PointToPoint Creates or edits aNXOpen.Drawings.PointToPointSectionLine
PointAndAngle Creates or edits aNXOpen.Drawings.PointAndAngleSectionLine
Pictorial Creates or edits aNXOpen.Drawings.PictorialSectionLine
HalfPictorial Creates or edits aNXOpen.Drawings.HalfPictorialSectionLine
Oriented Creates or edits aNXOpen.Drawings.OrientedSectionLine
-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-