SectionLineStyleBuilder Class¶
-
class
NXOpen.Drawings.
SectionLineStyleBuilder
¶ Bases:
NXOpen.Builder
Represents a Drawings.
SectionLineStyleBuiler. The SectionLineStyleBuilder is used to specify section line style.
To create a new instance of this class, use
NXOpen.Drawings.SectionLineCollection.CreateSectionLineStyleBuilder
New in version NX6.0.0.
Properties¶
Property | Description |
---|---|
ArrowLength | Returns or sets the arrow length |
ArrowheadAngle | Returns or sets the arrowhead angle |
ArrowheadLength | Returns or sets the arrowhead length |
ArrowheadStyle | Returns or sets the arrowhead style |
BorderToArrowDistance | Returns or sets the border to arrow distance |
CreateSectionLine | Returns or sets a value that indicates whether or not to create a view for the section line |
DisplayJisrotationLetter | Returns or sets the display jisrotation letter |
DisplayLabel | Returns or sets the display label |
Font | Returns or sets the font |
LabelLocation | Returns or sets the label location |
Letter | Returns or sets the letter |
LineLength | Returns or sets the line length |
Offset | Returns or sets the offset |
SelectLetter | Returns the selected note for jisrotation letter |
Standard | Returns or sets the standard |
StubLength | Returns or sets the stub length |
Tag | Returns the Tag for this object. |
UseOffset | Returns or sets the use offset |
Width | Returns or sets the width |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetColor | Returns the color @return |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetObject | Returns the object currently being edited by this builder. |
SetColor | Sets the color |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Enumerations¶
SectionLineStyleBuilderArrowheadStyleType Enumeration | This enum represents arrowhead style type. |
SectionLineStyleBuilderCreateSectionLineType Enumeration | This enum represents whether or not to create a view for the section line. |
SectionLineStyleBuilderFontStyle Enumeration | This enum represents section line font style type. |
SectionLineStyleBuilderLabelLocationStyle Enumeration | This enum represents section line label location for ISO128 section lines. |
SectionLineStyleBuilderStandardStyle Enumeration | This enum represents section line standard style type. |
SectionLineStyleBuilderWidthStyle Enumeration | This enum represents section line width style type. |
Property Detail¶
ArrowLength¶
-
SectionLineStyleBuilder.
ArrowLength
¶ Returns or sets the arrow length
-------------------------------------
Getter Method
Signature
ArrowLength()
Returns: Return type: float New in version NX6.0.0.
Deprecated since version NX10.0.0: Use
NXOpen.Drawings.ViewSectionLineBuilder.ArrowLength
instead.License requirements: None.
-------------------------------------
Setter Method
Signature
ArrowLength(arrowLength)
Parameters: arrowLength (float) – New in version NX6.0.0.
Deprecated since version NX10.0.0: Use
NXOpen.Drawings.ViewSectionLineBuilder.ArrowLength
instead.License requirements: drafting (“DRAFTING”)
ArrowheadAngle¶
-
SectionLineStyleBuilder.
ArrowheadAngle
¶ Returns or sets the arrowhead angle
-------------------------------------
Getter Method
Signature
ArrowheadAngle()
Returns: Return type: float New in version NX6.0.0.
Deprecated since version NX10.0.0: Use
NXOpen.Drawings.ViewSectionLineBuilder.ArrowheadAngle
instead.License requirements: None.
-------------------------------------
Setter Method
Signature
ArrowheadAngle(arrowheadAngle)
Parameters: arrowheadAngle (float) – New in version NX6.0.0.
Deprecated since version NX10.0.0: Use
NXOpen.Drawings.ViewSectionLineBuilder.ArrowheadAngle
instead.License requirements: drafting (“DRAFTING”)
ArrowheadLength¶
-
SectionLineStyleBuilder.
ArrowheadLength
¶ Returns or sets the arrowhead length
-------------------------------------
Getter Method
Signature
ArrowheadLength()
Returns: Return type: float New in version NX6.0.0.
Deprecated since version NX10.0.0: Use
NXOpen.Drawings.ViewSectionLineBuilder.ArrowheadLength
instead.License requirements: None.
-------------------------------------
Setter Method
Signature
ArrowheadLength(arrowheadLength)
Parameters: arrowheadLength (float) – New in version NX6.0.0.
Deprecated since version NX10.0.0: Use
NXOpen.Drawings.ViewSectionLineBuilder.ArrowheadLength
instead.License requirements: drafting (“DRAFTING”)
ArrowheadStyle¶
-
SectionLineStyleBuilder.
ArrowheadStyle
¶ Returns or sets the arrowhead style
-------------------------------------
Getter Method
Signature
ArrowheadStyle()
Returns: Return type: NXOpen.Drawings.SectionLineStyleBuilderArrowheadStyleType
New in version NX6.0.0.
Deprecated since version NX10.0.0: Use
NXOpen.Drawings.ViewSectionLineBuilder.Style
instead.License requirements: None.
-------------------------------------
Setter Method
Signature
ArrowheadStyle(arrowheadStyle)
Parameters: arrowheadStyle ( NXOpen.Drawings.SectionLineStyleBuilderArrowheadStyleType
) –New in version NX6.0.0.
Deprecated since version NX10.0.0: Use
NXOpen.Drawings.ViewSectionLineBuilder.Style
instead.License requirements: drafting (“DRAFTING”)
BorderToArrowDistance¶
-
SectionLineStyleBuilder.
BorderToArrowDistance
¶ Returns or sets the border to arrow distance
-------------------------------------
Getter Method
Signature
BorderToArrowDistance()
Returns: Return type: float New in version NX6.0.0.
Deprecated since version NX10.0.0: Use
NXOpen.Drawings.ViewSectionLineBuilder.BorderToArrowDistance
instead.License requirements: None.
-------------------------------------
Setter Method
Signature
BorderToArrowDistance(borderToArrowDistance)
Parameters: borderToArrowDistance (float) – New in version NX6.0.0.
Deprecated since version NX10.0.0: Use
NXOpen.Drawings.ViewSectionLineBuilder.BorderToArrowDistance
instead.License requirements: drafting (“DRAFTING”)
CreateSectionLine¶
-
SectionLineStyleBuilder.
CreateSectionLine
¶ Returns or sets a value that indicates whether or not to create a view for the section line
-------------------------------------
Getter Method
Signature
CreateSectionLine()
Returns: Return type: NXOpen.Drawings.SectionLineStyleBuilderCreateSectionLineType
New in version NX6.0.0.
Deprecated since version NX10.0.0: Use
NXOpen.Drawings.ViewSectionLineBuilder.ShowSectionLine
instead.License requirements: None.
-------------------------------------
Setter Method
Signature
CreateSectionLine(createSectionLine)
Parameters: createSectionLine ( NXOpen.Drawings.SectionLineStyleBuilderCreateSectionLineType
) –New in version NX6.0.0.
Deprecated since version NX10.0.0: Use
NXOpen.Drawings.ViewSectionLineBuilder.ShowSectionLine
instead.License requirements: drafting (“DRAFTING”)
DisplayJisrotationLetter¶
-
SectionLineStyleBuilder.
DisplayJisrotationLetter
¶ Returns or sets the display jisrotation letter
-------------------------------------
Getter Method
Signature
DisplayJisrotationLetter()
Returns: Return type: bool New in version NX6.0.0.
Deprecated since version NX10.0.0: Use
NXOpen.Drawings.ViewSectionLineBuilder.DisplayRotationLetter
instead.License requirements: None.
-------------------------------------
Setter Method
Signature
DisplayJisrotationLetter(displayJISRotationLetter)
Parameters: displayJISRotationLetter (bool) – New in version NX6.0.0.
Deprecated since version NX10.0.0: Use
NXOpen.Drawings.ViewSectionLineBuilder.DisplayRotationLetter
instead.License requirements: drafting (“DRAFTING”)
DisplayLabel¶
-
SectionLineStyleBuilder.
DisplayLabel
¶ Returns or sets the display label
-------------------------------------
Getter Method
Signature
DisplayLabel()
Returns: Return type: bool New in version NX6.0.0.
Deprecated since version NX10.0.0: Use
NXOpen.Drawings.ViewSectionLineBuilder.Display
instead.License requirements: None.
-------------------------------------
Setter Method
Signature
DisplayLabel(displayLabel)
Parameters: displayLabel (bool) – New in version NX6.0.0.
Deprecated since version NX10.0.0: Use
NXOpen.Drawings.ViewSectionLineBuilder.Display
instead.License requirements: drafting (“DRAFTING”)
Font¶
-
SectionLineStyleBuilder.
Font
¶ Returns or sets the font
-------------------------------------
Getter Method
Signature
Font()
Returns: Return type: NXOpen.Drawings.SectionLineStyleBuilderFontStyle
New in version NX6.0.0.
Deprecated since version NX10.0.0: Use
NXOpen.Drawings.ViewSectionLineBuilder.LineColorFontWidth
instead.License requirements: None.
-------------------------------------
Setter Method
Signature
Font(font)
Parameters: font ( NXOpen.Drawings.SectionLineStyleBuilderFontStyle
) –New in version NX6.0.0.
Deprecated since version NX10.0.0: Use
NXOpen.Drawings.ViewSectionLineBuilder.LineColorFontWidth
instead.License requirements: drafting (“DRAFTING”)
LabelLocation¶
-
SectionLineStyleBuilder.
LabelLocation
¶ Returns or sets the label location
-------------------------------------
Getter Method
Signature
LabelLocation()
Returns: Return type: NXOpen.Drawings.SectionLineStyleBuilderLabelLocationStyle
New in version NX6.0.0.
Deprecated since version NX10.0.0: Use
NXOpen.Drawings.ViewSectionLineBuilder.LabelLocation
instead.License requirements: None.
-------------------------------------
Setter Method
Signature
LabelLocation(labelLocation)
Parameters: labelLocation ( NXOpen.Drawings.SectionLineStyleBuilderLabelLocationStyle
) –New in version NX6.0.0.
Deprecated since version NX10.0.0: Use
NXOpen.Drawings.ViewSectionLineBuilder.LabelLocation
instead.License requirements: drafting (“DRAFTING”)
Letter¶
-
SectionLineStyleBuilder.
Letter
¶ Returns or sets the letter
-------------------------------------
Getter Method
Signature
Letter()
Returns: Return type: str New in version NX6.0.0.
Deprecated since version NX10.0.0: Use
Drawings.ViewCommonViewLabelBuilder.Letter
instead.License requirements: None.
-------------------------------------
Setter Method
Signature
Letter(letter)
Parameters: letter (str) – New in version NX6.0.0.
Deprecated since version NX10.0.0: Use
Drawings.ViewCommonViewLabelBuilder.Letter
instead.License requirements: drafting (“DRAFTING”)
LineLength¶
-
SectionLineStyleBuilder.
LineLength
¶ Returns or sets the line length
-------------------------------------
Getter Method
Signature
LineLength()
Returns: Return type: float New in version NX6.0.0.
Deprecated since version NX10.0.0: Use
NXOpen.Drawings.ViewSectionLineBuilder.LineLength
instead.License requirements: None.
-------------------------------------
Setter Method
Signature
LineLength(lineLength)
Parameters: lineLength (float) – New in version NX6.0.0.
Deprecated since version NX10.0.0: Use
NXOpen.Drawings.ViewSectionLineBuilder.LineLength
instead.License requirements: drafting (“DRAFTING”)
Offset¶
-
SectionLineStyleBuilder.
Offset
¶ Returns or sets the offset
-------------------------------------
Getter Method
Signature
Offset()
Returns: Return type: float New in version NX6.0.0.
Deprecated since version NX10.0.0: Use
NXOpen.Drawings.ViewSectionLineBuilder.UseOffset
instead.License requirements: None.
-------------------------------------
Setter Method
Signature
Offset(offset)
Parameters: offset (float) – New in version NX6.0.0.
Deprecated since version NX10.0.0: Use
NXOpen.Drawings.ViewSectionLineBuilder.UseOffset
instead.License requirements: drafting (“DRAFTING”)
SelectLetter¶
-
SectionLineStyleBuilder.
SelectLetter
¶ Returns the selected note for jisrotation letter
-------------------------------------
Getter Method
Signature
SelectLetter()
Returns: Return type: NXOpen.SelectTaggedObject
New in version NX6.0.0.
Deprecated since version NX10.0.0: Use
NXOpen.Drawings.ViewSectionLineBuilder.SelectRotationLetter
instead.License requirements: None.
Standard¶
-
SectionLineStyleBuilder.
Standard
¶ Returns or sets the standard
-------------------------------------
Getter Method
Signature
Standard()
Returns: Return type: NXOpen.Drawings.SectionLineStyleBuilderStandardStyle
New in version NX6.0.0.
Deprecated since version NX10.0.0: Use
NXOpen.Drawings.ViewSectionLineBuilder.TypeStandard
instead.License requirements: None.
-------------------------------------
Setter Method
Signature
Standard(standard)
Parameters: standard ( NXOpen.Drawings.SectionLineStyleBuilderStandardStyle
) –New in version NX6.0.0.
Deprecated since version NX10.0.0: Use
NXOpen.Drawings.ViewSectionLineBuilder.TypeStandard
instead.License requirements: drafting (“DRAFTING”)
StubLength¶
-
SectionLineStyleBuilder.
StubLength
¶ Returns or sets the stub length
-------------------------------------
Getter Method
Signature
StubLength()
Returns: Return type: float New in version NX6.0.0.
Deprecated since version NX10.0.0: Use
NXOpen.Drawings.ViewSectionLineBuilder.Overhang
instead.License requirements: None.
-------------------------------------
Setter Method
Signature
StubLength(stubLength)
Parameters: stubLength (float) – New in version NX6.0.0.
Deprecated since version NX10.0.0: Use
NXOpen.Drawings.ViewSectionLineBuilder.Overhang
instead.License requirements: drafting (“DRAFTING”)
UseOffset¶
-
SectionLineStyleBuilder.
UseOffset
¶ Returns or sets the use offset
-------------------------------------
Getter Method
Signature
UseOffset()
Returns: Return type: bool New in version NX6.0.0.
Deprecated since version NX10.0.0: Use
NXOpen.Drawings.ViewSectionLineBuilder.UseOffset
instead.License requirements: None.
-------------------------------------
Setter Method
Signature
UseOffset(useOffset)
Parameters: useOffset (bool) – New in version NX6.0.0.
Deprecated since version NX10.0.0: Use
NXOpen.Drawings.ViewSectionLineBuilder.UseOffset
instead.License requirements: drafting (“DRAFTING”)
Width¶
-
SectionLineStyleBuilder.
Width
¶ Returns or sets the width
-------------------------------------
Getter Method
Signature
Width()
Returns: Return type: NXOpen.Drawings.SectionLineStyleBuilderWidthStyle
New in version NX6.0.0.
Deprecated since version NX10.0.0: Use
NXOpen.Drawings.ViewSectionLineBuilder.LineColorFontWidth
instead.License requirements: None.
-------------------------------------
Setter Method
Signature
Width(width)
Parameters: width ( NXOpen.Drawings.SectionLineStyleBuilderWidthStyle
) –New in version NX6.0.0.
Deprecated since version NX10.0.0: Use
NXOpen.Drawings.ViewSectionLineBuilder.LineColorFontWidth
instead.License requirements: drafting (“DRAFTING”)
Method Detail¶
GetColor¶
-
SectionLineStyleBuilder.
GetColor
¶ Returns the color
Signature
GetColor()
Returns: Return type: Id New in version NX6.0.0.
Deprecated since version NX10.0.0: Use
NXOpen.Drawings.ViewSectionLineBuilder.LineColorFontWidth
instead.License requirements: None.
SetColor¶
-
SectionLineStyleBuilder.
SetColor
¶ Sets the color
Signature
SetColor(color)
Parameters: color (Id) – New in version NX6.0.0.
Deprecated since version NX10.0.0: Use
NXOpen.Drawings.ViewSectionLineBuilder.LineColorFontWidth
instead.License requirements: drafting (“DRAFTING”)
Validate¶
-
SectionLineStyleBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.