SectionLineCollection Class¶
Methods¶
Method | Description |
---|---|
CreateSectionLineBuilder | Creates the section line builder @return |
CreateSectionLineSegmentBuilder | Creates the section line segment builder @return |
CreateSectionLineStyleBuilder | Creates the Section Line Style Builder @return |
CreateSketchSectionLineBuilder | Creates the Sketch Section Line builder @return |
Method Detail¶
CreateSectionLineBuilder¶
-
SectionLineCollection.
CreateSectionLineBuilder
¶ Creates the section line builder
Signature
CreateSectionLineBuilder(sectionLine)
Parameters: sectionLine ( NXOpen.Drawings.SectionLine
) –Returns: Return type: NXOpen.Drawings.SectionLineBuilder
New in version NX6.0.0.
Deprecated since version NX10.0.0: Use
Drawings.SectionViewBuilder.SectionLineSegments
instead.License requirements: drafting (“DRAFTING”)
CreateSectionLineSegmentBuilder¶
-
SectionLineCollection.
CreateSectionLineSegmentBuilder
¶ Creates the section line segment builder
Signature
CreateSectionLineSegmentBuilder()
Returns: Return type: NXOpen.Drawings.SectionLineSegmentBuilder
New in version NX6.0.0.
Deprecated since version NX10.0.0: Use
Drawings.SectionViewBuilder.SectionLineSegments
instead.License requirements: drafting (“DRAFTING”)
CreateSectionLineStyleBuilder¶
-
SectionLineCollection.
CreateSectionLineStyleBuilder
¶ Creates the Section Line Style Builder
Signature
CreateSectionLineStyleBuilder(sectionline)
Parameters: sectionline ( NXOpen.Drawings.SectionLine
) –Returns: Return type: NXOpen.Drawings.SectionLineStyleBuilder
New in version NX6.0.0.
Deprecated since version NX10.0.0: Use
NXOpen.Drawings.ViewSectionLineBuilder
instead.License requirements: drafting (“DRAFTING”)
CreateSketchSectionLineBuilder¶
-
SectionLineCollection.
CreateSketchSectionLineBuilder
¶ Creates the Sketch Section Line builder
Signature
CreateSketchSectionLineBuilder(sectionLine)
Parameters: sectionLine ( NXOpen.Drawings.SectionLine
) –Returns: Return type: NXOpen.Drawings.SketchSectionLineBuilder
New in version NX10.0.0.
License requirements: drafting (“DRAFTING”)